Dev Tools
  • Products
  • More
Dev Tools
Forum ATMEL  ATAVRZUSBSTICK  AT86RF230, USB STICK
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 81 subscribers
  • Views 731 views
  • Users 0 members are here
  • at90usb1287
  • atavrzusbstick
Related

ATMEL  ATAVRZUSBSTICK  AT86RF230, USB STICK

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

Can you confirm me on the following technical information –

 

1.Does this USB stick support 6LoWPAN so that when it is connected to a PC, it shall act as a 6LoWPAN Edge router out-of-box? If not, is there any programming required, and if so what are the components required?

2.Does this USBstick work properly with Windows 7, 8, 8.1, Ubuntu Linux 14.04 LTS, ContikiOS?

3.Can this stick be configured to act as a n/w sniffer? What all protocol level debugging – 6LoWPAN, IPv6 etc. can this support?

4.Related to point 1 – can it’s firmware be modified to make it act like a simple 6LoWPAN node and 6LoWPAN host (some minimalistic routing capabilities to support mesh networking). If not, do you have any other device which can support this functionality.

 

Regards,

PMK

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Well the good news is you can do all you want to do. See http://www.atmel.com/Images/doc5131.pdf . But this is a physical device with the programming up to you. You will need to set the Pan id. You will need to implement the edge router. This is NOT a turnkey solution. It does all the packet level handling including FCS generation. the details are in the PDF above. pmkulkarni is this what you want?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem,

     

         The information that you have given me is about the 802.15.4 transceiver which is useful for someone who is developing h/w for 6LoWPAN and would need to write the device drivers.

     

         However, I am looking for a USB-6LoWPAN dongle which I can connect to my PC and configure my PC to act as a 6LoWPAN Edge router OR 6LoWPAN node. I  want to write small applications using this product (dongle) where I can send-receive sensor data using 6LoWPAN n/w and not delve into the intricacies of the transceiver chip. The actual product (USB-6LoWPAN dongle) is mentioned in the link - AVR RZ USB stick module.

     

         To give an analogy, if we have USB-WiFi dongles, then I can connect it to the USB port of my PC and convert my PC (which does not have in-built WiFi support) into a Wi-Fi device. I am not really writing device driver or programming the WiFi chip, but instead using it to run my WiFi based applications. I am looking at this type of scenario with the USB-6LoWPAN dongle - I would like to convert my PC to act as a 6LoWPAN Edgerouter / 6LoWPAN node. I expect that the drivers for the same should already be present in the firmware of this USB-6LoWPAN device. Considering this in mind, would you let me know on the following -

     

    1.Does this USB stick support 6LoWPAN so that when it is connected to a PC, it shall act as a 6LoWPAN Edge router out-of-box? If not, is there any programming required, and if so what are the components required? Do you have any firmware which I can directly write to the USB stick using PC's USB port with the stick acting as a USB memory device without the need for any additional h/w?

     

    2.Does this USBstick work properly with Windows 7, 8, 8.1, Ubuntu Linux 14.04 LTS, ContikiOS?

     

    3.Can this stick be configured to act as a n/w sniffer? What all protocol level debugging – 6LoWPAN, IPv6 etc. can this support?

     

    4.Related to point 1 – can it’s firmware be modified to make it act like a simple 6LoWPAN node and 6LoWPAN host (some minimalistic routing capabilities to support mesh networking). If not, do you have any other device which can support this functionality.

     

         Hope this helps to give clarity to what I am looking for.

     

    Regards,

    PMK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem,

     

         The information that you have given me is about the 802.15.4 transceiver which is useful for someone who is developing h/w for 6LoWPAN and would need to write the device drivers.

     

         However, I am looking for a USB-6LoWPAN dongle which I can connect to my PC and configure my PC to act as a 6LoWPAN Edge router OR 6LoWPAN node. I  want to write small applications using this product (dongle) where I can send-receive sensor data using 6LoWPAN n/w and not delve into the intricacies of the transceiver chip. The actual product (USB-6LoWPAN dongle) is mentioned in the link - AVR RZ USB stick module.

     

         To give an analogy, if we have USB-WiFi dongles, then I can connect it to the USB port of my PC and convert my PC (which does not have in-built WiFi support) into a Wi-Fi device. I am not really writing device driver or programming the WiFi chip, but instead using it to run my WiFi based applications. I am looking at this type of scenario with the USB-6LoWPAN dongle - I would like to convert my PC to act as a 6LoWPAN Edgerouter / 6LoWPAN node. I expect that the drivers for the same should already be present in the firmware of this USB-6LoWPAN device. Considering this in mind, would you let me know on the following -

     

    1.Does this USB stick support 6LoWPAN so that when it is connected to a PC, it shall act as a 6LoWPAN Edge router out-of-box? If not, is there any programming required, and if so what are the components required? Do you have any firmware which I can directly write to the USB stick using PC's USB port with the stick acting as a USB memory device without the need for any additional h/w?

     

    2.Does this USBstick work properly with Windows 7, 8, 8.1, Ubuntu Linux 14.04 LTS, ContikiOS?

     

    3.Can this stick be configured to act as a n/w sniffer? What all protocol level debugging – 6LoWPAN, IPv6 etc. can this support?

     

    4.Related to point 1 – can it’s firmware be modified to make it act like a simple 6LoWPAN node and 6LoWPAN host (some minimalistic routing capabilities to support mesh networking). If not, do you have any other device which can support this functionality.

     

         Hope this helps to give clarity to what I am looking for.

     

    Regards,

    PMK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    1. No/No

    2. No, driver not provided

    3 Maybe

    4 No.

     

    This does what you want http://www.ti.com/tool/CC2531EMK?keyMatch=2531&tisearch=Search-EN

    Clem