Dev Tools
  • Products
  • More
Dev Tools
Forum Help needed to find component
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 80 subscribers
  • Views 527 views
  • Users 0 members are here
Related

Help needed to find component

e14 Contributor
e14 Contributor over 10 years ago

Hello All,

I regularly hand build my project boards using proto board with a 0.1 inch (2.54mm) pin spacing.


I am looking for a suitable SIL socket similar to http://uk.farnell.com/harwin/d01-9972042/socket-sil-20way/dp/1023034, that will mate with a SIL header similar to M20-9992046 - HARWIN - Board-To-Board Connector, M20 Series, Through Hole, Header, 20, 2.54 mm, Tin | Farnell element14.

 

The problem I have is that I cannot find any SIL socket of the type above that will accept the SIL header, as the socket is to small for the header PIN. And I need SIL socket strips that I can cut to size.

 

Can anyone suggest a suitable SIL socket from Farnell?

 

thanks,

Alex

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Fischer makes some: BL1.36Z - FISCHER ELEKTRONIK - Wire-To-Board Connector, BL Series, Through Hole, Receptacle, 36, 2.54 mm, Tin | Farnell … 3M makes some: 929974-01-16 - 3M - CONNECTOR, RECEPTACLE, 16…
  • dougw
    dougw over 10 years ago

    Fischer makes some:

    BL1.36Z - FISCHER ELEKTRONIK - Wire-To-Board Connector, BL Series, Through Hole, Receptacle, 36, 2.54 mm, Tin | Farnell …

     

    3M makes some:

    929974-01-16 - 3M - CONNECTOR, RECEPTACLE, 16 POSITION, 1ROW, 2.54MM | Farnell element14

     

    Wurth makes some although they are not breakable:

    61303211821 - WURTH ELEKTRONIK - Wire-To-Board Connector, WR-PHD Series, Through Hole, Receptacle, 32, 2.54 mm, Gold | F…

     

    TE Connectivity makes some:

    1-215297-0 - TE CONNECTIVITY / AMP - Wire-To-Board Connector, Vertical, AMPMODU HV-100 Series, Through Hole, Receptacle,…

    1-215297-6 - TE CONNECTIVITY / AMP - Wire-To-Board Connector, Vertical, AMPMODU HV-100 Series, Through Hole, Receptacle,…

     

    Sullins Makes some

     

    etc

     

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to dougw

    Thanks Doug,

    that's a great help. I'll order some of the FISCHER connectors to give them  a test out.

     

    Alex