Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Possible Schottky?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 80 subscribers
  • Views 738 views
  • Users 0 members are here
  • frontpage
Related

Possible Schottky?

ghendricks18
ghendricks18 over 10 years ago

I have this component that I am trying to get a part number off of I can't find a manufacturer that used this marking code.  I believe it is a Schottky DIode based on the circuit it is in but I need to know the specifications.

image

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    jc2048 over 10 years ago

    Several manufacturers (Vishay for instance) use codes like U3J and S3J, for ultrafast and standard rectifiers respectively [package marking same as part code]. The 3 is 3A and the J indicates 600V. It's possible you might find a manufacturer that uses 3J for the standard part without a prefix, but I think they would be physically bigger than the part you show.

     

    What leads you to think it's a Schottky? Have you measured the forward voltage?

     

    To help narrow your search down a bit, you could measure the package and work out what it is.

     

    Other than that it's difficult to help. With everyone making up their own codes and not even publishing sensible lists of what they are it's painful trying to identify parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ghendricks18
    ghendricks18 over 10 years ago in reply to jc2048

    It measures as a DO-214AB package, the circuit is with a LM2596 and all the other components match the Adjustable output series Buck regulator.  That circuit from TI indicated that it is a 1N5825 but because of the marking I want to make sure that is what I have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ghendricks18
    ghendricks18 over 10 years ago in reply to jc2048

    It measures as a DO-214AB package, the circuit is with a LM2596 and all the other components match the Adjustable output series Buck regulator.  That circuit from TI indicated that it is a 1N5825 but because of the marking I want to make sure that is what I have.