Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog [FRDM-K64F + Kinetis Design Studio (KDS)+Processor Expert(PE)] Interfacing inbuilt 6-axis sensor FXOS8700 and displaying the data on terminal
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 11 Feb 2015 7:46 AM Date Created
  • Views 2835 views
  • Likes 2 likes
  • Comments 16 comments
  • fxos8700cq
  • frdm-k64f
  • k64f
Related
Recommended

[FRDM-K64F + Kinetis Design Studio (KDS)+Processor Expert(PE)] Interfacing inbuilt 6-axis sensor FXOS8700 and displaying the data on terminal

bheemarao
bheemarao
11 Feb 2015

Here is a project created to interface and explore the features of FXOS8700 sensor available onboard with K64F freedom board.

 

FXOS8700CQ is a small, low-power, 3-axis linear accelerometer and 3-axis magnetometer combined into a single package. The device features a selectable I2C or point-to-point SPI serial interface with 14-bit accelerometer and 16-bit magnetometer ADC resolution along with smart-embedded functions.

 

Before we start this project below are the pre-requisites:

  1. KDS software tool from Freescale
  2. FRDM-K64F Freedom development board

Let’s start on creating a project to interface this sensor board using Kinetis Design studio on Processor Expert platform.

 

image

 

 

Next select the device: you have 2 options for selecting it, one is by “Boards” and other is by “Processors” i am selecting it from the “Boards” option.

 

image

 

Select the board part number FRDM-K64 and proceed further


Make the selection of processor expert in standalone as shown below:

image

 

Click finish

 

You can see the project creation progress bar

 

image

 

 

Now select the pin settings from components view and select the I2C section as shown below:

 

image

 

 

As the sensor FXOS8700 are physically connected to I2C pins of K64 board toPTE24 and PTE25.


Expand the I2C window and assign I2C0 (channel-0) SCL-> PTE24 and I2C0 (channel-0) SDA -> PTE25 as shown in below snap shot

image


 

Next select UART window from pin configuration main menu as shown below:


As UART0’s RX is connected to PTB16 and UART’s TX is connected to PTB17.


This UART port pins are required for console terminal output.

 

image

 

 

Next we need to add FXOS8700 device module which is available in component library.

 

image


 

Double click on the FXOS8700CQ module so that it is added to our project.


Automatically its referenced components get added to the components of project.


Click on WAIT1 and ok button for adding it to reference component.


image

WAIT1 and GI2C1 modules gets added as shown below.

 

image

 

Click on FXOS8700CQ component and configure the settings as shown below:

 

image

 

 

Make sure slave address is “1D” and there are 2 dependant components GI2C1 and WAIT1 for FXOS component module


Next double click on GI2C1: GenericI2C module to set the parameters.

 

image

 

 

Next click on “>”  button

 

image

 

 

You need to assign the I2C channels, and I2C pins for this module

 

image

 

As this board is connected to sensor through I2C channel 0 and we had assigned the same earlier in pins configuration i.e I2C0 (channel-0)  SCL-> PTE24 and SDA -> PTE25

 

Now set the parameters of the I2C module as shown below:

 

 

image

 

Next add the ConsoleIO component module from component library as shown below:

 

image

 

Double click on the module component to add to our project:

 

image

 

 

Next click on ConsoleIO_Serial_LDD button as shown below:

 

image

We have configured UART0 as shown below:

image

 

Now generate the project by clicking the below shown button

image

 

It Builds with no errors as shown below:


image


Now we are going to add our code in “main.c” file

 

#include "Cpu.h"

#include "Events.h"

#include "Pins1.h"

#include "FX1.h"

#include "GI2C1.h"

#include "WAIT1.h"

#include "CI2C1.h"

#include "CsIO1.h"

#include "IO1.h"

/* Including shared modules, which are used for whole project */

#include "PE_Types.h"

#include "PE_Error.h"

#include "PE_Const.h"

#include "IO_Map.h"

#include "PDD_Includes.h"

#include "Init_Config.h"

/* User includes (#include below this line is not maintained by Processor Expert) */

 

/*lint -save  -e970 Disable MISRA rule (6.3) checking. */

 

int main(void)

/*lint -restore Enable MISRA rule (6.3) checking. */

{

  /* Write your local variable definition here */

 

  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/

  PE_low_level_init();

  /*** End of Processor Expert internal initialization.                    ***/

 

  /* Write your code here */

 

 

  int16_t x,y,z,xm,ym,zm;

  int16_t value1, value2, value3, addr;

  uint8_t ret;

  byte res = ERR_OK;

  int16_t *data[3];

  uint8_t who, temp;

  uint16_t magX, magY, magZ;

 

 

  printf("Hello\n");

  FX1_Init();

 

 

  for(;;) {

        /* get WHO AM I values */

 

      if (FX1_WhoAmI(&who)!=ERR_OK) {

          return ERR_FAILED;

      }

 

      printf("Who Am I  value in decimal \t: %4d\n",who);

      for(xm=0;xm<=30000;xm++); //delay

 

 

      /* get raw temperature values */

 

      if (FX1_GetTemperature(&temp)!=ERR_OK) {

                return ERR_FAILED;

            }

 

      printf("RAW Temperature value in decimal \t: %4d\n",temp);

       for(xm=0;xm<=30000;xm++);  //delay

 

 

 

//set up registers for accelerometer and magnetometer values

 

      if (FX1_WriteReg8(FX1_CTRL_REG_1, 0x00) != ERR_OK) {

          return ERR_FAILED;

      }

      if (FX1_WriteReg8(FX1_M_CTRL_REG_1, 0x1F) != ERR_OK) {

          return ERR_FAILED;

      }

      if (FX1_WriteReg8(FX1_M_CTRL_REG_2, 0x20) != ERR_OK) {

          return ERR_FAILED;

      }

      if (FX1_WriteReg8(FX1_XYZ_DATA_CFG, 0x00) != ERR_OK) {

          return ERR_FAILED;

      }

      if (FX1_WriteReg8(FX1_CTRL_REG_1, 0x0D) != ERR_OK) {

          return ERR_FAILED;

      }

 

 

  // get the X Y Z accelerometer values

 

        x = FX1_GetX();

        y = FX1_GetY();

        z = FX1_GetZ();

 

 

   printf("Accelerometer value \tX: %4d\t Y: %4d\t Z: %4d\n",x,y,z);

          for(xm=0;xm<=30000;xm++); //delay

 

 

   

// get the X Y Z magnetometer values

 

        if (FX1_GetMagX(&magX)!=ERR_OK) {

                  return ERR_OK;

              }

        if (FX1_GetMagY(&magY)!=ERR_OK) {

                         return ERR_OK;

                     }

        if (FX1_GetMagZ(&magZ)!=ERR_OK) {

                         return ERR_OK;

                     }

 

 

  printf("Magnetometer value \tX: %4d\t Y: %4d\t Z: %4d\n",magX,magY,magZ);

        for(xm=0;xm<=30000;xm++); //delay

 

 

  }

 

 

 

  /* For example: for(;;) { } */

 

  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/

  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/

  #ifdef PEX_RTOS_START

    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */

  #endif

  /*** End of RTOS startup code.  ***/

  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/

  for(;;){}

  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/

} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

 

/* END main */

/*!

** @}

*/

/*

** ###################################################################

 

 

Explanation of code:

 

if (FX1_WhoAmI(&who)!=ERR_OK) {

                return ERR_FAILED;

         }

 

The FX1_WhoAmI( ) function Returns the value of the WHO_AM_I (0x0D) register. The return value is stored in variable ‘who’ its value is “199” in decimal and ‘C7’ in Hex which is printed in output terminal

 

if (FX1_GetTemperature(&temp)!=ERR_OK) {

                       return ERR_FAILED;

                }

 

 

The function ‘FX1_GetTemperature( )’ reads the value from the register 0x51 which returns the temperature of the die as signed 8bit and stores in variable temp, this value

 

Below are the setup values written to the registers to get the magnetometer and accelerometer values

 

if (FX1_WriteReg8(FX1_CTRL_REG_1, 0x00) != ERR_OK) {

                return ERR_FAILED;

         }

 

write 0000 0000 = 0x00 to accelerometer control register 1 to place FXOS8700 into standby

[7-1] = 0000 000

[0]= active=0

 

if (FX1_WriteReg8(FX1_M_CTRL_REG_1, 0x1F) != ERR_OK) {

                return ERR_FAILED;

         }

 

write 0001 1111 = 0x1F to magnetometer control register 1

[7]: m_acal=0: auto calibration disabled

[6]: m_rst=0: no one-shot magnetic reset

[5]: m_ost=0: no one-shot magnetic measurement

[4-2]: m_os=111=7: 8x oversampling (for 200Hz) to reduce magnetometer noise

[1-0]: m_hms=11=3: select hybrid mode with accel and magnetometer active

 

if (FX1_WriteReg8(FX1_M_CTRL_REG_2, 0x20) != ERR_OK) {

                return ERR_FAILED;

         }

 

write 0010 0000 = 0x20 to magnetometer control register 2

[7]: reserved

[6]: reserved

[5]: hyb_autoinc_mode=1 to map the magnetometer registers to follow the accelerometer registers

[4]: m_maxmin_dis=0 to retain default min/max latching even though not used

[3]: m_maxmin_dis_ths=0

[2]: m_maxmin_rst=0

[1-0]: m_rst_cnt=00 to enable magnetic reset each cycle

 

if (FX1_WriteReg8(FX1_XYZ_DATA_CFG, 0x00) != ERR_OK) {

                return ERR_FAILED;

         }

 

write 0000 0001= 0x00 to XYZ_DATA_CFG register

[7]: reserved

[6]: reserved

[5]: reserved

[4]: hpf_out=0

[3]: reserved

[2]: reserved

[1-0]: fs=00 for accelerometer range of +/-2g range with 0.244mg/LSB

 

if (FX1_WriteReg8(FX1_CTRL_REG_1, 0x0D) != ERR_OK) {

                return ERR_FAILED;

         }

 

write 0000 1101b = 0x0D to accelerometer control register 1

[7-6]: aslp_rate=00

[5-3]: dr=001=1 for 200Hz data rate (when in hybrid mode)

[2]: lnoise=1 for low noise mode

[1]: f_read=0 for normal 16 bit reads

[0]: active=1 to take the part out of standby and enable sampling

 

 

Now it’s time to build the project:

 

image

 

image

 

You can see the build is finished successfully with no errors

image

 

Now it is ready to debug/execute


Click on Debug configuration as shown below:

image


image

 

Then it shows the project name automatically as “K64-FXOS8700-PE_Debug_Segger”

 

image

 

Now connect the K64 board to OPEN SDA port to your computer through USB cable, Then click on Debug button.


You can see below Debug window screen


image

 

Make sure you have open the corresponding hyperterminal window from your ‘Computer Management’ Device manager window:

In my case it is connected to COM23 port

 

image

 

Now click on green ‘Resume’ button

 

image

 

Open COM23 port from any of the hyper terminal application (putty in my case)

 

image

 

You can see the output of the accelerometer/magnetometer values in hyper terminal as shown below:

 

image

 

Happy Sensing  image image image

 

 


Attachments:
K64-FXOS8700-PE.rar
  • Sign in to reply

Top Comments

  • bheemarao
    bheemarao over 11 years ago +1
    I have enclosed the Project folder for your hands-on / reference. Best Regards Bheema Rao
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to bheemarao

    thanks for ur reference, i was do it..its easy when using PE ADC, but unfornatelly PE cant access DMA-ADC.

    So i must using PE Init_ADC (many sample project use it ), again i find problem, PE Init_ADC can't change and develop ADC0_Init.C. Furthermore, i can't access variable in ADC0_Init.c in main.c. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bheemarao
    bheemarao over 10 years ago in reply to e14 Contributor

    Hi Amin,

     

    You can refer to the mcuoneclipse link below:

    http://mcuoneclipse.com/2013/02/10/tutorial-adc-with-the-freedom-board/

     

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to bheemarao

    ok thanks bheema. please can u give me a spesific sample. its dificult to me to learn many sample and reference about dma-adc-K64F.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bheemarao
    bheemarao over 10 years ago in reply to e14 Contributor

    Hi Amin,

     

    Please find below few of the reference links for your requirement:

     

    Measuring all ADC inputs on FRDM-KL25 using DMA

    https://community.freescale.com/docs/DOC-96507

    http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4631.pdf

     

     

    ADC with Freedom board mcuon eclipse link:

     

    http://mcuoneclipse.com/2013/02/10/tutorial-adc-with-the-freedom-board/

    and few of the Freescale community link for DMA

    https://community.freescale.com/message/462300?et=watches.email.thread#462300

    https://community.freescale.com/thread/317421

     

    App note for Using DMA to Emulate ADC

    http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf

    http://cache.freescale.com/files/32bit/doc/app_note/AN4590SW.zip

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    hello bheemaro,

     

    i want build high speed ADC send to high speed hyperterminal. so it is must using buffer via DMA.

    i want capture signal more than 50kHz and then send to hyperterminal, that i plan to reconstruction to GUI software.

    btw i use K64F FRDM.

    can u give me reference sample project link?

     

    thanks for ur creativity that many sample project i can learn form you.

     

    Best Regards,

    Amin_iman

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>