Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform

Blog

  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Evaluating FRDM-KW41Z using NXP Test and Tool Utility

    bheemarao
    bheemarao
    This blog demonstrates on testing the freedom KW41Z board using NXP’s Test and Tool utility software. We are testing the board using MAC2006 FSCI packet error rate.  The Test Tool utility is a Windows®︎ based graphical interface that communicates...
    • 28 Nov 2016
  • Getting started with demo-apps and executing ecompass application for FRDM-KW41Z NXP Freedom Development Platform

    bheemarao
    bheemarao
    This document shows how to execute the demo-apps for  FRDM-KW41ZFRDM-KW41Z that comes along with connectivity software package To proceed further the below are the prerequisites: 1. KDS3.2.0 installed on your computer(You can download lates...
    • 21 Nov 2016
  • Getting Started with KSDK and FreeRTOS [Running Freertos_mutex example using FRDM-KW41Z]

    bheemarao
    bheemarao
    Kinetis Software Development Kit (KSDK) 2.0 provides a comprehensive software package with pre-integrated FreeRTOS OS. Freescale provides FreeRTOS OS additions, such as RTOS driver wrappers, RTOS ready FatFs file system, and the implementation of Fre...
    • 21 Nov 2016
  • Wireless UART demo using Kinetis BLE android app with FRDM-KW41Z Freedom Board

    bheemarao
    bheemarao
    In my earlier blog i had demonstrated Wireless UART using two KW41Z board for demonstrating wireless uart using BLE.Here in part-2 we will execute with one KW41Z board + the other with Smart phone with Kinetis BLE Toolbox android app. Required:1...
    • 11 Nov 2016
  • Running Wireless UART application using Bluetooth®︎ Low Energy with FRDM-KW41Z

    bheemarao
    bheemarao
    This blog describes the Bluetooth®︎ Low Energy Stack enablement for the Freescale Freedom development platform with the Kinetis KW41Z dual wireless mode system-on-chip (SoC). The Software Development Package provides a Bluetooth Low Energy v4.2-compli...
    • 9 Nov 2016
  • Running a Hello World demo on FRDM-KW41Z using Kinetis Design Studio IDE

    bheemarao
    bheemarao
    This blog describes the steps required to configure Kinetis Design Studio(KDS IDE to build run and debug example applications The helloworld demo application targeted for the  FRDM-K64FFRDM-K64F Freedom hardware platform is used as an example th...
    • 6 Nov 2016
  • Part-2: Executing SMAC connectivity demo application using KW41Z freedom board on terminal window

    bheemarao
    bheemarao
    In continuation to Part-1 (Part-1: Getting started with FRDM-KW41Z [executing MKW41Z SMAC based Connectivity Test application]) of SMAC connectivity demo, we will see how to execute the demo application on hyperterminal. Open a putty or tera ter...
    • 24 Oct 2016
  • Part-1: Getting started with FRDM-KW41Z [executing MKW41Z SMAC based Connectivity Test application]

    bheemarao
    bheemarao
    This blog introduces to New  FRDM-KW41ZFRDM-KW41Z Wireless Microcontrollers(MCU development board and demonstrates the connectivity test application  The  FRDM-KW41ZFRDM-KW41Z development board is an evaluation environment supporting N...
    • 24 Oct 2016
  • Displaying 12-bit ADC value on hyperterminal by connecting a potentiometer and indicating through LED [Implementing 12-bit ADC using KSDK on FRDM-KL28Z freedom board by polling method]

    bheemarao
    bheemarao
    This blog gives an overview on implementing 12-bit ADC by polling method and displaying the digital values over hyper terminal. Corresponding to the digital values the Red Green and Blue LED’s are indicated. For 12-bit resolution ADC the digital...
    • 4 Oct 2016
  • Introduction to KSDK Project Generator 2.2 tool and how to create new project using KL28Z [Create a project using KSDK Project Generator and toggling an LED on FRDM-KL28Z NXP Freedom Development Platform]

    bheemarao
    bheemarao
    The KSDK Project Generator requires the user to install an instance of KSDK 1.2.0, 1.3.0 or 2.x before generating new projects. Visit www.nxp.com/ksdk to get the Kinetis SDK. Features of KSDK Project Generator 2.2:The following features are avai...
    • 3 Oct 2016
  • Getting Started with FRDM-KL28Z NXP Freedom Development Platform [Running a Bubble demo application using Kinetis Development Studio IDE and its tool chain]

    bheemarao
    bheemarao
    This document introduces new freedom development board FRDM-KL28Z and demonstrates the bubble application And how to import the existing project of Kinetis SDK V2.0(for FRDM-KL28 using the kinetis Design Studio version 3.2.0 implemented using  F...
    • 19 Sep 2016
  • Kinetis SDK V2.0 configuration generation for FRDM-KL28Z

    bheemarao
    bheemarao
    The below steps are to be followed to start working on New freedom board FRDM-KL28Z using Kinetis Expert system configuration tool. Open the nxp link   https://kex.nxp.com/en/welcome  Click on Build an SDK as shown and select “New...
    • 18 Sep 2016
  • How to set and check the 48-bit BLE MAC Address into KW4xZ/3xZ

    bheemarao
    bheemarao
    The content has been cited from https://community.nxp.com/thread/429919  Below is the summary on how to write and read MAC address for KW40/41 MCUs cited from NXP community https://community.nxp.com/thread/429919  On the BLE Host Stack...
    • 22 Aug 2016
  • Executing Wireless messenger Application using KW40Z connectivity software [Demonstrating and executing the cloning of wireless messenger project using FRDM-KW40Z NXP Freedom Development Platform]

    bheemarao
    bheemarao
    This document shows a brief demonstration on executing wireless messenger application using NXP Bluetooth FRDM-KW40Z wireless development board. To proceed further the below are the prerequisites:1.   The freedom hardware board i.e FRD...
    • 19 Aug 2016
  • Demonstrating Power Measurement tool (PMT) using LPCXpreso on LPC4367 development board

    bheemarao
    bheemarao
    Refer to my earlier blog on working with OM13088-LPC4367 LPCXpresso development board; i am using the same project executable of peripheral timer which blinks LED at every 1 second interrupt for demonstrating the PMT The Power measurement tool e...
    • 7 Aug 2016
  • Working on with LPCXpresso development board OM13088 with LPC4367 MCU

    bheemarao
    bheemarao
    The LPCXpresso family of boards provides a powerful and flexible development system for NXP®︎'s Cortex-M MCUs. The LPCXpresso4367 board has been developed by NXP to enable evaluation of and prototyping with the LPC4300 series of MCUs, and features the...
    • 4 Aug 2016
  • Create a binary file *.srec for OTAP application using KW40Z freedom board

    bheemarao
    bheemarao
     What is OTAP? OTAP is the acronym for On The Air Programming. A BLE OTAP system consists of an OTAP Server and an OTAP Client which exchange an image file over the air using the infrastructure provided by BLE (GAP, GATT, SM) via a custom G...
    • 1 Aug 2016
  • Out-of-box demo of OM13078 (LPC54102+ Sensor Shield Board (SSB)) NXP LPC54102-based Application-in-a-box Sensor Processing/Motion Solution

    bheemarao
    bheemarao
    This blog demonstrated out of box demo for NXP’s  OM13078OM13078 development board and describes the NXP LPC54102 Sensor Processing/Motion Solutions(SPM-S The LPC54102 Sensor Processing/Motion Solution(SPM-S combines the LPC54102 MCU and a range...
    • 25 Jul 2016
  • Executing Wireless UART Application using KW40Z connectivity software [Demonstrating and executing the cloning of wireless uart project using FRDM-KW40Z NXP Freedom Development Platform]

    bheemarao
    bheemarao
    This document shows a brief demonstration on executing wireless uart application using NXP Bluetooth Low Energy Software for the KW40Z wireless microcontroller platforms. To proceed further the below are the prerequisites:1.   The free...
    • 11 Jul 2016
  • Cloning the BLE projects from KW40Z connectivity software and executing it using IAR tool [Demonstrating the cloning of Bluetooth example project using FRDM-KW40Z NXP Freedom Development Platform]

    bheemarao
    bheemarao
    Here in this document we shall explore the KW40Z connectivity software package and flow through the process of cloning the Bluetooth example projects i.e reusing the existing projects and modifying it as per requirement which saves design and coding ...
    • 4 Jul 2016
  • Creating multicore  Master- Slave project pair using LPCXpresso LPC54102 development board (Cortex-M4 core as master, M0+ as slave)

    bheemarao
    bheemarao
    This blog is in continuation to my earlier blog “Working with Multicore blinky example (M4 core as master, M0 as slave) using OM13077[exploring multicore platform using existing example project using LPC54102 microcontroller on LPCXpresso]” the conte...
    • 27 Jun 2016
  • Working with Multicore blinky example (M4 core as master, M0 as slave) using OM13077[exploring multicore platform using existing example project using LPC54102 microcontroller on LPCXpresso]

    bheemarao
    bheemarao
    This blog is an understanding and introduction to multicore platform, working with existing multicore blinky example (M4 core as master, M0 as slave). This multicore example sets up the M4 core as the MCU master that communicates with the M0 core ru...
    • 27 Jun 2016
  • Hackster.io contest for Hexiwear: 3x drones DJI Phantom3 Pro Ltd Ed Carbon with 4K camera to WIN ($1,500 value)

    GregC
    GregC
    Contest Summary NXP is sponsoring a customer contest with hackster.io and the community users already familiar with NXP (ex-Freescale) Kinetis MCU programming (especially FRDM-K64F and FRDM-KW40Z ones) could be interested to participate.Particip...
    • 22 Jun 2016
  • How to create new project on LPCXpresso for OM13077[Creating new project on GPIO button polling method and turning on/off LED]

    bheemarao
    bheemarao
    This blog is in continuation to my earlier blog on out of box on  OM13077OM13077 LPCXpresso board Introduction to OM13077 Dual processor cores NXP LPCXpresso development board and demonstrating the existing project using LPCXpresso tool [Importi...
    • 10 Jun 2016
  • Build and Run the BLE Wireless Connectivity Example Demos on the FRDM-KW40Z [Demonstrating Heart Rate monitor using android app based on Bluetooth Low Energy implemented on KW40Z]

    bheemarao
    bheemarao
    In continuation to my earlier blog on [demonstrating wireless point-to-point out of the box connectivity based on SMAC] This document demonstrates the simulation of the Heart rate sensor (emulating by connecting a potentiometer) using NXP Blueto...
    • 2 Jun 2016
>