Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog [FRDM-KL25Z - PE - Eclipse] Project: Snake Game with Nokia 5110 Display
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 14 Jul 2014 12:23 PM Date Created
  • Views 1472 views
  • Likes 1 like
  • Comments 3 comments
  • freescale
  • kinetis
  • kl25z
  • freedom
Related
Recommended

[FRDM-KL25Z - PE - Eclipse] Project: Snake Game with Nokia 5110 Display

bheemarao
bheemarao
14 Jul 2014

“This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.”


So I have a graphics driver for a Nokia display (see “Zero Cost 84×48 Graphical LCD for the Freedom Board“), I have a joystick shield (see “JoyStick Shield with the FRDM Board“) and I do have a Freescale Freedom board: why not creating a simple game for it? Snake!

Snake Game with FRDM-KL25Z Board

Snake Game with FRDM-KL25Z Board

My first mobile phone was a Nokia with a 84×48 black/white display, and I loved it for many reasons, including having the ‘Snake’ game (see: http://en.wikipedia.org/wiki/Snake_%28video_game%29). An ARM Cortex M0+ is way overpowered for that simple game, still it is fun to make and game it :-).

The game is very simple: A snake is running around, and I can control it with the cursor/joystick with up, down, left and right. The snake has to ‘eat’ the ‘food’, and the snake gets longer the more food is eaten. But the snake shall *not* touch the outside border.

idea: Usually there is another rule that the snake shall not touch itself.  But I was too lazy to make it.

 

Snake with Food

Snake with Food

For the project I ordered a black joystick shield for $11.27, as the soldering quality of the previous ‘white’ one was very bad. The Nokia 5110 LCD I ordered from DX.com for $3.87so it would directly match with the joystick shield. So makes $30 in total including the FRDM-KL25Z board.

Startup Screen for Snake Game

Startup Screen for Snake Game

Ready to Play Snake Game

Ready to Play Snake Game

 

The video shows the game in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Snake game runs as a FreeRTOS task. The drawing and graphics including fonts are implemented with Processor Expert components:

Graphical Display Driver

Graphical Display Driver

Font and Font Driver

Font and Font Driver

Summary

So I have another nice usage for my boards and the joystick shields image. I need to admit that I’m not very good at the game. My daughter reached level 4 in the first attempt, while my max level is 2, maybe it is just the age image. But I’m too honest *not* to build in a cheat mode, or should I? Maybe image

As always, the sources are available on GitHub.

Happy Snaking image

  • Sign in to reply
  • shabaz
    shabaz over 12 years ago in reply to bheemarao

    Hi Bheema,

     

    Definitely. I think a user interface/control panel type shield could be useful for many projects, so I'm trying to make it fairly generic and open source. I originally planned to have an LED display (for visibility from a distance) but the OLED displays are fairly bright and are the same cost or cheaper and give a lot more flexibility in what can be displayed (and more easier to lay out on a PCB). This is for the KL25Z but hopefully it will work on at least a couple of other FRDM boards (I've got three different ones to test with).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bheemarao
    bheemarao over 12 years ago in reply to shabaz

    That's really good,

    Can you share what you are doing(on which freedom board) which will be really helpful for the users who might be working on similar kind of implementation (if it's not confidential)

     

    Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago

    That's very cool!

     

    I've been using this OLED displaythis OLED display recently, I'm making a shield with this on it, and some push-buttons for the FRDM series.

    Not really a gaming shield, but more for use as a control panel.