Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog [FRDM-KL46Z + KDS + PE + Mikroe Click SHT11] Tutorial: Interfacing SHT1x click module and displaying sensor data on hyperterminal
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 5 May 2015 12:42 PM Date Created
  • Views 753 views
  • Likes 1 like
  • Comments 1 comment
  • sht1x
  • click_shield
  • click_board
  • frdm-kl46z
Related
Recommended

[FRDM-KL46Z + KDS + PE + Mikroe Click SHT11] Tutorial: Interfacing SHT1x click module and displaying sensor data on hyperterminal

bheemarao
bheemarao
5 May 2015

Here is a project created to interface SHT11 click module (humidity and temperature sensor) with FRDM-KL46Z freedom board.


Before we start this project below are the pre-requisites:

  • KDS 2.0.0 software tool from Freescale

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE)

  • FRDM-KL46Z Freedom development board
  • FRDM-KL46Z click shield / Arduino UNO click shield [MIKROE-1581] (optional)

(http://www.mikroe.com/click/frdm-kl46z-shield/)

  • SHT1x click module [MIKROE-949]



SHT11 details:


[http://www.mikroe.com/click/sht1x/]

 

SHT11 Click is an accessory board in mikroBusTm form factor. It includes a digital humidity and temperature sensor SHT11. A unique capacitive sensor element is used to measure relative humidity while the temperature is measured by a band-gap sensor. Serial I2C interface and factory calibration, allow easy and fast system integration. Board is set to use 3.3V power supply by default.

image

 

Communication with the SHT11 sensor is done using I2C interface. Temperature can be represented in 12-bit or 14-bit format in operating range from -40 to +100°C with accuracy of +/- 0.5°C at room temperature. Humidity can be represented in 8-bit or 12-bit resolution with +/- 3% accuracy.

The schematic of the click board is as shown below:

 

image

 

FRDM-KL46Z click shield details:

 

image

 

http://www.mikroe.com/click/frdm-kl46z-shield/

 

 

FRDM-KL46Z click shield is an extension for Freescale's FRDM-KL46Z development platform. It's a simple shield with two mikroBUSTm host sockets that allow you to interface more than 100 different types of click boards with the Kinetis L series KL4x MCU aboard FRDM-KL46Z. Quickly add functionalities like GSM, GPS, WiFi, ZigBee, Bluetooth, or thunder detection, proximity and color sensing and so on. The package includes two 1x8 headers, and single 1x10, and 1x6 headers.

mikroBUSTm is specially designed pinout standard with SPI, I2C, Analog, UART, Interrupt, PWM, Reset and Power supply pins.

FRDM-KL46Z click shield allows you to use click add-on boards from MikroElektronika on Freescale’s FRDM-KL46Z development platform.


Key features

  • Two mikroBUSTm host connectors for attaching click boards.
  • Oscillator probe

 

Key Benefits

  • Shield is designed to stay within dimensions of FRDM-KL46Z for smooter integration.
  • Brings click board connectivity to Freescale’s Kinetis L Series KL4x

 

So let me start from creating the new project:

image

 

Create a New KDS project name as shown, i have selected “KL46-sht1x”

image

Next select the device: you have 2 options for selecting it, one is by “Boards” and other is by “Processors” i am selecting it from the “Boards” option.

image

 

Select the board part number FRDM-KL46Z and proceed further


Make the selection of processor expert in standalone as shown below:

image

 

Click finish and proceed further.

 

Now we will proceed further by adding our components: as we are implementing the I2C logic using Bit Banging we need only 2 bits as SDA/SCL which can act as both input and output by software logic.


The required components are as follows:

  1. BitIO_LDD:  for SDA bit I/O
  2. BitIO_LDD:  for SCL bit I/O
  3. Wait:
  4. ConsoleIO: for hyper terminal output

 

Select component library and select BitIO_LDD component as shown below:

image

 

Add this component two times as we require 2 Bits for SDA and SCL interface signal

Now rename the component Bit1 IO as SDA as shown below:


image

Now select the pin for I/O in our case the SDA bit is connected to PTC2 of the freedom board

 

image

 

Similarly connect Bit2 component as shown below:

SCL is connected to PTC1


image

 

Now add the component “Wait” as shown below:
image


 

Next add the ConsoleIO component module from component library as shown below:

image


 

Double click on the module component to add to our project:


As UART0’s RX is connected to PTA1 and UART0’s TX is connected to PTA2.


This UART port pins are required for console terminal output.


Next click on ConsoleIO_Serial_LDD button as shown below:

 

image

We have configured UART0 as shown below:

image

 

 

We can see all the four components added with required settings as shown below:


Now generate the project by clicking the below shown button

 

image

 

It Builds with no errors as shown below:

 

image

 

Now we are going to add our code in “main.c” file

 

int main(void)
/*lint -restore Enable MISRA rule (6.3) checking. */
{
/* Write your local variable definition here */
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
 PE_low_level_init();
/*** End of Processor Expert internal initialization.                    ***/
/* Write your code here */
/* For example: for(;;) { } */
unsignedint *p_value1, *p_value2;
 SDA_Init(SDA_Ptr);
 SCL_Init(SCL_Ptr);
while(1){
       Read_SHT11(&temp, &rel_hum);
       WAIT1_Waitms(250);
printf(" Temperature value T: %f %% degC\t", temp);
printf(" Humidity value RH: %f pct\r\n", rel_hum);
       }


Below are the driver functions required:


void s_transstart()
{
 //Initial state
SDA_SetDir(SDA_Ptr, 0); //SDA_SetDir(SDA_Ptr, 1); //set as output// SDA_dir = 1;                            //release DATA-line
SDA_SetVal(SDA_Ptr);  // giving high to the bit// SDA_pin = 1;
SCL_ClrVal(SCL_Ptr);  // giving 0 to the bit//SCL_pin = 0;                           // SCL Low

 WAIT1_Waitus(1);   //Delay_uS(1);
 SCL_SetVal(SCL_Ptr);  // giving high to the bit // SCL_pin = 1;
 WAIT1_Waitus(1);//Delay_uS(1);

 SDA_SetDir(SDA_Ptr, 1); //set as output //SDA_dir = 0;   // define SDA as output
 SDA_ClrVal(SDA_Ptr);   //SDA_pin = 0;                           // SDA low
 WAIT1_Waitus(1); //Delay_uS(1);

 SCL_ClrVal(SCL_Ptr); //SCL_pin = 0;
 WAIT1_Waitus(3);      // Delay_uS(3);
 SCL_SetVal(SCL_Ptr);   //SCL_pin = 1;

 WAIT1_Waitus(1); //Delay_uS(1);
 SDA_SetDir(SDA_Ptr, 0); //SDA_dir = 1;
 WAIT1_Waitus(1);    //Delay_uS(1);
 SCL_ClrVal(SCL_Ptr); //SCL_pin = 0;
}

 

 

unsigned char s_read_byte(unsigned char ack)
{
 unsigned char i=0x80;
 unsigned char val=0;

 //Initial state
 SDA_SetDir(SDA_Ptr, 1);               //release DATA-line
 SDA_SetVal(SDA_Ptr);
 SCL_ClrVal(SCL_Ptr);                // SCL Low

 while(i)                //shift bit for masking
 {
 SCL_SetVal(SCL_Ptr); //clk for SENSI-BUS
 SDA_SetDir(SDA_Ptr, 0); //input mode  added
 WAIT1_Waitus(1);     // Delay_uS(1);
 if (SDA_GetVal(SDA_Ptr) == 1)
 {
 val=(val | i);      //read bit
 }
 SCL_ClrVal(SCL_Ptr);
 WAIT1_Waitus(1); //Delay_uS(1);
 i=(i>>1);
 }

 SDA_SetDir(SDA_Ptr, 1);

 if (ack)
 {
 //in case of "ack==1" pull down DATA-Line
 SDA_ClrVal(SDA_Ptr);
 }
 else
 {
 SDA_SetVal(SDA_Ptr);
 }

 SCL_SetVal(SCL_Ptr); //clk #9 for ack
 WAIT1_Waitus(3);   //Delay_uS(3);
 SCL_ClrVal(SCL_Ptr);
 WAIT1_Waitus(1);   // Delay_uS(1);

 SDA_SetDir(SDA_Ptr, 1);                           //release DATA-line
 SDA_SetVal(SDA_Ptr);
 return (val);
}

 

 

unsigned char s_write_byte(unsigned char value)
{
 unsigned char i=0x80;
 unsigned char error=0;

 SDA_SetDir(SDA_Ptr, 1);

 while(i)
 { //shift bit for masking
 if (i & value)
 {
 SDA_SetVal(SDA_Ptr);    //masking value with i , write to SENSI-BUS
 }
 else
 {
 SDA_ClrVal(SDA_Ptr);
 }

 SCL_SetVal(SCL_Ptr);  //clk for SENSI-BUS
 WAIT1_Waitus(3); //Delay_uS(3);
 SCL_ClrVal(SCL_Ptr);
 WAIT1_Waitus(3); //Delay_uS(3);
 i=(i>>1);
 }

 SDA_SetDir(SDA_Ptr, 1);                           //release DATA-line
 SDA_SetVal(SDA_Ptr);

 SCL_SetVal(SCL_Ptr);                           //clk #9 for ack
 WAIT1_Waitus(3);         //Delay_uS(3);
 SDA_SetDir(SDA_Ptr, 0); //added input mode

 if (SDA_GetVal(SDA_Ptr) == 1) error = 1; //check ack (DATA will be pulled down by SHT11)
 WAIT1_Waitus(1);         //Delay_uS(1);
 SCL_ClrVal(SCL_Ptr);

 return(error); //error=1 in case of no acknowledge
}



unsigned char s_measure(unsigned int *p_value, unsigned char mode)
{
 unsigned char i=0;
 unsigned char msb,lsb;
 unsigned char checksum;

 *p_value=0;
 s_transstart(); //transmission start

 if(mode)
 {
 mode = MEASURE_HUMI;
 }
 else
 {
 mode = MEASURE_TEMP;
 }

 if (s_write_byte(mode)) return(1);
 // normal delays: temp i=70, humi i=20

 SDA_SetDir(SDA_Ptr, 0);  // SDA_dir = 1;

 while(i<240)
 {
 WAIT1_Waitms(1);
 WAIT1_Waitms(1);
 WAIT1_Waitms(1);
 if (SDA_GetVal(SDA_Ptr) == 0)
 {
 i=0;
 break;
 }
 i++;
 }

 // or timeout
 if(i) return(2);

 msb=s_read_byte(ACK); //read the first byte (MSB)
 lsb=s_read_byte(ACK); //read the second byte (LSB)
 checksum=s_read_byte(noACK);                //read checksum (8-bit)

 *p_value=(msb<<8)|(lsb);

 return(0);
}

 


float calc_sth11_temp(unsigned int t)
{
 float t_out;
 t_out =  t*0.01 - 40;
 return t_out;
}

 


float calc_sth11_humi(unsigned int h, int t)
{
 float rh_lin;                      // rh_lin:  Humidity linear
 float rh_true;                   // rh_true: Temperature compensated humidity
 float t_C;                 // t_C   : Temperature [°C]

 t_C=t*0.01 - 40;                    //calc. temperature from ticks to [°C]
 rh_lin=C3*h*h + C2*h + C1;             //calc. humidity from ticks to [%RH]
 rh_true=(t_C-25)*(T1+T2*h)+rh_lin; //calc. temperature compensated humidity

 // now calc. Temperature compensated humidity [%RH]
 // the correct formula is:
 // rh_true=(t/10-25)*(0.01+0.00008*(sensor_val))+rh;
 // sensor_val ~= rh*30
 // we use:
 // rh_true=(t/10-25) * 1/8;

 if(rh_true>100)rh_true=100;               //cut if the value is outside of
 if(rh_true<0.1)rh_true=0.1;               //the physical possible range

 return rh_true;
}

 


void Read_SHT11(float *fT, float *fRH)
{
 unsigned int t;
 unsigned int h;

 float value=0;
 ucSens_Error = 0;

 ucSens_Error = s_measure(&t, 0);
 *fT = calc_sth11_temp(t);
 ucSens_Error = s_measure(&h, 1);
 *fRH = calc_sth11_humi(h, t);
}

 

 


char s_read_statusreg(unsigned char *p_value)
{
 unsigned char checksum = 0;

 s_transstart();                             //transmission start
 if(s_write_byte(STATUS_REG_R)) return 1;    //send command to sensor
 *p_value=s_read_byte(ACK);                  //read status register (8-bit)
 checksum=s_read_byte(noACK);                //read checksum (8-bit)
 return 0;
}

 

 


char s_write_statusreg(unsigned char value)
{
 s_transstart();                             //transmission start
 if(s_write_byte(STATUS_REG_W)) return 1;    //send command to sensor
 if(s_write_byte(value)) return 1;           //send value of status register

 return 0;
}

 

 

void s_connectionreset()
{
 unsigned char i;

//Initial state
 SDA_SetDir(SDA_Ptr, 1);                            //release DATA-line
 SDA_SetVal(SDA_Ptr);
 SCL_ClrVal(SCL_Ptr);                           // SCL Low

 for(i=0; i<9; i++) //9 SCK cycles
 {
 SCL_SetVal(SCL_Ptr);
 WAIT1_Waitus(3);
 SCL_ClrVal(SCL_Ptr);
 WAIT1_Waitus(3);
 }
 s_transstart(); //transmission start
}

 

 

unsigned char s_softreset(void)
{
 s_connectionreset();                         //reset communication
                                               //send RESET-command to sensor
 return (s_write_byte(RESET));                //return=1 in case of no response form the sensor
  }


Explanation of code:

 

The below are the function/driver required for this code:

 

void s_transstart()

unsigned char s_read_byte(unsigned char ack)

unsigned char s_write_byte(unsigned char value)

unsigned char s_measure(unsigned int *p_value, unsigned char mode)

float calc_sth11_temp(unsigned int t)

float calc_sth11_humi(unsigned int h, int t)

void Read_SHT11(float *fT, float *fRH)

char s_read_statusreg(unsigned char *p_value)

char s_write_statusreg(unsigned char value)

void s_connectionreset()

unsigned char s_softreset(void)

 

 

Inside main we are calling the function Read_SHT11() which in turn returns the temperature and humidity values

 

The function “calc_sth11_temp()” will generate the required I2C signals by Bit Banging method i.e it simulates the signal without using the internal resource.

and gives you the temperature value.

 

The function ”calc_sth11_humi()” will generate the necessary I2C signal (Bit Banging) and get the humidity value.

 

For more details on timing signal refer to the SHT11 datasheet:

http://www.sensirion.com/fileadmin/user_upload/customers/sensirion/Dokumente/Humidity/Sensirion_Humidity_SHT1x_Datasheet_V5.pdf

 

 

Now it’s time to build the project, click on the hammer button as shown


image

 

You can see the build is finished successfully with no errors

 

image

 

 

Now it is ready to debug/execute


Now connect the KL46Z board to OPEN SDA port to your computer through USB cable. The hardware setup is as shown below, the click board is connected via click shield

 

image

Click on Debugger configuration as shown below:


image

 

Then select the settings for the current project


image

 

Now click on Apply and Debug


You can see below Debug window screen

image

 

Make sure you have open the corresponding hyperterminal window from your ‘Computer Management’ Device manager window:


In my case it is connected to COM24 port

 

image

 

Now click on green ‘Resume’ button

 

image

 

Open COM24 port from any of the hyper terminal application (putty in my case)

 

image

 

The output seen in the terminal is as shown below:

 

image

 

Happy SHT11 click interfacing  image image image image


I have enclosed the project folder and SREC executable for quick reference.

Attachments:
KL46-sht1x.rar
KL46-sht1x-srec.rar
  • Sign in to reply
  • mcb1
    mcb1 over 11 years ago

    bheemarao

    Bheemarao

    Another very clear and easily followed guide to using these boards.

     

    Thanks

    Mark