Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog Importing project from kinetis SDK2.0: [How to import the existing project from Kinetis SDK and execute using FRDM-K64F ]
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 29 Mar 2016 12:37 PM Date Created
  • Views 1501 views
  • Likes 1 like
  • Comments 1 comment
  • ksdk2.0
  • frdm-k64f
  • kds3.2.0
Related
Recommended

Importing project from kinetis SDK2.0: [How to import the existing project from Kinetis SDK and execute using FRDM-K64F ]

bheemarao
bheemarao
29 Mar 2016

This document shows how to import the existing project of Kinetis SDK v2 using the kinetis Design Studio version: 3.2.0

 

KSDK V2.0

Kinetis SDK v2 is a collection of comprehensive software enablement for NXP Kinetis Microcontrollers that includes system startup, peripheral drivers, USB and connectivity stacks, middleware, and real-time operating system (RTOS) kernels. The Kinetis SDK also includes getting started and API documentation along with usage examples and demo applications designed to simplify and accelerate application development on Kinetis MCUs.

 

Pre-requisite:

1)   KDS3.2.0 installed on your computer

(You can download latest version of KDS from Here or direct download from below link:)

2) Download a Kinetis SDK Package online

Unpack the downloaded archive file to a folder (recommended into c:\nxp (e.g. (c:\nxp\SDK_v2.0-K64F) or into /nxp on other systems)

3)   Install Kinetis SDK v2.0 into Kinetis Design Studio

4)   Finally the  FRDM-K64FFRDM-K64F freedom hardware development board

 

 

Now let us begin to start working on the setup the downloaded SDK v2.0 is having set of example projects to work on Let us see how we can import these projects and execute on our target board i.e  FRDM-K64FFRDM-K64F development board

If we explore the downloaded sdk v2.0 we can find below folders

image

The Kinetis SDK architecture consists of five key components listed below:

 

1. The ARM Cortex Microcontroller Software Interface Standard (CMSIS) CORE compliance device specific header files, SOC Header, and CMSIS math/DSP libraries.

2. Peripheral Drivers

3. Real-time Operating Systems (RTOS)

4. Stacks and Middleware that integrate with the Kinetis SDK

5. Demo Applications based on the Kinetis SDK

 

image

Example projects can be found in folder

“C:\NXP ksdk2.0 workspace\SDK_2.0_FRDM-K64F\boards\frdmk64f”

image

 

Let us examine the demo apps folder in which we can find many projects as shown:

image

We will be executing ecompass example on KDS3.2.0

Open the KDS 3.2.0 and click on File > Import

image

Next select on “Existing Projects into Workspace” as shown below:

image

Navigate to the demo apps existing folder i.e

“C:\NXP ksdk2.0 workspace\SDK_2.0_FRDM-K64F\boards\frdmk64f\demo_apps\ecompass"

image

Click on finish

image

After opening the ecompass project you will see below

 

 

image

The E-Compass demo application demonstrates the use of the FXOS8700 sensor. The tilt-compensated algorithm calculates all three angles (pitch, roll, and yaw or compass heading).

 

Build the project

image

image

 

image

To Run the project click on debug configuration as shown

image

image

After clicking the debug you can see the compilation to debug the project as shown below:

 

 

image

Now establish a serial communication with your computer via com port

Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

 

To know your com port click on device manager: in my case it is com43 port connected to the K64 board

image

Open a serial terminal with the following settings:

    - 115200 baud rate - 8 data bits - No parity - One stop bit - No flow control

 

I am using the application putty with below configuration:

 

 

image

Now click on Resume button on KDS tool:

 

image

image

At starting of execution the project will ask for calibration of the sensors

image

When the demo runs successfully, you can see the information below printed to the terminal.

Note: you must rotate the board 360 degrees to get the max / min value of the magnetic field.

 

image

 

Happy Importing and execution of the project with KSDK2.0...  image image image

  • Sign in to reply
  • clem57
    clem57 over 10 years ago

    Nice to know how to import rather than some other tedious way.

    Thanks,

    Clem