Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Blink Red Led with TPM (Timer PWM Module)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 31 Jul 2015 7:18 AM Date Created
  • Views 604 views
  • Likes 0 likes
  • Comments 0 comments
  • kds+ksdk1.2
  • kds-v3.0.0
  • frdm-kl43z
  • tpm
Related
Recommended

Kinetis Design Studio 3.0 Kinetis SDK 1.2 Processor-Expert using FRDM-KL43Z: Blink Red Led with TPM (Timer PWM Module)

bheemarao
bheemarao
31 Jul 2015

Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This is a project for blinking an RED LED using TPM module of PE implemented using freedom board FRDM-KL43Z.


Requirements

To run successfully this exercise, you need first to download following packages (link enclosed):


- IDE toolchain Kinetis Design Studio (KDS) min v3.0
- microcontroller Library
Kinetis Software Development Kit (KSDK) min 1.2
-
FRDM-KL43Z materials (schematics, Quick Start Package and Sample Code Package)
- latest
P&E Micro windows drivers and SDA Applications

[http://www.pemicro.com/downloads/main_downloads_temp/201507291203137773819/Pemicro_OpenSDA_Debug_MSD_Update_Apps_2015_03_12.zip ]


Before connecting your FRDM-KL43Z for the first time to the USB port of your computer, install the P&E Micro windows driver to ensure a correct detection of the board.


Install first the IDE toolchain KDS and when the installation ended successfully, install the MCU Library KSDK keeping the proposed installation path c:\freescale\kds or ksdk unchanged.

Launch KDS and define your workspace path, then select Help, Install New Software, Add, Archive, C:\Freescale\KSDK_1.2.0\tools\eclipse_update, select KSDK_1.2.0_Eclipse_Update.zip and press Open, OK, select KSDK Eclipse Update, press Next, Accept the Licence Agreement and press Finish. The KSDK libraries are now directly available in the IDE toolchain.


The automated code generator Processor Expert is already included in the IDE Toolchain (available separately as Processor Expert Driver Suite for other IDE toolchains).

 

Tutorial instructions

The tutorial shows how to toggle LED with KSDK 1.2.0 in KDS 3.0 and Processor Expert using a Timer Output for FRDM-KL43Z.

Guide is prepared for red LED which is connected to Timer/PWM Module 0 (TPM0), channel 2 (according to FRDM-KL43Z schematics).

image


Create new project
Create new project in KDS 3.0 with KSDK 1.2.0

image

Type the project name e.g. “FRDM-KL43 toggle using TPM ” choose the board FRDM-KL43Z, mark off options Kinetis SDK and Processor Expert

image

image

image

image

Now, your project structure looks like this in the project explorer and Processor Expert windows:

image


Set Processor Expert Settings

Now, go to Components Library, find fsl_tpm component using filters KSDK 1.2.0 and Applicable to Project and by double click add the component to the Processor Expert Component View of your project.

image

Double click on tpmTmr1:fsl_tpm in Components View and Component Inspector view should open automatically


First turn the Component Inspector view to Classical view by unselecting the Tab View option.

image

Enable to reload the counter on Trigger


Set the counter frequency to 1Hz with a Duty cyle of 50%
Allocate TPM0 Channel 4 to Pin LED2_RED (defined by board selection)


Select Clock source MCGIRCLK and choose the Prescaler Divide by 128
Enable the Initialization of TPM0 Channel 4

image

image

Save the configuration by pressing ctrl+s

Generate the Processor Expert Code for the component tpmTmr1 that we have just configured

image

Build your project by clicking on the hammer button as shown below:

image

Debugging the FRDM-KL43Z board for the first time, you need to define a Debug Configuration by selecting the appropriate option from the toolbar

image

The FRDM-KL43Z embeds a multimode programming and debug interface easily reconfigurable by drag’n droping from the file explorer new SDA applications in Bootloader mode.


For this example, we are going to select the PEMicro OpenSDA Debug mode.
Select the Debugger tab to choose the Interface OpenSDA Embedded Debug - USB Port
You can now start the Debug session!!


image

Launch the configuration

image

You should now see Red LED blink at 1Hz frequency.


image


I will work on dimming the red led from 0-100% (varying the brightness) in my next blog.


I have enclosed the project folder and executables for your quick reference.


image image image image

Attachments:
FRDM-KL43 toggle using TPM.rar
FRDM-KL43 toggle using TPM srec.rar