Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog Kinetis Design Studio 3.0 + Kinetis SDK 1.2 Processor-Expert using FRDM-KL46Z: Blink Red Led with TPM (Timer/PWM Module)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 13 Jul 2015 9:41 AM Date Created
  • Views 1208 views
  • Likes 0 likes
  • Comments 3 comments
  • kds3.0
  • kds+ksdk
  • ksdk1.2.0
  • frdm-kl46z
Related
Recommended

Kinetis Design Studio 3.0 + Kinetis SDK 1.2 Processor-Expert using FRDM-KL46Z: Blink Red Led with TPM (Timer/PWM Module)

bheemarao
bheemarao
13 Jul 2015

Here is a Project created using new KDS version 3.0 and Kinetis software development kit 1.2 on processor expert platform. This is a project for blinking an RED LED using TPM module of PE implemented using freedom board FRDM-KL46Z.


Requirements

To run successfully this exercise, you need first to download following packages (link enclosed):


- IDE toolchain Kinetis Design Studio (KDS) min v3.0
- microcontroller Library Kinetis Software Development Kit (KSDK) min 1.2
- FRDM-KL46Z materials (schematics, Quick Start Package and Sample Code Package)
- latest P&E Micro windows drivers and SDA Applications


Before connecting your FRDM-KL46Z for the first time to the USB port of your computer, install the P&E Micro windows driver to ensure a correct detection of the board.

Install first the IDE toolchain KDS and when the installation ended successfully, install the MCU Library KSDK keeping the proposed installation path c:\freescale\kds or ksdk unchanged.


Launch KDS and define your workspace path, then select Help, Install New Software, Add, Archive, C:\Freescale\KSDK_1.2.0\tools\eclipse_update, select KSDK_1.2.0_Eclipse_Update.zip and press Open, OK, select KSDK Eclipse Update, press Next, Accept the Licence Agreement and press Finish. The KSDK libraries are now directly available in the IDE toolchain.


The automated code generator Processor Expert is already included in the IDE Toolchain (available separately as Processor Expert Driver Suite for other IDE toolchains).

 

Tutorial instructions

The tutorial shows how to toggle LED with KSDK 1.2.0 in KDS 3.0 and Processor Expert using a Timer Output for FRDM-KL46Z.

Guide is prepared for red LED which is connected to Timer/PWM Module 0 (TPM0), channel 2 (according to FRDM-KL46Z schematics).


image


Create new project


Create new project in KDS 3.0 with KSDK 1.2.0

image

Type the project name e.g. frdm-kl46z_red_blinky_tpm, choose the board FRDM-KL46Z, mark off options Kinetis SDK and Processor Expert

image

 

image

image

Now, your project structure looks like this in the project explorer and Processor Expert windows:

image

image

 

Set Processor Expert Settings


Now, go to Components Library, find fsl_tpm component using filters KSDK 1.2.0 and Applicable to Project and by double click add the component to the Processor Expert Component View of your project.


image

Rename the component tpmTmr:fsl_tpm to RedLed.

image

Double click on RedLed:fsl_tpm in Components View and Component Inspector view should open automatically


First turn the Component Inspector view to Classical view by unselecting the Tab View option.

image

Enable to reload the counter on Trigger


Set the counter frequency to 2Hz with a Duty cyle of 50%


Allocate TPM0 Channel 2 to Pin LED2_RED (defined by board selection)


Select Clock source MCGIRCLK and choose the Prescaler Divide by 64


Enable the Initialization of TPM0 Channel 2


image

 

image

image

Save the configuration by pressing ctrl+s
The star beside Component Inspector tab should have disappeared.

image

Generate the Processor Expert Code for the component RedLed that we have just configured

image

Build your project by choosing the right toolbar shortcut

image

 

Debugging the FRDM-KL46Z board for the first time, you need to define a Debug Configuration by selecting the appropriate option from the toolbar


image

The FRDM-KL46Z embeds a multimode programming and debug interface easily reconfigurable by drag’n droping from the file explorer new SDA applications in Bootloader mode.


For this example, we are going to select the PEMicro OpenSDA Debug mode.


Select the Debugger tab to choose the Interface OpenSDA Embedded Debug - USB Port
You can now start the Debug session!!

image

image

Launch the configuration

image


You should now the Red LED blink with a 2Hz frequency


image


Attachments:
KL46-TPM example.rar
KL46-TPM example-srec.srec.zip
  • Sign in to reply

Top Comments

  • bheemarao
    bheemarao over 11 years ago +1
    Hi, I have added project folder and executable SREC file for quick reference. Best Regards Bheema Rao
  • DAB
    DAB over 11 years ago

    I agree, very good detailed post.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bheemarao
    bheemarao over 11 years ago

    Hi,

     

    I have added project folder and executable SREC file for quick reference.

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Nice simple to follow instructions....thanks

    I just need to find the time to sit down with this stuff ...maybe I should throw some boards in my suitcase .....image

     

    Thanks

    Mark