Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog Loading the OpenSDA V2 firmware to K64F board provided from Segger
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 15 Sep 2014 9:40 AM Date Created
  • Views 939 views
  • Likes 0 likes
  • Comments 0 comments
  • k64
  • freedom-board
  • kinetis
  • frdm-k64f
  • kds
  • led-toggling
  • opensda-v2
Related
Recommended

Loading the OpenSDA V2 firmware to K64F board provided from Segger

bheemarao
bheemarao
15 Sep 2014

Loading the OpenSDA V2 firmware to K64F board provided from Segger:

 

By default the board comes loaded with MSD application driver by which you can reprogram the board with available different binaries.

 

The FRDM-K64F platform features OpenSDAv2, the Freescale open-source hardware embedded serial and debug adapter running an open-source bootloader. OpenSDAv2 comes preloaded with the CMSIS-DAP bootloader – an open-source mass storage device (MSD) bootloader and the CMSIS-DAP Interface firmware (aka mbed interface), which provides a MSD flash programming interface, a virtual serial port interface, and a CMSIS-DAP debug protocol interface.


Now since we need to develop a new project and debug / run it on boards, the board should be loaded with different application driver i.e Debug application driver OpenSDA V2 which is supported by Segger, P&E Micro.

OpenSDAv2 is a serial and debug adapter circuit which includes an open-source hardware design, an open-source bootloader, and debug interface software. It bridges serial and debug communications between a USB host and an embedded target processor


There are two alternative firmware files available for the FRDM-K64F (which runs OpenSDAv2)

1. P&E OpenSDAv2 which emulates a P&E OpenSDA/Multilink

2. Segger OpenSDAv2 which emulates a Segger J-Link


To install the firmware:


1.    Go to http://www.segger.com/opensda.html and come down to “Getting started with OpenSDA V2” section and download the firmware scroll to the end of the page with the OpenSDAv2 section and download the firmware.

(The firmware can be downloaded here: Firmware download)


2.    Unpack the content of the zip file (JLink_OpenSDA_V2.bin).


image

3.    Connect the board to the PC via SDA USB while keeping the reset button of the board pressed.                   

image

4.    The board enumerates as BOOTLOADER as shown below:

  image

5.    Copy the file “JLink_OpenSDA_V2.bin” which was extracted earlier and paste this into the BOOTLOADER drive (you can drag and drop too)

 

image

6.    After the file is copied, the green OpenSDAv2 LED will blink faster. Unplug the board and power it again


7.    After power-cycling the hardware, the OpenSDA platform will enumerate as J-Link on the PC.


Now our board is loaded with J-link driver ready for Debug with KDS tool.