Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog New project: miniRobot (Part 1)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yuritikhonov
  • Date Created: 25 Oct 2014 7:48 AM Date Created
  • Views 1412 views
  • Likes 4 likes
  • Comments 11 comments
  • mini_robot
  • python
  • digikey
  • robot
  • frdm-k64f
  • mbed
  • arduino
  • linux
Related
Recommended

New project: miniRobot (Part 1)

yuritikhonov
yuritikhonov
25 Oct 2014

Good day comrades!

Today I want to move aside from tricopter and tell you about one more common project.

image

 

Introduction

 

Not so long ago I was participating in AXP Logic Design Contest and took an honorable place there. I created an ultra-miniature robot that I called "nanoRobot". If you are interested in this project you can read about it in my article.

On the prototyping stage I had to significantly increase the robot’s size. After that I created a new power system, control system and sensors system. As you understand it was an absolutely different robot. I called it "miniRobot" and want to tell about this project in this post.

 

Hardware

 

So what is a miniRobot?

  • 4WD robot chassis with two DC motors.
  • Dual DC Motor Driver (H-bridge type).
  • The heart of the system: Arduino Yun.
  • Echo sensor: HC-SR04.
  • Power supply: 2S LiPo battery.
  • Some little things.

 

My regular readers probably know that I wanted to use Arduino Yun in my tricopter's OSD system (link), But after some reflections I rejected this solution: and the reason was simple: Yun is excessively powerful board for this project. So, look at pictures of my miniRobot:

image

 

Firmware

 

Arduino Yun is a dual processor module and for this board you need two independent software modules: MCU firmware and Linux software.


The first part – MCU firmware responsible for the connection between low level hardware and the core of the system (Linino Linux PC). Low level hardware consits of:

  • DC Motor Drivers;
  • echo Sensor;
  • voltmeter.

 

#include <Bridge.h>
#define trigPin A1
#define echoPin A0
#define volt_Pin A2
#define LM1 10
#define LM2 9
#define RM1 5
#define RM2 6
#define SPEED 64

void setup()
{
  Bridge.begin();
  pinMode(trigPin, OUTPUT);
  pinMode(echoPin, INPUT);
  GoForward(0);
}

void GoForward(char spd)
{
  analogWrite(LM1,spd);
  analogWrite(LM2,0);
  analogWrite(RM1,spd);
  analogWrite(RM2,0);
}

void GoBack(char spd)
{
  analogWrite(LM1,0);
  analogWrite(LM2,spd);
  analogWrite(RM1,0);
  analogWrite(RM2,spd);
}

void TurnRight(char spd)
{
  analogWrite(LM1,spd);
  analogWrite(LM2,0);
  analogWrite(RM1,0);
  analogWrite(RM2,spd);
}

void TurnLeft(char spd)
{

  analogWrite(LM1,0);
  analogWrite(LM2,spd);
  analogWrite(RM1,spd);
  analogWrite(RM2,0);
}

int getEcho(void)
{
  long duration, distance;
  digitalWrite(trigPin,LOW);
  delayMicroseconds(2000);
  digitalWrite(trigPin, HIGH);
  delayMicroseconds(1000);
  digitalWrite(trigPin, LOW);

  duration = pulseIn(echoPin, HIGH);
  distance = (duration/2) / 29.1;

  if (distance > 200) return 200;
  if (distance < 0) return 0;
  return distance;
}

int charToInt(char a, char b, char c)
{
  int ans;
  if (a>'9' || b>'9' || c>'9') return 0;
  if (a<'0' || b<'0' || c<'0') return 0;
  ans = (a - 48)*100 + (b - 48)*10 + (c - 48);
  if (ans > 255) ans = 255;
  return ans;
}

char str[4];
void intToChar(int dat)
{
  int d = dat;

  if (dat<100) str[0] = '0';
  else
  {
    str[0] = d/100 + 48;
    d %= 100;
  }
  if (dat<10) str[1] = '0';
  else
  {
    str[1] = d/10 + 48;
    d %= 10;
  }
  str[2] = d + 48;
}
void loop()
{
  char dat[5], b;
  Bridge.get("COM",dat,4);
  b = toupper(dat[0]);

  int spd = charToInt(dat[1],dat[2],dat[3]);

  if (b == 'F') GoForward(spd);
  if (b == 'B') GoBack(spd);
  if (b == 'R') TurnRight(spd);
  if (b == 'L') TurnLeft(spd);
  if (b == 'N') GoForward(0);

  if (b == 'V')
  {
    intToChar(analogRead(volt_Pin) / 4);
    Bridge.put("DAT",str);
  }
  if (b == 'E')
  {
    intToChar(getEcho());
    Bridge.put("DAT",str);
  }
}

 

The second part – Actually I have a lot of control software, all of them written in my favorite programming language: python (files *.py):

image

 

However in this post I wish to talk only about two of them:

  • remote control software (RC);
  • autonomous control software (AC).

                       

RC-software works in the following way: you are connecting to the robot via SSH (you can use KiTTY for this goal), run the python script and after that you use your keyboard to move the robot. Pretty simple! I made an interesting experiment: I provided access in my LAN to my friend who lives in South Africa. He connects to my WEB-camera and to the SSH terminal of my robot. He was able to control my robot from another point of the planet! After this experiment I know that we live in a world of the future image

image

 

The second program is created for the bypassing the obstacles: if the robot sees the wall in his way it stops then moves back and rotates by ~90 degrees (actually, everything is more complicated, but the essence is not in it), after that the robot goes forward and the cycle repeats. For more info look at this picture with my nanoRobot:

image

 

This is a really funny experiment! Look at this:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the end I realize that my miniRobot is so beautiful that I have not opportunities to hide it in "my little world". As you probably know, I work as a teacher in the university and in this semester I decided to implement this wonderful machine in my work program. For this goal I created a special set of control programs but it is a theme of another article

 

European Freedom Design Contest 2014

 

Everything went on as usual but one day I received a message from eeweb with proposals to participate in the European Freedom Design Contest. No doubt, I should participate and the project, of course, must be miniRobot. But there was one problem: in my project I must use one of Freescale FRDM development board. Carefully reading the documentation, I decided to opt for FRDM K64F. Why for this model? It's very simple! It has pin-to-pin compatibility with Arduino Yun and has a similar functionality, i.e. I only need to unmount my Arduino Yun and mount a new FREM K64F. Pretty simple!

image

But of course we need to start from the schematics. For development of the scheme according to the contest rules I need to use free online scheme editor from DigiKey (link). No sooner said than done!

image

The scheme is pretty simple and I think you'll not have problems with understanding. By the way, it is my first encounter with cloud CAD. By the way this is my first experience with online scheme editor. I was greatly surprised that this editor works even on my Nokia Lumia smartphone!

image

 

I need to found a FRDM board after that I need to fork my Arduino firmware on the new board. But I did the opposite: first of all I wrote the firmware. for this goal according to the contest rules I used another cloud service: mbed.org. I'll be honest - never in my life working with FRDM, I have finished forking just over an hour! This service is worked out so perfectly! I'll not go into technical details, I'll only show the final result:

 

#include "mbed.h"
#include "echo_sensor.h" // echo sensor library

#define LM1_ D3
#define LM2_ D7
#define RM1_ D6
#define RM2_ D5
#define RX_  D0
#define TX_  D1

PwmOut LM1(LM1_); // motors configuration
PwmOut LM2(LM2_);
PwmOut RM1(RM1_);
PwmOut RM2(LM2_);

//Serial link(TX_, RX_);  // bluetooth serial port
Serial link(USBTX, USBRX); // USB serial port

void analogWrite(mbed::PwmOut *prt, char spd) // write to PWM
{
  float a = spd / 2.56; // convert 0..256 to '%'
  *prt = a;
}

void GoForward(char spd)
{
  analogWrite(&LM1,spd);
  analogWrite(&LM2,0);
  analogWrite(&RM1,spd);
  analogWrite(&RM2,0);
}

void GoBack(char spd)
{
  analogWrite(&LM1,0);
  analogWrite(&LM2,spd);
  analogWrite(&RM1,0);
  analogWrite(&RM2,spd);
}

void TurnRight(char spd)
{
  analogWrite(&LM1,spd);
  analogWrite(&LM2,0);
  analogWrite(&RM1,0);
  analogWrite(&RM2,spd);
}

void TurnLeft(char spd)
{

  analogWrite(&LM1,0);
  analogWrite(&LM2,spd);
  analogWrite(&RM1,spd);
  analogWrite(&RM2,0);
}

int charToInt(char a, char b, char c)
{
  int ans;
  if (a>'9' || b>'9' || c>'9') return 0;
  if (a<'0' || b<'0' || c<'0') return 0;
  ans = (a - 48)*100 + (b - 48)*10 + (c - 48);
  if (ans > 255) ans = 255;
  return ans;
}

char str[4];
void intToChar(int dat)
{
  int d = dat;

  if (dat<100) str[0] = '0';
  else
  {
    str[0] = d/100 + 48;
    d %= 100;
  }
  if (dat<10) str[1] = '0';
  else
  {
    str[1] = d/10 + 48;
    d %= 10;
  }
  str[2] = d + 48;
}

char toupper(char ch)
{
  if (ch >= 'a' && ch <= 'z') return ch;
  if (ch >= 'A' && ch <= 'Z') return ch - 'A' + 'a';
  return 0;
}

int main(void)
{
  char dat[5], b, i;
  link.baud(9600);
  initEcho();  // initialize echo sensor
  GoForward(0); // stop all motors

  while (!link.readable());    // we are trying to find a starting byte
  while (link.getc() != 'Z');

  while (true)
  {
    if(link.readable()) // read data from the bluetooth serial port
    {
        for (i=0; i<5; i++)
        dat[i] = link.getc();
    }

    b = toupper(dat[0]);

    int spd = charToInt(dat[1],dat[2],dat[3]);

    if (b == 'F') GoForward(spd); // movements
    if (b == 'B') GoBack(spd);
    if (b == 'R') TurnRight(spd);
    if (b == 'L') TurnLeft(spd);
    if (b == 'N') GoForward(0);

    if (b == 'E') // echo sensor
    {
      intToChar(getEcho());
      link.printf(str);
    }
  }
}

 

In general all is simple: the robot receives the package of data from PC (via USB, RS-232 or Bluetooth), decodes it and after that runs one of procedures:

  • Nxxx – robot stops;
  • Fxxx – robot goes forward at ‘xxx’ speed;
  • Bxxx – robot goes back at ‘xxx’ speed;
  • Lxxx / Rxxx – robot turns left / right at ‘xxx’ speed;
  • Exxx – the robot measures the distance to the obstacle and returns the result to the sender;

 

As you can see, everything is very simple! For normal operation of the program some debugging is needed, but in general I think everything is OK.

 

At the end of the road to the rebuilding of the robot, I was in for an unpleasant surprise: the contest would end in just 2 weeks! And I still did not have a development board. Unfortunately it was impossible to deliver the parcel to Russia for such a short time and I was never able to complete tests of the robot with the new board… However, I am absolutely sure that if I had at hand this board, final debugging of the program would take me a couple of hours and the robot undoubtedly would show a good drive image

 

Unfortunately at this place I have to put a point now. But the project is alive and I will try to please my readers with new articles in near future! Of course, I can't fully describe the miniRobot in one post, so if you have any questions, do not hesitate to ask them! Wish me luck and see you soon!

 

UPD: Good news! FRDM K64F will soon be in my hands, so the project will continue!

  • Sign in to reply
  • yuritikhonov
    yuritikhonov over 10 years ago in reply to e14 Contributor

    1. 2S LiPo - is just an example that I found in junk (voltage of 2S LiPo = 6 ... 8.4v).

    2. you can use any types of battery - the key is a PWM (you can connect 12v battery to 6v motor if your PWM=0..50% and 12v motor if your PWM=0..100%).

    3. current - 2A per motor in my application.

    4. I do not recomend to connect motors in serial. But if it's just for fun - do it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to yuritikhonov

    Thanks Yuri.

     

    Well, I have few more questions regarding the selection of components.

     

    The Voltage Regulator 78L05 you have used in the circuitry has 12V input and 5V output. So is it that you have used 12V battery? But, I think you used 2s Lipo Battery. How much voltage does it give, as which one did you purchase (7.4V/11.1V)? Also, what is its current rating? Apart from that if I connect 2 6v Motors in series in my implementation, would it be fine for the 12V output?

     

    Thanks,

    Gokul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuritikhonov
    yuritikhonov over 10 years ago in reply to e14 Contributor

    1. motor controller on the photo - L298N (you can find datasheet for it on the Internet)

    2. yes I have only 2 motors

    3. output voltage on the motors - 12v

    4. I have not PCB layout

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to yuritikhonov

    Thanks for the timely response Yuri. I did go through the 2nd part as well. I wanted to know how the motor controlling is handled using the driver module. And you had only 2 motors for the bot?? And what was the output voltage to the motor, is it 5v or 12v. Also, it would be really great if you could share the pcb layout for the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuritikhonov
    yuritikhonov over 10 years ago in reply to e14 Contributor

    Hi Gokul! I finished this project a long times ago but you probably did not read the second part: [link]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>