Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog [NEWS] Freescale Kinetis Design Studio v2.0.0 is now available on the web !
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 24 Nov 2014 9:38 AM Date Created
  • Views 880 views
  • Likes 1 like
  • Comments 2 comments
  • compiler
  • freescale
  • free
  • Cortex-M
  • kinetis
  • eclipse
  • kds
  • arm
  • toolchain
Related
Recommended

[NEWS] Freescale Kinetis Design Studio v2.0.0 is now available on the web !

FreescaleTools_and_Software
FreescaleTools_and_Software
24 Nov 2014

Hello Freedom users

 

The new release v2.0.0 of Kinetis Design Studio (KDS) the Freescale 100% FREE toolchain is now available on the web

Simply jump to http://www.freescale.com/kds and select the Downloads tab to get it

 

V2.0.0 is a new full release, supporting Windows 7 and 8 (both 32bit and 64bit) and Linux (64bit binaries for Ubuntu, RHE and CentOS):

 

What's new:

  • Support for 64bit Linux with 64bit binaries.
  • Improved NPW (New Project Wizard) which automatically creates debugger launch configurations for OpenOCD, P&E and Segger.
  • Automatic device filtering in the NPW.
  • Greatly improved Kinetis SDK support with automatically adding compiler include paths for new Kinetis SDK component and files.
  • Updated P&E and Segger debug connections
  • Built-in support for the upcoming Kinetis SDK v1.1 release
  • Updated Processor Expert (V10.4.2)
  • Many bug fixes and other improvements


Details in the Kinetis Design Studio V2.0.0 release notes available in the Documentation Tab


As with the previous V1.1.0 release, you need to download the Kinetis Software Development Kit (KSDK) package to add new device support (library, examples ...)

KSDK is available at http://www.freescale.com/ksdk just move to the Downloads sections to get it

IMPORTANT: To complete KDS and KSDK install, you need to open the SDK Eclipse update (available in KSDK package) from the KDS toolchain using the commands 'Help/Install new software' then 'Add/Archive' and select 'C:\Freescale\KSDK_1.0.0\tools\eclipse_update\SDK_1.0.0-GA_Update_for_Eclipse.zip'.

See the release notes for more details.

 

There is no need to uninstall V1.1.1, as V2.0.0 can be installed in parallel, and projects are compatible. Moving to V2.0.0 is highly recommended for Linux users and anyone using the Kinetis SDK.

 

Thanks for supporting Freescale and its Kinetis ARM Cortex-M MCUs !

  • Sign in to reply

Top Comments

  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 11 years ago in reply to clem57 +1
    Hi Clem Mac support of KDS is scheduled with the next release planed April/May timeframe next year I am also a Mac user, keeping a Bootcamp dualboot Maverick/Windows7 to run software only compatible with…
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 11 years ago in reply to clem57

    Hi Clem

    Mac support of KDS is scheduled with the next release planed April/May timeframe next year

    I am also a Mac user, keeping a Bootcamp dualboot Maverick/Windows7 to run software only compatible with Windows, so be sure that I fully understand your situation

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    That is good news except for Mac users since no support! Any chance in near future? Thanks