• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Forum Freescale Freedom Development Platform (Questions and Answers)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 9 subscribers
  • Views 6899 views
  • Users 0 members are here
  • 32bit
  • low_power
  • cortex-m0+
  • freescale
  • freedom_board
  • Cortex-M
  • microcontrollers
  • kinetis
  • arm_cortex_m
  • cortex
  • arm_cortex
  • kinetis-l
  • microcontroller
  • mcu
  • cortex-m0
  • arm
  • arduino
  • freedom
Related

Freescale Freedom Development Platform (Questions and Answers)

FreescaleTools_and_Software
FreescaleTools_and_Software over 13 years ago

Hello FRDM-KL25Z buyer

 

You are already thousands of customers who ordered this board.

In order to make your life easier, with a single place where to find relevant informations concerning this tool, I will try to collect in this post the answered questions concerning FRDM-KL25Z, found in different places like Freescale community, groups from Element14 Community or anywhere on the web ...

 

I will publish regularly (in the document section from this group) some very instructive tutorials produced by my colleague Erich Styger, which should help you to take in hand FRDM-KL25Z and its software tools (Codewarrior 10.3beta, Processor Expert ...).

 

Don't hesitate to post here your new questions that we can answer it and share it with the community.


  • Sign in to reply
  • Cancel
Parents
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 13 years ago

    QUESTION

    You need to use the Freescale FRDM-KL25Z Freedom Board to run a small robot project.

    You need 2 PWM channels to run 2 motors, 2 to 3 channels to send 10 us trigger pulse for Ultrasonic sensors and 3 to 5 channels to capture the return pulses from Ultrasonic sensors.

    You are  having trouble setting up the timer module TPM2  on Codewarrior 10.3 to have 2 PWM channels with 4kHz to control the duty cycle of the motors ( L293D)

    How to get the right set-up for the timer ?

     


    ANSWER

    If you are using different channels from the same TPM and you want 4 kHz in both, use the same Timer Unit in channel 0 and channel 1.

    The TimerUnit component uses different channel for your configuration, you can see this in the image.


    imageimageTU1.JPG

     

      

    This configure the same frequency of 4kHz in channel 0 and channel 1 but you can set the duty cycle for each channel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 13 years ago

    QUESTION

    You need to use the Freescale FRDM-KL25Z Freedom Board to run a small robot project.

    You need 2 PWM channels to run 2 motors, 2 to 3 channels to send 10 us trigger pulse for Ultrasonic sensors and 3 to 5 channels to capture the return pulses from Ultrasonic sensors.

    You are  having trouble setting up the timer module TPM2  on Codewarrior 10.3 to have 2 PWM channels with 4kHz to control the duty cycle of the motors ( L293D)

    How to get the right set-up for the timer ?

     


    ANSWER

    If you are using different channels from the same TPM and you want 4 kHz in both, use the same Timer Unit in channel 0 and channel 1.

    The TimerUnit component uses different channel for your configuration, you can see this in the image.


    imageimageTU1.JPG

     

      

    This configure the same frequency of 4kHz in channel 0 and channel 1 but you can set the duty cycle for each channel.