Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Forum How to use Arduino's datalogger Shields along with FRDM-KL25Z Board?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 6 subscribers
  • Views 694 views
  • Users 0 members are here
Related

How to use Arduino's datalogger Shields along with FRDM-KL25Z Board?

bheemarao
bheemarao over 13 years ago

Need to know whether Arduino's shield be used along with freedom board, if so how it can be explored to interface Arduino's datalogger shield.

  • Sign in to reply
  • Cancel
Parents
  • bheemarao
    bheemarao over 13 years ago

    I got to know Freedom FRDM-KL25Z board supports Arduino platform ecosystem with Arduino compatible headers.

     

    Arduino Data-Logger Shield can be interfaced to Freedom board. Datalogger board features an SD card with level shifter (required to work with 3.3V and 5V devices), two LED’s, a reset button, an I2C battery buffered realtime clock plus a prototype area. The minimal SD card pins (MISO, MOSI, DeviceSelect, BusCock) and I2C (SDA, SCL) bus are connected to the shield connector rows, while the two LEDs and the card write protect and card detect pins can be routed to any pins with a wire or any other kind of connection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bheemarao
    bheemarao over 13 years ago

    I got to know Freedom FRDM-KL25Z board supports Arduino platform ecosystem with Arduino compatible headers.

     

    Arduino Data-Logger Shield can be interfaced to Freedom board. Datalogger board features an SD card with level shifter (required to work with 3.3V and 5V devices), two LED’s, a reset button, an I2C battery buffered realtime clock plus a prototype area. The minimal SD card pins (MISO, MOSI, DeviceSelect, BusCock) and I2C (SDA, SCL) bus are connected to the shield connector rows, while the two LEDs and the card write protect and card detect pins can be routed to any pins with a wire or any other kind of connection.