• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Codewarrior Trick & Tips : Migrating Kinetis-L Projects from Beta to final version MCU 10.3
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 4 Jan 2013 2:00 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:23 AM
  • Views 1067 views
  • Likes 1 like
  • Comments 0 comments
Related
Recommended

Codewarrior Trick & Tips : Migrating Kinetis-L Projects from Beta to final version MCU 10.3

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

 

Fullscreen contentimage_22326.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>
Fullscreen contentimage_22327.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

 

I have successfully used CodeWarrior for MCU10.3 beta version for many projects. With the advent of the final CodeWarrior for MCU10.3, I want to migrate my existing projects to the new and final version. First: my existing projects work as well in the final version, which is good news. But there are two things to change to take advantage of the final 10.3:

 

  1. Linker file memory split
  2. ARM Micro Trace Buffer (MTB) support

 

 

Linker File Memory Split at 0×2000’0000

 

In the beta version, linker files for Kinetis L family had a memory split at address 0×2000’0000:

 

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000000C0

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001FBF0

  m_data_1FFFF000 (RW) : ORIGIN = 0x1FFFF000, LENGTH = 0x00001000

  m_data      (RW) : ORIGIN = 0x20000000, LENGTH = 0x00003000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

 

 

In the above linker file, the whole SRAM is splitted into m_data and m_data_1FFFF000. Such a memory split is required for the Kinetis K family (e.g. K60), as different memory controllers are used for each area. As such, linker objects shall not cross that boundary at 0×2000’0000.

 

However, the L family implements things differently, and such a split is not necessary any more. Keeping that split is not a big issue at first hand. But if I want to use the whole SRAM memory, having such an unneeded split is complicating things. New projects created with MCU10.3 do not have that split any more. So I want to apply this to my existing projects too.

  

:idea: Such an ‘unsplitted’ memory map is as well needed for the MTB (Micro Trace Buffer) feature presented later in this post.

  

To migrate existing Processor Expert projects to the simplified memory map, I select the CPU component. In the Build Options tab I choose ‘Click to set default’ to apply the new memory map:

 

Fullscreen contentimage_22328.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Click to set default

 

 

 

Actually, it means clicking into the field and then click on the ‘…’ button:

 

:idea: Clicking into the property field first to show the ‘…’ button is a problem of the UI.

  

 

Fullscreen contentimage_22329.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Click button to set default

 

 

 

This triggers a confirmation dialog:

 

Fullscreen contentimage_22330.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Do you really want to set all areas to the default

 

 

 

After confirming that, my memory areas get reduced, and after code generation my linker file gets simplified too:

 

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000000C0

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001FBF0

  m_data      (RW) : ORIGIN = 0x1FFFF000, LENGTH = 0x00004000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

 

 

Now my SRAM is in one nice and large memory area. And this will hep me with the Micro Trace Buffer support, which is the next topic.

 

 

Micro Trace Buffer in Linker File

 

The other change is that Processor Expert adds the following to support the Micro Trace Buffer:

 

/* reserve MTB memory at the beginning of m_data */

.mtb : /* MTB buffer address as defined by the hardware */

{

  . = ALIGN(8);

  _mtb_start = .;

  KEEP(*(.mtb_buf)) /* need to KEEP Micro Trace Buffer as not referenced by application */

  . = ALIGN(8);

  _mtb_end = .;

} > m_data

 

 

:idea: The KEEP GNU gcc linker directive is needed to avoid that the linker dead-strips that buffer from my application. Usually the linker will remove any variables which are not used. That trace buffer is not used by the application, but it is used by the trace feature in the debugger. As such, the KEEP directive tells the linker to keep it. Don’t worry that it will occupy SRAM if not used: if not used, that buffer size will be zero (more on this below). 

 

Recreating the linker file with Processor Expert adds the above section. If I have switched off linker file creation, then I should add the above part to my linker file. More about why such an entry is needed in the next paragraph…

 

 

Micro Trace Buffer Support

 

One of the greatest added features in MCU10.3 is the ability to trace my application with a MTB (Micro Trace Buffer). For this there is a setting in the Debug/Launch configuration:

 

Fullscreen contentimage_22331.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Enable Trace And Profile

  

  

In order to have this functionality working, it needs a software buffer in RAM. That’s what has been added as .mtb in the linker file (see above). Projects created with MCU10.3 add that trace buffer to the sources:

 

 

Fullscreen contentimage_22332.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

sa_mtb.c in project

  

  

  

To enable trace support for 10.3 beta project, that file has to be added. This can be done with creating a new project with 10.3 and then copy that file over, or simply create a new file sa_mtb.c with following content:

 

/*

02 * sa_mtb.c

03 *

04 * Contains the definition of the buffer used for allocating SRAM space for the MTB trace.

05 */

06 

07 #if (defined(__SA_MTB_SIZE) && (__SA_MTB_SIZE > 0))

08 /*

09 * MTB (Micro Trace Buffer) is using its own section name, which is used in the linker script.

10 */

11 

12 #define SA_MTB_ALIGNEMENT 64 /* alignment of the MTB buffer */

13 

14 unsigned char __attribute__((section (".mtb_buf"))) mtb_buf[__SA_MTB_SIZE] __attribute__ ((aligned (SA_MTB_ALIGNEMENT)));

15 

16 #endif /* __SA_MTB_SIZE */

 

 

If I enable trace, then it will tell me to rebuild my project:

 

 

Fullscreen contentimage_22333.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Trace Enabled. Please rebuild the project

 

 

 

The reason is, it has set a define in the compiler setting with the trace buffer size:

 

Fullscreen contentimage_22334.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

__SA_MTB_SIZE defined in the GCC Preprocessor Settings

 

 

 

:idea: NOTE: If I enable trace through Project Properties > Run/Debug Settings, then the compiler define does not get properly set. But it works if I do it through the menu Run > Debug Configurations.

 

 

Summary

 

To take advantage of MCU10.3, two simple things are needed for my beta projects: Resetting the linker memory map and to add the sa_mtb.c file to my project. With this I have the advantage of a simpler memory map, plus I can use the hardware trace functionality. How to use the MTB will be a topic in one of my next posts.

 

:idea:  The Freedom FRDM-KL25Z projects I have made available here are already migrated.

 

Happy migrating :-)

  • freescale
  • kinetis
  • migrating
  • frdm
  • codewarrior
  • frdm-kl25z
  • migration
  • beta
  • kinetis-l
  • freedom