• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Codewarrior Tutorial for FRDM-KL25Z & ARDUINO : Freescale Freedom Zumo Robot
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Mar 2013 3:15 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:26 AM
  • Views 1015 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Codewarrior Tutorial for FRDM-KL25Z & ARDUINO : Freescale Freedom Zumo Robot

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

image image

    

 

The cool thing with the Freedom board is: there are many exciting Arduino boards out there which want to be used with the FRDM-KL25Z. I have spent most of my last week-end with creating a little black beauty:

    

 

 

FRDM Zumo Robot

FRDM Zumo Robot

 

 

 

   

   

When I was looking for some nice DC motors with quadrature encoders for my next lecture project, I stumbled over the Pololu web site which had *exactly* the DC motors I was looking for. And their Zumo Robot Robot Kit was something which attracted my eyes.

 

 

   

   

I always joked :roll: about women shopping habits. But my wife is right: If it is about electronics, I’m not different at all :grin:

 

 

   

   

That robot is smaller than 10 cm on each size, so it qualifies as a Mini-Sumo. Although I have a different purpose in mind for my robot…..

   

   

 

 

Chassis and Motors

 

   

I ordered the chassis with two 75:1 Micro High Performance Metal Gearmotors which enable the chassis to move about 50 cm in a second. The chassis includes a battery compartement on the bottom for 4 AA batteries (so up to 6V):

   

 

 

Zumo Chassis with DC Motors

Zumo Chassis with DC Motors

 

 

   

   

:idea: I did *not* follow the Pololu instructions to solder the motor with the Arduino shield: instead I used flexible wires to attach the motors to the board. That allows me to change motors or disassemble the kit in a much simpler way.

   

   

 

 

Arduino Board

 

   

The Arduino board comes with a few parts unpopulated (Buzzer, Headers, Switches). The board features a tiny (but powerful) Dual Full-H Bridge, a Buzzer, Battery Voltage Sensing and a I2C Accelerometer+Magnetometer sensor:

     

 

 

Zumo Arduino Board

Zumo Arduino Board

 

 

   

   

Freedom Board

 

   

The FRDM-KL25Z needs to connected ‘face down’ to the Zumo board. I plan to layout an intermediate PCB with my to-be-added hardware. But for now I’m using normal breakable header rows as ‘interconnection’. This is necessary as otherwise the Freedom board is very close to the Zumo board components:

 

 

   

Headers to increase distance between boards

Headers to increase distance between boards

 

 

    

   

Power Supply

 

   

The FRDM-KL25Z is powered from the batteries through P5-9V_IN. But: the Freedom board only generates the 3.3V from P5-9V_IN, and but not the needed 5V to the header (see this post). That 5V is needed by the Shield. So for now I’m using a rather bulky DC-DC converter and supply the needed 5V from the battery to the USB 5V supply line, until I can replace the DC-DC converter with a smaller one. At least everything is working now :-) .

   

   

 

 

Software, and Next Steps

 

   

The software in CodeWarrior with Processor Expert is ready for most parts. Motors (speed/direction), LED’s and Buzzer are working. Magnetometer/Accelerometer and Battery Voltage Sensing are in progress. The current software was attached to this docuement but I would recommend to download the updated version on GitHub with all the Processor Expert components. And: I have a Bluetooth module ready to integrate, plus I want to add a line scanning module too. So enough fun for a couple of dark nights and week-ends :-) .

   

 

 

FRDM Zumo backside

FRDM Zumo backside

 

 

   

   

Happy Zumoing :-)

Attachments:
Freedom_Zumo.zip
  • tutorial
  • avr
  • microchip
  • hardware
  • cortex-m0+
  • sports_technology
  • freescale
  • robots
  • Cortex-M
  • kinetis
  • robot
  • cortex
  • embedded
  • frdm-kl25z
  • stm32
  • Design
  • kinetis-l
  • prototyping
  • platform
  • cortex-m0
  • arduino_development_environment
  • arm
  • arduino
  • freedom
  • pic
  • atmel