• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Codewarrior Tutorial for FRDM-KL25Z & ARDUINO: Zumo Line Following with Freescale Freedom Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Mar 2013 3:38 PM Date Created
  • Last Updated Last Updated: 12 Mar 2013 6:24 PM
  • Views 801 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Codewarrior Tutorial for FRDM-KL25Z & ARDUINO: Zumo Line Following with Freescale Freedom Board

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

image image

   

 

 

With the Zumo I have a base platform for cool robotics applications. So why not build a line following robot with this? Especially as Pololu offers a reflectance sensor array for it. The result is: I have a line following robot :-)

  

 

 

Line Following ZumoBot

Line Following ZumoBot

 

 

  

  

It turned out that things were not working out of the box with the FRDM-KL25ZFRDM-KL25Z board. So if you want to do the same thing, here are some tips how to make it working with the Freedom board.

    

   

 

 

 

5V Power for the Shield

 

   

The Freedom board does not generate 5V from the V_IN (Battery) supply voltage. The Zumo Arduino shield expects the 5V generated from the Arduino microcontroller board. To overcome this limitation, I’m using a tiny S7V7F5 DC-DC step up/down voltage converter which generates 5V from 2.7..11.8V. I have it soldered on a 3 pin header and placed it on the Zumo shield:

  

 

 

Voltage Converter

Voltage Converter

 

 

  

  

On the backside, I have the DC-DC converter connected to GND and V_IN on the shield headers, and wired the 5V output to the 5V pin:

   

 

DC-DC Converter Connection  Backside

DC-DC Converter Connection Backside

  

  

Reflectance Sensor Array Supply

 

  

The Reflectance Sensor Array is using 5V logic levels by default, as designed to work with 5V Arduino (or compatible) boards. While that works with 5V tolerant input pins, it is not ideal from a timing perspective to use it with 3.3V logic levels (charging and discharging the sensor capacitors). So I changed the supply voltage to 3.3V which is the logic level for the Freedom board. Unfortunately the sensor array connector does not offer a 3.3V option, so I have cut the 5V pin and wired it to the 3.3V on the shield:

  

 

 

3.3V Sensor Array Connection

3.3V Sensor Array Connection

   

  

 

 

3.3V Power Connection for Reflectance Array

3.3V Power Connection for Reflectance Array

  

  

 

 

:idea: Pololu offers another sensor array which is designed for both 3.3V and 5V which could be used with the Zumo.

  

  

 

 

D4 and Kinetis NMI

 

  

The other issue with the original Pololu sensor module is that the leftmost sensor is connected to the Arduino shield data 4 (D4) pin. Unfortunately this pin is connected to the NMI (Non-Maskable Interrrupt) of the Kinetis Cortex-M4 on the Freedom Board. That way it happens that it creates an NMI interrupt.

 

  

:idea: It is possible to disable the NMI functionality of that pin for the KL25Z. However, depending on the sensor state during startup/power-on of the microcontroller, this still very likely will raise an NMI, especially right after flashing/debugging the device. The problem can be avoided if debugging is done without powering the sensor array. That means that the battery supply voltage needs to be switched off during flashing and startup of the microcontroller. This worked for me, but was painful after a while.

 

  

The solution is to re-route the D4 sensor to another pin. For this a trace on the sensor board needs to be cut, and rerouted to another pin. I used A0 as this pin is available on the connector and I have not used it otherwise:

  

 

 

D4 Sensor Rerouting to A0

D4 Sensor Rerouting to A0

  

  

 

 

Software

 

  

The software is written with the help of Processor Expert components. It runs FreeRTOS as operating system:

   

 

 

Processor Expert Components

Processor Expert Components

  

   

 

 

It features a command line (shell) interface using the OpenSDA USB CDC connection:

  

 

 

Shell Commands

Shell Commands

  

  

 

 

The shell commands are manually control the motors, perform calibration of the sensors or inspect the state of the system:

  

 

 

System Status in Shell

System Status in Shell

  

  

 

 

ZumoBot in Action

 

   

The following video shows the ZumoBot following a line. After power-up, the sensors get calibrated with moving the sensors over the line, while the sounder is on. Another press of the button runs the line following (PD control loop) algorithm. If the robot does not detect a line any more, it stops:

 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

   

The current software was attached to this document but I would recommend to download the updated version on GitHub with all the Processor Expert components.

  

 

Happy Line Following :-)

Attachments:
1541.Freedom_Zumo.zip
  • avr
  • microchip
  • zumo
  • cortex-m0+
  • kl25
  • freescale
  • Cortex-M
  • kinetis
  • robot
  • cortex
  • stm32
  • kinetis-l
  • line_following
  • microcontroller
  • cortex-m0
  • nxp
  • st
  • arm
  • arduino
  • freedom
  • pic
  • atmel
  • lpc