Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Codewarrior Tutorial for FRDM-K20D50M : USB CDC driver
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 14 Jun 2013 7:32 AM Date Created
  • Last Updated Last Updated: 14 Jun 2013 8:01 AM
  • Views 1055 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Codewarrior Tutorial for FRDM-K20D50M : USB CDC driver

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

image image

   

   

Good news for everyone owning the FRDM-K20D50MFRDM-K20D50M board: I have extended the FSL_USB_Stack with USB CDC device class support for the K20D50M :-) .

     

USB CDC Test Application with the FRDM-K20D50M 

USB CDC Test Application with the FRDM-K20D50M

  

 

Demo Application

  

The demo projects is made with Processor Expert components so it can be easily copied or ported to another board:

    

FRDM-K20D50M USB CDC Application Components 

FRDM-K20D50M USB CDC Application Components

 

I have created a demo application which echoes the entered text back on the console, with incrementing a counter:

   

USB CDC Test Application with the FRDM-K20D50M 

USB CDC Test Application with the FRDM-K20D50M

    

FSL_USB_Stack with FSL_USB_CDC_Device

With just two additional Processor Expert components, it is possible to add USB CDC functionality to an existing projects in just a few minutes. See “USB Component Splitted and Updated” for architectural information. The component has now added a Kinetis K20D50 option:

   

Kinetis K20D50 in FSL_USB_CDC_Device Component 

Kinetis K20D50 in FSL_USB_CDC_Device Component

 

 

:idea:  The FSL_USB_CDC_Device component features now an optional timeout feature. With this, it is easer to use the component in a bare-metal environment. It is using the extra ‘Timeout’ component which implements a timer based timeout to avoid stalling of the stack.
    

  

USB Clock Configuration

 

The most difficult part is the clock configuration. The USB block needs a 48 MHz clock to sample the 24 MHz USB signal. In the CPU component properties, I configured the System oscillator 0 to use the external 8 MHz crystal in Low power mode:

  

System Oscillator Settings 

System Oscillator Settings

 

The MCG Is set to PEE and 48 MHz PLL output clock:

     

MCG Settings 

MCG Settings

   

:!: It should be possible to use a 96 MHz PLL clock and then divide it down in the USB peripheral to a clock of 48 MHz. This is what I did first, and lost a lot of time, because this did not work :-( . I have not investigated it further, but this is either a bug in the silicon or in Processor Expert? 48 MHz without prescaler in the USB worked.

 

     

Derived from this, the system clocks are set up like this:

   

System Clock Settings 

System Clock Settings

 

In the Init_USB_OTG, the clock gate has to be enabled and the PLL/FLL clock to be used with 48 MHz:

  

USB Init_USB_OTG Settings 

USB Init_USB_OTG Settings

 

:!: From the settings it would be possible to use a 96 MHz PLL clock and then to scale it down ot 48 MHz. However, with this my device did *not* enumerate :-(

  

That’s it! The rest is just writing a small test application.

 

Sources

The above project/sources and last Processor Expert Components are attached to this post. The same repostitory hosts the updated FSL_USB_Stack and FSL_USB_CDC_Device Processor Expert components.

Happy CDCing :-)

Attachments:
ProcessorExpert_Beans.zip
FRDM-K20D50M.zip
  • cortex-m4
  • freescale
  • freedom_board
  • cdc
  • cortex-m3
  • Cortex-M
  • frdm-k20d50m
  • usb
  • codewarrior
  • microcontroller
  • development_board
  • arm
  • arduino
  • freedom
  • low-cost
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • bheemarao
    bheemarao over 9 years ago in reply to lorean

    Hi Dominique,

     

    Can i know which version of dev tool you are using i.e processor expert/KDS

    i checked on kds3.2 version below are the snap shot which shows controller K20D50 can be selected:

    image

    and

    image

    have a look on below links regarding USB CDC:

    https://community.nxp.com/thread/380656

    try downloading the components Download Components 2016-12-12.zip (9.1 MB) from below link:

    https://sourceforge.net/projects/mcuoneclipse/files/PEx%20Components/

     

    Best regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lorean
    lorean over 9 years ago

    sorry, i've already download the FSL_USB_CDC_Device but it doesnt give the option for cpu k20d50m. where can i get it?