• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Review for FRDM-KL25Z rev E and Modify it to Generate 5V from V_IN
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Aug 2013 12:39 PM Date Created
  • Last Updated Last Updated: 8 Aug 2013 1:24 PM
  • Views 1276 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Review for FRDM-KL25Z rev E and Modify it to Generate 5V from V_IN

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

imageimage

  

 

About a year ago I started to use the FRDM-KL25Z board (RevD).
Finally, I had it in my hands: the RevE board :-)
Using the RevD board, I faced several problems:

  1. 3.3V supply voltage drop because of low-cost diode D1
  2. Hard to use USB host mode, as no 5V supplied to the USB bus
  3. No 5V generated from V_IN

The good news: all of them have been improved :-) in the FRDM-KL25Z RevE Schematics:

  
FRDM-KL25Z RevE Board

FRDM-KL25Z RevE Board
 
 

 

Board Frontside

 
The picture below shows the most important changes:
  

FRDM-KL25Z RevE Changes

FRDM-KL25Z RevE Changes
 
  

Board Power Supply

 
There are changes to the board with respect of power supply. The 3.3V power supply voltage drop has been fixed with better diodes with less voltage drop. Additionally the board has header J20 to bypass the voltage drop over D12:
  

J20 header to bypass D12 (Source: Freescale KL25Z RevE Schematics)

J20 header to bypass D12 (Source: Freescale KL25Z RevE Schematics)
 
 

J20 on FRDM-KL25Z RevE

J20 on FRDM-KL25Z RevE
 
 

Nearby J20 there is as well the unpopulated D7: before this diode was part of D1 on RevD. With this diode unpopulated, using the batter connector on the backside of the board requires this footprint populated (either with diode or 0-Ohm resistor).
 
 

5V Voltage Converter

 
As the RevD is not able to generate 5V to the Arduino header (pin 10 on J9), this makes it difficult to use it with any Arduino shield which needs to be supplied with 5V e.g. from the battery voltage. So far I have added a 5V regulator as the Pololu (seee ’5V Power for the Shield’ in this post). Another way is to solder a 5V (e.g. Pololu tiny S7V7F5) converter to the Ardunino shield as shown in this post):
 

5V Voltage Converter

5V Voltage Converter
 
  

Now the board has a 3 pin header (J22) on the board so such a converter (or a 3 pin ) can be soldered.

 
J22 Schematic (Source: Freescale FRDM-KL25Z RevE Schematic)

J22 Schematic (Source: Freescale FRDM-KL25Z RevE Schematic)
 
 

Additionally there is space for 3 10 uC capacitors (C26, C27, C28). Alternatively a 7805 in a TO-220 package can be used as low-cost alternative.

  

J22 for a 5V converter

J22 for a 5V converter
 
 

USB Host 5V Voltage

 
For USB host mode, the board needs to supply 5V to the bus. So far I had to use a wire (see this post). Now the board has a header J21 and resistor R82 option:
   

J21 with R82 on FRDM-KL25Z RevE

J21 with R82 on FRDM-KL25Z RevE (Source: Freescale KL25Z RevE Schematics)

   

With J21 I can supply 5V to the bus, and with R82 I can pull down the USB ID pin.
 

J21 Near KL25Z

J21 Near KL25Z
 
 

R82 near USB Connector

R82 near USB Connector
  
 

:!: The 5V are *not* protected against over-current. So I need to make sure I do not draw too much current.

 

  
Board Backside
 
The backside of the board has the RevE sticker. The pads for J6 and J8 are a bit smaller now to make it easier to solder a SWD 10pin debug connector. Additionally the wrong pin name writing has been fixed:
 

FRDM-KL25Z RevE Board Backside

FRDM-KL25Z RevE Board Backside
  
   

The new RevE fixes many limitations of the RevD board, and makes it easier to be used either in USB Host mode or with Arduino shields. Until then I’ll use my patched boards, but I’ll start using the new RevE boards in my courses as soon as I run out with the RevD boards.
 

 
Modify your FRDM-KL25Z revE to Generate 5V from V_IN   

  
The
Freescale Freedom boards like the FRDM-KL25ZFRDM-KL25Z feature an Arduino header so I can stack shields on it. Unfortunately, the Freedom board does not generate 5V if not connected to the USB cable. This makes it not possible to be used with many shields like the Adafruit Motor Shield: such shields expect that the Arduino board is providing 5V through the Arduino header (Pin 10 on J9 on the FRDM-KL25Z). So I had to do hardware changes to generate that 5V if I used my board disconnected from USB, e.g. running from batteries through V_IN (pin16 (P5-9V_IN) on the FRDM-KL25Z.

  

  

J22 with Capacitors on FRDM-KL25Z RevE

J22 with Capacitors on FRDM-KL25Z RevE

   

 

The good news is that the Rev.E of the Freedom FRDM-KL25Z board has now a header J22 to make things easier:

 

 

 

FRDM-KL25Z Schematic

 

This header can be populated to generate the needed 5V from V_IN:

 

J22 Schematic (Source: Freescale FRDM-KL25Z RevE Schematic)

J22 Schematic (Source: Freescale FRDM-KL25Z RevE Schematic)

  

 

:?: The schematic/board provides footprints for several capacitors to counter LC voltage spikes. As I’m using low loads with short cables, I probably do not need them. Have a look at this Pololu article on this subject.

  

Pololu 5V Converter

  

Pololu sells a the “Pololu 5V Step-Up/Step-Down Voltage Regulator S7V7F5” 5V Buck Converter (Part number 2119) which generates 5V from an input voltage between 2.7V and 11.8V. This makes it ideal to generate the 5V from batteries.

 

The tiny 9×12 mm module has three normal 2.54 mm pins for VIN, GND and VOUT (5V):

 

S7V7F5 Back Side

S7V7F5 Back Side

  

 

S7V7F5 Front Side

S7V7F5 Front Side

  

  

Soldering the Headers to the Module

  

Pololu ships the module with two different headers (straight and right-angle male headers). I used the straight one:

 

Straight Header Soldered on Module

Straight Header Soldered on Module

 

 

Top side with straight header soldered

Top side with straight header soldered

 

 

Mounting on FRDM-KL25Z

  

Then the converter gets soldered on the FRDM-KL25Z:

  

Module Soldered on FRDM-KL25Z

Module Soldered on FRDM-KL25Z

 

 

:idea: I intentionally used the header in the above way (with the 3 pins going above the module: that way I have more test or connection points on the board. Of course otherwise it would make sense to cut the pins. Cutting the pins is advised if they could get in contact with components on a shield above the converter.

  

Summary

As the FRDM boards to not generate the needed 5V from V_IN as needed by many shields, I need to add a buck converter or similar power source to have 5V on the Arduino header. The FRDM-KL25Z RevE board makes it easier to add such a thing like a Pololu 5V Step-Up/Step-Down converter. That converter costs less than $5.

  

Happy Powering :-)

  • 32bit
  • cortex-m0+
  • freescale
  • freedom_board
  • Cortex-M
  • kinetis
  • usb
  • frdm-kl25z
  • kinetis-l
  • microcontroller
  • mcu
  • cortex-m0
  • arduino
  • 5v
  • freedom