Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents [FRDM-K64F - PE - Eclipse] Project: Create a Data Logger
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 15 Jul 2014 5:07 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:52 AM
  • Views 1023 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

[FRDM-K64F - PE - Eclipse] Project: Create a Data Logger

“This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.”


The Freescale FRDM-K64F is a great board for data logger applications: it has a powerful ARM Cortex M4F with 120 MHz, 1 MB Flash and 256 KByte RAM. Best of all: it already has a micro SD card socket on the board image


Data Logger with FRDM-K64F

Data Logger with FRDM-K64F

 

Outline

In “Arduino Data-Logger Shield with the FRDM-KL25Z Board” I already used the FRDM-KL25Z with the Arduino Data-Logger shield with CodeWarrior. Basically the same can be applied to the FRDM-K64F. I moved to Eclipse Kepler (see “Constructing a Classroom IDE with Eclipse for ARM“), so here is an updated tutorial: how to create a data logger application with the FRDM-K64F and Eclipse Kepler.

You need:

  1. Eclipse Kepler with Processor Expert as outlined in “Constructing a Classroom IDE with Eclipse for ARM“
  2. Freescale FRDM-K64F board with USB cable
  3. A micro SD card
image: This tutorial can be used with CodeWarrior for MCU10.x, Processor Expert Driver Suite or Kinetis Design Studio too. The principle is the same, but the project creation steps will be somewhat different.


Make sure you have loaded the latest Processor Expert components from GitHub (see “Processor Expert Component *.PEupd Files on GitHub“).The project created in this tutorial is available on GitHub:https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/Eclipse/FRDM-K64F/FRDM-K64F120M/FRDM-K64F_DataLogger.In principle, this tutorial can be applied to any other board: Just make sure you select the microcontroller on your board, and adopt the pin settings for the devices you have.While it would make sense to use an RTOS like FreeRTOS for a data logger, I’m showing here a ‘bare metal’ data logger. An RTOS with tasks then can be easily added to the project.

Creating the Project

image: The steps below are for standard DIY Eclipse Kepler IDE and GNU ARM Eclipse. If you are using Kinetis Design Studio (KDS), then use the File > New > Kinetis Design Studio menu. If using CodeWarrior for MCU10.6, then use the File > New > Bareboard project. Note that the wizard pages are different. Create a Processor Expert project for the MK64FN1M0xxx12.


Use the menu File > New > C Project to create a new

New Project

                                             New Project

 

Provide a name for the Cross ARM GCC Freescale Processor Expert C/C++ Project:

DataLogger Cross ARM GCC Project for Processor Expert

               DataLogger Cross ARM GCC Project for Processor Expert


Then select the M4 core with the PEx Driver Suite 10.4 Wizard invocation:

M4 core for PEx DriverSuite 10.4

                             M4 core for PEx DriverSuite 10.4

 

In the next dialog I usually deselect the ‘Release’ configuration:

 

image: In the Embedded World typically there is no such thing like ‘Release’ or ‘Debug’: it is always ‘Debug’, see “Debug vs. Release?“

 

Debug only

                                        Debug only


In the next dialog I have the opportunity to configure the tool chain.


image: I’m using the ${gcc_path} Eclipse variable to point to my GNU ARM Embedded tool chain (see “Constructing a Classroom IDE with Eclipse for ARM“)

 

Cross GNU ARM Toolchain

                                        Cross GNU ARM Toolchain


Press ‘Finish’, and the project wizard calls the Processor Expert wizard to configure the microcontroller. Select the MK64FN1M0xxx12 which is present on the FRDM-K64F board:


MK64FN1M0xxx12

                                        MK64FN1M0xxx12


In the next dialog I use ‘Linked’: this means that the project uses links to the Processor Expert library files. Alternatively you can use ‘Standalone’, then the files get copied into the project.


Linked Mode

                                                  Linked Mode


Then I select the GNU C Compiler:

GNU C Compiler

                              GNU C Compiler


With ‘Finish’ the project gets created. Processor Expert opens a help window explaining how to convert a project for Processor Expert. We can ignore this as the wizard already has done everything for us image


DataLogger Project

          DataLogger Project

 

image: I’m using Processor Expert views in the next step. If this is your first Processor Expert project, make sure select the menu Processor Expert > Show Views to open the needed views.

Project Cleanup and Adjustments

While the project created is fine, I usually do some cleanup. First I remove the ‘RAM’ configuration with the context menu, as I’m only going to use the FLASH target:

Deleting Configuration

                    Deleting Configuration


Same for the obsolete CPU (orphaned now as it was tight to the RAM configuration image

                Removing RAM Configuration CPU

                                           Removing RAM Configuration CPU



The MK64FN1M0VLQ12 derivative is a LQFP 144-pin package, but the FRDM-K64F board is using a LQFP 100-pin package. In the component inspector, I change it to the 100-pin package:


image: Right click on CPU, select Inspector menu item to open the ‘Component Inspector’ view if not already open.

 

Changing CPU package

                              Changing CPU package


The PinSettings component can be removed, as we will care ourselves about the pin settings in the components:

         PinSettings Component

                                   PinSettings Component

 

Now the project is clean and using the 100-pin VLL12 package:

 

            100-pin VLL12 package

                                  100-pin VLL12 package

 

Generating Code

The project is still ‘empty’, but at this stage I prefer to verify that I can generate code, build it and download it to the target. To generate the Processor Expert code I use the toolbar icon:

 

Generate Processor Expert Code

                         Generate Processor Expert Code

Building Project

To build the project I select the project and use the ‘Hammer’ drop down icon:


Building Project

                    Building Project


It should build with no errors:

Console View with no Errors

                         Console View with no Errors

 

Debugging

I’m using here the Segger OpenSDAv2 debug firmware on the FRDM-K64F board. I select the project and open the Debug Configurations:


Menu Debug Configurations

                         Menu Debug Configurations


The double-click on the GDB Segger J-Link Debugging item to create a new configuration: The .elf and project name should be filled automatically:


New Segger Launch Configuration

                         New Segger Launch Configuration


In the Debugger tab I make sure the proper device name (MK64FN1M0xxx12) and interface (SWD) is selected:Device name and interface for Segger

                         Device name and interface for Segger


In the Startup tab I make sure semihosting and SWO are disabled:Segger Semihosting and SWO disabled

               Segger Semihosting and SWO disabled


Pressing Apply (if any changes), then press Debug to launch the debugger, and I should be debugging:Initial Debug Session

                    Initial Debug Session

 

So with this I know that everything works from building to debugging. Time to terminate the debugging session:Terminating the debug session

               Terminating the debug session


And to return to the C/C++ perspective:

Return to C and C++ Perspective

          Return to C and C++ Perspective

 

FatFS File System

To use the SD card with the FAT file system, I add the FatFS component to the project:As to write files to the file system I need date/time information, it asks me to add a clock component. I select the GenericTimeDate component:Adding GenericTimeDate Component

               Adding GenericTimeDate Component


Next, FatFS needs a memory component, and here I select the SD_Card component:


Adding Memory Component for FatFS

                    Adding Memory Component for FatFS


To protect the critical sections, it asks me to select the component I want to use. It already should have added a Critical Section (CS1) component, so I go with the CS1 choice:

 

Linking to CS1 component

                         Linking to CS1 component


With this, I have new components added to my project. Some with a red X indicate that some settings are missing:FatFS Components added

               FatFS Components added


I need to configure the pins for the SPI which talks to the SD card. For this I open the Component inspector for the SPI component:Need to configure the SPI

                         Need to configure the SPI


As the SD card on the board is connected to SPI1, I choose SPI1 as device with

  1. MISO/Input pin: PTE1
  2. MOSI/Output pin: PTE3
  3. SCLK/Clock pin: PTE2
  4. and no chip select list (use the ‘-’ button to remove it)

MISO, MOSI, Clock and chip select

                    MISO, MOSI, Clock and chip select


The chip select list is not needed as the FatFs component will handle the chip select on its own. Scrolling down I need to configure the clock details. For this I clock on the ‘…’:

 

Configuring the clock

                              Configuring the clock


From the available timings, I double-click from the list on the right hand side to have a value assigned:Selecting timing value

                              Selecting timing value


Then press OK, and do the same for the three delay timing needed:

 

Delay timing assigned

                    Delay timing assigned


For the clock rate we not only need one timing, but three: initial/low and high-speed. Again clicking on the ‘…’ for the Clock rate to open the dialog.I want to assign values in kHz, so I select that from the Unit drop down list (click into the Value field to have it updated):Clocks in kHz

                                        Clocks in kHz


As I need two values, I configure it as ‘List of values’:

List of Values

                              List of Values


Then I assign for the low value a maximum value of 375 kHz, and for high I can go up to 12 MHz (my clock configuration only allows 10 MHz max image

 

SPI Clock Values

                                        SPI Clock Values


Pressing OK to close the SPI clock configuration. To use the two configurations, I need to add a second attribute set. Because the ‘Tabs View’ uses a lot of screen real estate, it is easier if I switch to the ‘classic’ non-tabs view (small triangle in view toolbar to reach the menu image


Deselecting Tabs View

                                   Disabling Tabs View


Next step is to enable the automatic initialization of the SPI component:Automatic initialization of the SPI component

                    Automatic initialization of the SPI component


I click into the Attribute set list box (where the ’1′ is) and click on the ‘+’:Adding New Attribute Set

                                        Adding New Attribute Set


Then specify that the SPI clock index 1 shall be used:

Clock Rate Index for Attribute Set 1

                    Clock Rate Index for Attribute Set 1


In the SD_Card Component, I need to specify that it can use the index 1 (10 MHz) for fast mode:


Fast Baud Rate Mode

                    Fast Baud Rate Mode


I order to be able to switch different clock configurations, I need to enable the method SelectConfiguration():Next I need to assign the chip select pin. This is inside the SD_Card component:

 

Need to configure SPI Chip Select

                    Need to configure SPI Chip Select


The chip select is on PTE4. I can click into the field and type in the name (or to select from the list) to assign it:Assigning PTE4 as Chip Select

                    Assigning PTE4 as Chip Select


Next we add the card detection (CD) pin: I select the SD_Card component and enable the pin:Enable Card Detection Pin

                    Enable Card Detection Pin


On the FRDM-K64F, the card detection is HIGH active, so I need to deselect the ‘Card Detect is LOW active’:Card Detect Low or High Active

               Card Detect Low or High Active

 

Realtime Clock

For the SD card I need a realtime clock. Our board does not have this, but I have configured a software realtime clock: GenericTimeDate. As in this tutorial I’m not going to use an RTOS, I add a TimerInt component to the project and configure it for 10 ms:


TimerInt component

                    TimerInt component


I need to call the AddTick() method of the realtime clock every 10 ms from above interrupt:

 

Realtime Clock AddTick() Method

                    Realtime Clock AddTick() Method


So I generate code:

 

Generate Code

                    Generate Code


Then I double-click on the OnInterrupt() event to open the Events.c source file with that event created:

 

Timer OnInterrupt()

                    Timer OnInterrupt()


Then I can drag&drop the AddTick() method to the source:


Drag and Drop AddTick() Method

                    Drag and Drop AddTick() Method


Then save the source changes:

Save Source Changes

                    Save Source Changes

 

The data to log: Accelerometer

With the FatFS I have everything to read and write the SD card. Only the data is missing. In this tutorial I’m using the accelerometer of the FRDM-K64F. So I’m adding the FXOS8700CQ component to the project.It will ask for the Wait component (which already is part of the project) and automatically adds the GenericI2C component to it. I enable the LDD I2C and add a new I2C_LDD component:Adding I2C_LDD with FXOS8700CQ

                         Adding I2C_LDD with FXOS8700CQ


The I2C_LDD component gets configured for I2C0, SDA (PTE25) and SCL (PTE24), with a clock configuration below 100 kHz:


Accelerometer I2C Configuration

                    Accelerometer I2C Configuration


Important and not to forget: according to the schematics, the SA1 is LOW and SA0 pin is HIGH, so the device has the address 0x1D:

Accelerometer Slave Address

                         Accelerometer Slave Address


With this, the hardware configuration is completed, and I can write the application code image.

 

Application Code

I add a header file Application.h (context menu with File > New > Header File) and source file Application.c (context menu File > New Source File) to the Sources folder:

 

Application Files

          Application Files


The header file needs only one function:

/*

* Application.h

*/

#ifndef APPLICATION_H_

#define APPLICATION_H_

 

void APP_Run(void);

 

#endif /* APPLICATION_H_ */


In main.c, I include that header file and call APP_Run:

 

Main.c calling application

                              Main.c calling application


APP_Run() implements my logger loop: initialize the accelerometer and mount the file system. Then it gets the accelerometer data and logs it to a file every second.First, I need to make sure I have a pull-down enabled for the SD card detection pin (PTE6). Because the BitIO component has no methods to change the electrical characteristics, I’m using PDD macros (see “Low-Level Coding with PDD (Physical Device Driver)”) image


/* SD card detection: PTE6 with pull-down! */

  PORT_PDD_SetPinPullSelect(PORTE_BASE_PTR, 6, PORT_PDD_PULL_DOWN);

  PORT_PDD_SetPinPullEnable(PORTE_BASE_PTR, 6, PORT_PDD_PULL_ENABLE);


For the file system I need to have a file system object and a file pointer. To keep things simple, I’m using global variables:

 

static FAT1_FATFS fileSystemObject;

static FIL fp;

 

The APP_Run() is implemented as below:


void APP_Run(void) {
  int16_t x,y,z;
  uint8_t res;

  /* SD card detection: PTE6 with pull-down! */
  PORT_PDD_SetPinPullSelect(PORTE_BASE_PTR, 6, PORT_PDD_PULL_DOWN);
  PORT_PDD_SetPinPullEnable(PORTE_BASE_PTR, 6, PORT_PDD_PULL_ENABLE);

  res = FX1_Enable(); /* enable accelerometer (just in case) */
  if (res!=ERR_OK) {
    Err();
  }
  if (FAT1_Init()!=ERR_OK) { /* initialize FAT driver */
    Err();
  }
  if (FAT1_mount(0, &fileSystemObject) != FR_OK) { /* mount file system */
    Err();
  }
  for(;;) {
    /* get accelerometer values */
    x = FX1_GetX();
    y = FX1_GetY();
    z = FX1_GetZ();
    /* log it to the file on the SD card */
    LogToFile(x, y, z);
    /* do this every second */
    WAIT1_Waitms(1000);
  }
}



The Err() function is used to indicate an error condition. I can show an error with LED’s or I simply stop application there:


static void Err(void) {
  for(;;){}
}


I want to append the accelerometer data to a file, with date/time information, separated with TABs so I can easily import it into Excel. To construct the strings, I’m going to use the Utility component, so I have added it to my project:

Utility Component

               Utility Component


With this, I write my data to the SD card in LogToFile():

  1. Open the log file (FAT1_open()) with FA_OPEN_ALWAYS (open the file if it already exists, otherwise create the file) and for writing (FA_WRITE).
  2. Move the file pointer to the end of the file to append the data (FAT1_lseek()).
  3. Get the current time information from the software realtime clock (TmDt1_GetTime()).
  4. Construct in a buffer the string to write with time and accelerometer data.
  5. Write it to the file with FAT1_write().
  6. Close the file with FAT1_close().

static void LogToFile(int16_t x, int16_t y, int16_t z) {
  uint8_t write_buf[48];
  UINT bw;
  TIMEREC time;

  /* open file */
  if (FAT1_open(&fp, "./log.txt", FA_OPEN_ALWAYS|FA_WRITE)!=FR_OK) {
    Err();
  }
  /* move to the end of the file */
  if (FAT1_lseek(&fp, fp.fsize) != FR_OK || fp.fptr != fp.fsize) {
    Err();
  }
  /* get time */
  if (TmDt1_GetTime(&time)!=ERR_OK) {
    Err();
  }
  /* write data */
  write_buf[0] = '\0';
  UTIL1_strcatNum8u(write_buf, sizeof(write_buf), time.Hour);
  UTIL1_chcat(write_buf, sizeof(write_buf), ':');
  UTIL1_strcatNum8u(write_buf, sizeof(write_buf), time.Min);
  UTIL1_chcat(write_buf, sizeof(write_buf), ':');
  UTIL1_strcatNum8u(write_buf, sizeof(write_buf), time.Sec);
  UTIL1_chcat(write_buf, sizeof(write_buf), '\t');

  UTIL1_strcatNum16s(write_buf, sizeof(write_buf), x);
  UTIL1_chcat(write_buf, sizeof(write_buf), '\t');
  UTIL1_strcatNum16s(write_buf, sizeof(write_buf), y);
  UTIL1_chcat(write_buf, sizeof(write_buf), '\t');
  UTIL1_strcatNum16s(write_buf, sizeof(write_buf), z);
  UTIL1_strcat(write_buf, sizeof(write_buf), (unsigned char*)"\r\n");
  if (FAT1_write(&fp, write_buf, UTIL1_strlen((char*)write_buf), &bw)!=FR_OK) {
    (void)FAT1_close(&fp);
    Err();
  }
  /* closing file */
  (void)FAT1_close(&fp);
}

All what is missing now is the include of the needed header files at the beginning of Application.c:

#include "Application.h"
#include "WAIT1.h"
#include "FX1.h"
#include "FAT1.h"
#include "UTIL1.h"
#include "PORT_PDD.h"

Result

Time to generate code, build and then debug. And it writes file log.txt to the card I can import into Excel:


   Data imported in Excel

                    Data imported in Excel

 

And visualized in a chart:


Visualized Data

                                        Visualized Data

 

Summary

Writing a data logger is not that difficult with Processor Expert components. As there are many complex components (file system, SPI, I2C, accelerometer) and drivers involved, it takes some time to set everything up. But once understood, it is very easy to have such a data logger implemented easily for any other hardware.

 

The tutorial project (with minor extensions) is available on GitHub as reference implementation:https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/Eclipse/FRDM-K64F/FRDM-K64F_DataLogger

Happy Logging image

  • freedom-board
  • freescale
  • kinetis
  • frdm-k64f