Dev Tools
  • Products & Partners
  • More
Dev Tools
Files ChipKit Pi MPIDE for Raspbian armhf
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

ChipKit Pi MPIDE for Raspbian armhf

Revisions:

MPIDE 0022 - 2011.12.14

[core / libraries]

* Adding an SD card library based on sdfatlib by Bill Greiman and the
  MemoryCard library by Philip Lindsay (follower) for SparkFun.
  http://arduino.cc/en/Reference/SD

* Added character manipulation macros (from Wiring): isAlphaNumeric(),
  isAlpha(), isAscii(), isWhitespace(), isControl(), isDigit(), isGraph(),
  isLowerCase(), isPrintable(), isPunct(), isSpace(), isUpperCase(),
  isHexadecimalDigit(), toAscii(), toLowerCase(), toLowerCase().
  http://code.google.com/p/arduino/issues/detail?id=418

* Added String.toInt() function.

* Refactoring core to use register-based, not CPU-based, #ifdefs.
  Patch by Mark Sproul.
  http://code.google.com/p/arduino/issues/detail?id=307
  http://code.google.com/p/arduino/issues/detail?id=315
  http://code.google.com/p/arduino/issues/detail?id=316
  http://code.google.com/p/arduino/issues/detail?id=323
  http://code.google.com/p/arduino/issues/detail?id=324
  http://code.google.com/p/arduino/issues/detail?id=340

* Modification of serial baud rate calculation to match bootloader and 8U2
  firmware at 57600 baud.
  http://code.google.com/p/arduino/issues/detail?id=394

* Fixed bug in tone() function.
  http://code.google.com/p/arduino/issues/detail?id=361

* Fixed SPI.setClockDivider() function.
  http://code.google.com/p/arduino/issues/detail?id=365

* Fixed EEPROM library on Mega 2560.
  http://code.google.com/p/arduino/issues/detail?id=381

* Hardware serial receive interrupt optimization.
  http://code.google.com/p/arduino/issues/detail?id=391

* Applying the timeout parameter of pulseIn() during measurement of the
  pulse, not just while waiting for it.

[environment]

* Fixed problem with copy as html and angle brackets.
  http://code.google.com/p/arduino/issues/detail?id=29

* Showing serial port selection dialog if serial port not found on upload.

* Remembering serial monitor window size and line ending selection.
  http://code.google.com/p/arduino/issues/detail?id=96
  http://code.google.com/p/arduino/issues/detail?id=330

* Replaced oro.jar regular expressions with java.regex ones (patch by
  Eberhard Fahle and Christian Maglie).
  http://code.google.com/p/arduino/issues/detail?id=171

* Building the user sketch before the core or libraries, so errors appear
  faster.  Patch by William Westfield and Paul Stoffregen.
  http://code.google.com/p/arduino/issues/detail?id=393

* Setting application icon under Windows.

ARDUINO 0021 - 2010.10.02

* Modifying VID / PID combination in 8U2 firmwares.
* Fixing analogWrite() bug on pins 9 and 10 (Arduino Uno).
* Patched RXTX to include /dev/ttyACM* on Linux.

ARDUINO 0020 - 2010.09.27

* Added support for the Arduino Uno and Arduino Mega 2560.
* Including ATmega8U2 firmware used by Uno and Mega 2560.
* Including source code to optiboot bootloader used by the Uno.
* Including source code to the stk500v2 bootloader used by Mega 2560.
* New application icon (by ToDo).

ARDUINO 0019 - 2010.09.03

[core / libraries]

* Revised Ethernet library (by Christian Maglie).  This depends on the
  new SPI library, so existing sketches will need: #include <SPI.h>
  added to the top of their code.

* Added an SPI library (by Christian Maglie).
  http://code.google.com/p/arduino/issues/detail?id=240

* Added aliases for the analog input pins: A0, A1, etc.
  http://code.google.com/p/arduino/issues/detail?id=244

* Added a String class.  

* Added a shiftIn() function (from Wiring).
  http://code.google.com/p/arduino/issues/detail?id=280

* Updated version of Firmata supports Mega and capability querying.

* More accurate delay() function from BenF.
  http://code.google.com/p/arduino/issues/detail?id=237

* Re-enabling PWM after tone() ends.
  http://code.google.com/p/arduino/issues/detail?id=228

* Added Serial.peek() method.
  http://code.google.com/p/arduino/issues/detail?id=270

* Added Stream base class to Serial object (w/ available(), read() and
  the write(), print(), and println() functions from the Print class).
  http://code.google.com/p/arduino/issues/detail?id=60

* Disabling interrupts while digitalWrite() and pinMode() write to pins.
  http://code.google.com/p/arduino/issues/detail?id=146

* Replacing INTERNAL analog reference with INTERNAL1V1 AND INTERNAL2V56 on
  the Arduino Mega.  http://code.google.com/p/arduino/issues/detail?id=194
 
[environment]

* Added Arduino Fio to the boards menu.

* Added Arduino Pro and Pro Mini (5V / 16 MHz) to the boards menu.
  http://code.google.com/p/arduino/issues/detail?id=81

* Synchronized with the Processing 1.1 code base, bringing various changes.

* Modified the parsing of avr-gcc / avr-g++ output and error messages.

* Toggling RTS on upload for auto-reset with FTDI cables on Linux.
  http://code.google.com/p/arduino/issues/detail?id=309

* Adding control over scrolling in serial monitor.
  http://code.google.com/p/arduino/issues/detail?id=97

* Added drop-down for selecting line endings to the serial monitor.
  http://code.google.com/p/arduino/issues/detail?id=119

* Fixed problem with tabs of the same name but different extensions.
  http://code.google.com/p/arduino/issues/detail?id=191

* Allowing third-party hardware platforms to reference programmers defined
  in other platforms.  http://code.google.com/p/arduino/issues/detail?id=283

[examples]

* Re-organized and numbered for easier access and better progression.

ARDUINO 0018 - 2010.01.29

[core / libraries]

* Added tone() and noTone() functions for frequency generation.
* Added Serial.end() command.
* Added precision parameter for printing of floats / doubles.
* Incorporated latest version of Firmata.
* Fixed bug w/ disabling use of the RW pin in the LiquidCrystal library. 
* No longer disabling interrupts in delayMicroseconds().
* Fixed bug w/ micros() returning incorrect values from within an interrupt.
* Fixed bug that broke use of analog inputs 8-15 on the Mega.

[environment]

* Synchronized with the Processing 1.0.9 code base, bringing various fixes,
  including to a bug causing saving to fail when closing the last sketch.

* Added support for third-party hardware in the SKETCHBOOK/hardware folder,
  mirroring the current structure of the hardware folder in Arduino.

* Added Ctrl-Shift-M / Command-Shift-M shortcut for serial monitor.

* Hold down shift when pressing the Verify / Compile or Upload toolbar 
  buttons to generate verbose output (including command lines).

* Moving build (on upload) from the applet/ sub-folder of the sketch
  to a temporary directory (fixing problems with uploading examples from
  within the Mac OS X disk image or a Linux application directory).

* Fixed bug the prevented the inclusion of .cpp and .h (or .c and .h) files
  of the same name in a sketch.

* Improved the Mac OS X disk image (.dmg): added a shortcut to the
  Applications folder, a background image with arrow, and new FTDI drivers.

ARDUINO 0017 - 2009.07.25

[documentation / examples]
* Many new and revised examples from Tom Igoe.

[core / libraries]
* Updated LiquidCrystal library by Limor Fried.  See reference for details.
* Updated Firmata library to version 2.1 (rev. 25).
* Replaced the Servo library with one (MegaServo) by Michael Margolis.
  Supports up to 12 servos on most Arduino boards and 48 on the Mega.
* Improving the accuracy of the baud rate calculations for serial
  communication (fixing double-speed problems on 8 MHz Arduino boards).
  Thanks to gabebear.

[environment]
* Synchronized with the Processing 1.0.3 code base (rev. 5503), bringing
  many improvements (listed below).
* New icons and about image by Thomas Glaser (envis precisely).
* Support for multiple sketch windows.
* The serial monitor now has its own window.
* Comment / Uncomment menu item (in Edit) and keyboard shortcut.
* Increase and Decrease Indent menu items (in Edit) and keyboard shortcuts.
* Support for third-party libraries in the SKETCHBOOK/libraries folder.
* Libraries are now compiled with the sketch, eliminating the delay when
  switching boards and the need to delete .o files when changing library
  source code.
* Arduino now comes as an app file (in a dmg) on the Mac.
* Adding the Arduino Nano w/ ATmega328 to the Tools > Board menu.

ARDUINO 0016 - 2009.05.30

[documentation / examples]
* New communication examples (w/ corresponding Processing and Max/MSP code) by
  Tom Igoe.

[core / libraries]
* Adding support for the Arduino Pro and Pro Mini 3.3V / 8 MHz w/ ATmega328.
* Adding support for the LilyPad Arduino w/ ATmega328.
* Adding write(str) and write(buf, size) methods to Print, Serial, and the
  Ethernet library Client and Server classes.  This allows for more efficient
  (fewer packet) Ethernet communication.  (Thanks to mikalhart.)
* Improvements to the way the Ethernet library Client class connects and
  disconnects.  Should reduce or eliminate failed connections and long
  timeouts.  (Thanks to Bruce Luckcuck.)
* Optimizing the timer0 overflow interrupt handler (used for millis() and
  micros()).  Thanks to westfw and mikalhart.
* Fixing bug that limited the bit() macro to 15 bits.  Thanks to Paul Badger.
* Adding ARDUINO version constant (thanks to prodding from mikalhart).
  
[environment]
* Ordering the items in the Tools > Board menu.
* Adding "Copy as HTML" command to the Tools menu.
* Eliminating (maybe) the occasional "Couldn't determine program size" errors.
  Thanks to the Clever Monkey.
* Moving selection of Linux look-and-feel into the arduino script so it can
  be changed by users.  Thanks to Eberhard Fahle.
  
[tools]
* Adding automatic dependency generation to the Makefile.  (Lars Immisch)

ARDUINO 0015 - 2009.03.26

[core / libraries]
* Adding support for the Arduino Mega (ATmega1280).

[environment]
* Reinstating use of core.a library in the build process, slightly shrinking
  compiled sketch sizes.  (Thanks to William Westfield.)
* Fixing bug in copy for forum (thanks to eried).

ARDUINO 0014 - 2009.03.07

[core / libraries]
* Fixing bug that prevented multiple outgoing Client connections with the
  ethernet library.
  
[environment]
* Clarifying ATmega168 vs. ATmega328 in the Tools > Boards menu.

[tools]
* Updating the Mac OS X AVR tools to AVR MacPack 20081213.  This includes
  avr-gcc 4.3.2, which should fix problems with functions called from 
  within interrupts.

ARDUINO 0013 - 2009.02.06

[documentation / examples]
* Adding examples for Parallax Ping Sensor and Memsic 2125 accelerometer.

[core / libraries]
* Adding support for the ATmega328.  The upload speed is 57600 baud, so you
  may need to edit boards.txt or reburn your bootloader if you bought an 
  ATmega328 w/ bootloader from adafruit or other supplier.
* Adding support for printing floats to Print class (meaning that it works
  in the Serial, Ethernet, and LiquidCrystal classes too).  Includes two
  decimal places.
* Added word, word(), bitRead(), bitWrite(), bitSet(), bitClear(), bit(),
  lowByte(), and highByte(); see reference for details.
* Working around problem that caused PWM output on pins 5 and 6 to never go
  to 0 (causing, for example, an LED to continue to glow faintly).
* Removing cast macros, since function-style casts are a feature of C++.  This
  should fix contributed libraries that broke in Arduino 0012.
* Modifying pulseIn() to wait for a transition to start timing (i.e. ignoring
  any pulse that had already started when the function was called).
* Fixing bug in random() that limited the ranges of values generated.  Thanks
  to Mikal Hart.
* Modifying delay() to pause for at least the given number of milliseconds.
* Fixing bug in Ethernet library that interfered with use of pins 8 and 9.
* Originating each outgoing network connection from a different port (in the
  Client class of the Ethernet library).  Thanks to Paul and joquer.
* Updating ATmega168 bootloader to work with standard distributions of avrdude
  (responding to signature requests made with the universal SPI command) and
  correctly store EEPROM data.  Thanks to ladyada.
  
[environment]
* Omitting unused functions from compiled sketches, reducing their size.
* Changing compilation process to allow for use of EEMEM directive (although
  not yet uploading EEPROM data).

ARDUINO 0012 - 2008.09.18

* Added Arduino Nano to the boards menu.
* Arduino Pro or Pro Mini (8 MHz) to the boards menu.
* Added Firmata library by Hans Steiner and others.  This provides a standard
  protocol for communicating with software on the computer.
* Added an Ethernet library for use with the Arduino Ethernet Shield.
* Added a Servo library based on the work of Jim Studt.
* Added a LiquidCrystal library based on the work in the playground.  It
  supports both 4- and 8-bit modes.
* Improved millis(): it now overflows after 49 days instead of 9 hours, but
  now uses slightly more processing power.
* Fixed reversing direction bug in Stepper library.  (Thanks to Wayne Holder.)
* Moved insertion of #include <WProgram.h> to after any comments and #include
  statements in the main sketch file.  This means that an #include <stdlib.h>
  now works.
* Upgraded to newer versions of avr-gcc (4.3.0) and avr-libc (1.6).  This
  provides support for newer Atmel chips, but may increase the size
  of sketches.
* Allowing per-board specification of the upload.using preference, allowing
  upload via bootloader to some boards and via a programmer to others.
* Added return values to some functions in the Wire library to allow for
  better error handling.
* Fixed random() to work with long values.
* Creation of an abstract Print base-class to allow Serial, SoftwareSerial,
  and LiquidCrystal to share code for print() and println().
* Incorporated ladyada's watchdog timer mods to the bootloader source, but
  only compiling them in for the Pro and Pro Mini (because they are included
  in the bootloader being burned on the boards by SparkFun).

ARDUINO 0011 - 2008.03.28

* Fixed Find in Reference.
* Added map() function for mapping values from one range to another.
* Added analogReference() function.
* Added interrupts() and noInterrupts() functions.
* Added degrees() and radians() functions.
* Added timeout parameter (in microseconds) to pulseIn(); default is 1 second.
* Support for uploading sketch using a programmer.
* Improved detection of functions that need prototyping.
* Placing function prototypes after #include's and #define's.
* No longer moving #include statements to the top of the sketch.
* Can now drag .pde files onto the Arduino dock icon on Mac OS X.
  Thanks to Peter Sgouros.
* New script for downloading the reference from Tom Pollard.  Thanks Tom!
* Miscellaneous Mac OS X and other patches from Wim Lewis.  Thanks Wim!
* Updated Mac OS X FTDI drivers.

ARDUINO 0010 - 2007.10.11

* Support for the LilyPad Arduino.
* Vista support.
* Mac OS X universal distribution.
* Printing!
* Copy for discourse.
* New Board menu replaces the Microcontroller menu.
* New Burn Bootloader menu offers a choice of programmers.
* New and improved keyboard shortcuts.
* Fixed some find/replace bugs.
* Better auto-format.
* Improved error messages when uploading.
* Support for COM10 and higher on Windows.
* Fixed automatic refresh of the Serial Port menu under Windows.
* Quaqua look-and-feel on Mac OS X.
* Reorganization of the Arduino application directory.

ARDUINO 0009 - 2007.08.06

* Added support for the Arduino Diecimila.
* Switched to using avrdude (instead of uisp) for uploading sketches.
* Added the ability to burn NG and Diecimila bootlaoders (with an AVRISPmkII).
* Fixed a bug in SoftwareSerial (a hardware serial function was being called
  instead of the software serial equivalent).  Thanks to brianbr for the
  report and fix.

ARDUINO 0008 - 2007.06.09

* Updated examples (in distribution and on the website).
* Added an EEPROM library (see reference for details).
* Added a Stepper motor library (see reference).
* Patched to reduce binary sketch sizes by building the Arduino core as
  a library (.a) file - now only the needed parts of the core are linked into
  a sketch.  Originally written by Nicolas Roland, revised by Don Cross.
* Fixed bug in Serial.available().  Report and fix by Don Cross.
* Now recompiling libraries when switching microcontrollers.  Report by
  Julian Bleecker; fix by Nicholas Zambetti.
* Cleaned up core functions: moved pin definitions into program space to save
  RAM, and other minor improvements.  Contributed by Jim Studt.
* Lots of reference additions and fixes from Paul Badger.
* Changed default microcontroller to ATmega168 from ATmega8.
* Removed the delay from analogRead().
* Activating TWI/I2C pullup resistors on the ATmega168 (in addition to the 
  ATmega8).

ARDUINO 0007 - 2006.12.25

* Smaller core (about 3.5 KB instead of 4.5 KB).
* Added a SoftwareSerial library (thanks to Antonio, Heather Dewey-Hagborg, and
  bigengineer for their help).
* Implemented a Serial.flush() routine; see reference for details.
* Digital pins 0 and 1 can be used for i/o until a call to Serial.begin().
* Replaced avr-lib's uart routines with custom code for handling serial
  communication and modified C++ serial commands to call the C serial commands;
  the code may behave slightly differently in border cases (e.g. non-standard
  speeds, or on overflow).
* Added attachInterrupt() and detachInterrupt() functions for handling of
  external interrupts on pins 2 and 3.
* Implemented shiftOut() routine; see reference for details.
* Defining binary constants: e.g. B1010 is 6.
* Mac versions no longer require running of the macosx_setup.command script.
* Windows version comes with the FTDI USB drivers already unzipped.
* New Linux binary distribution (still requires some programs to be
  pre-installed).

ARDUINO 0006 - 2006.10.21

* Mac version no longer requires Java 1.5, meaning it should run on 10.3.9.
* Added support for analog inputs 6 and 7 and pwm on pins 5 and 6 on the
  on the ATmega168 used in the Arduino Mini (extra analog inputs not available
  in DIP ATmega168s).
* You now select the baud rate for the serial monitor from within the editor
  status bar when the serial monitor is running instead of from the Tools menu.
* Pressing enter within the serial monitor edit box no longer appends a newline
  to the message sent to the board.
* Included the Wire (TWI) library from Wiring.
* Updated the reference.

ARDUINO 0005 - 2006.09.26

* Applied patch from Hans Steiner to improve Linux support by searching for avr
  tools in the user's path instead of expecting them at a fixed location.
* Added an upload.verbose preference for help in debugging.
* ATmega168 support!
* New Wiring-compatible randomSeed(), random(max) and random(min, max) functions
  (except operating on longs instead of floats).
* Fixed bug that sometimes caused uploading of old versions of a sketch.
* Serial monitor nows include an interface to send messages to the Arduino
  board.  Pressing return appends a newline, pushing the send button doesn't.
* Now displaying "burning bootloader..." and "compiling..." status messages.

ARDUINO 0004 - 2006.04.26

* Main sketch is now compiled as C++ (instead of C).
* Updated avr toolchain.
* printInteger(), printHex(), etc. now handle longs.
* millis() fixed (now overflows after days, not minutes)
* Fixed path to java in Windows run.bat.
* Added Matrix and Sprite libraries (written with Nicholas Zambetti).
* PWM now working on pin 11 (in addition to pins 9 and 10).
* Slowed PWM frequency (on all three PWM pins) to 1KHz.
* Now give an error if compiled sketch is too big.
* Fixed abs(), min(), max(), and constrain() macros.
* Added menu items to the IDE to burn bootloader.
* Now display binary sketch size on upload, and give error if too big.
* Added C++ serial library.
* Resynced with Processing/Wiring IDE code (improved auto-format, faster logging
  to serial monitor console, other bug fixes)
* New library system.
* Updated to latest version of the RXTX serial library; Mac users will need to
  rerun macosx_setup.command.

ARDUINO 0003 - 2006.01.16

API Changes
* Reversed the analog input pins to correspond to newer boards.  This means
  a call, for example, to analogRead(0) must be changed to analogRead(5) in
  order to read the same physical pin.
* Added a printNewline() function (which sends '\n' = ASCII 10).

New Stuff
* Reference is included (features native to C not yet documented).
* Serial monitor added (click the toolbar button to turn it on or off).  Baud
  rate is controlled by the Serial Monitor Baud Rate Menu, defaults to 9600.
  Icon and implementation from Wiring.
* Serial port menu now automatically refreshes when opened.
* New blue color scheme and icons courtesy of Noah Shibley (colors are hardcoded
  into the source to ensure consistency with image files).
* Keyspan and FTDI USB drivers included with Mac and Windows distributions.

Bug Fixes
* millis() now updates every millisecond instead of every second.
* Bootloader included with Windows distribution (it was already in the Mac
  dist).
* Updated icon of the Windows executable.
* Now flushing the serial port before uploading (should fix some errors).
* Improved accuracy of the delayMicroseconds() function.

Other
* Upload rate no longer selectable from a menu within the IDE.  Instead, edit
  the serial.download_rate item in the preferences.txt file.
* Created Xcode project for building Arduino on the Mac (doesn't yet regenerate
  the grammar files or package the distribution); active target should be "App".
* Removed unused or unimplemented items from menus.

ARDUINO 0002 - 2005.10.05

* New build process no longer uses makefiles; now controlled by preferences.txt.
* core/ replaced with targets/; can now link against Wiring libraries.
* Replaced print() with printString, printInteger, printHex, printByte, etc.
* Added menu for selecting serial port speed.
* Updated icon.
* Bootloader shrunk to less than 1 KB; fuses updated accordingly.
* Added serialRead(), serialAvailable(), and delayMicroseconds().

ARDUINO 0001 - 2005.08.25 

* This is the first released of the unified IDE + language library
  it's a terrible hack... but it works. at the moment it's in alpha stage
  but it can be used to work.
* The processing preprocessor is included but not used.

Taken from Raspbian image chipkit_pi.zip / ChipKitPi.zip previously provided

  • chipkit pi
  • pi
  • mpide
  • chipkit
  • raspberry pi
  • raspbian
cstanton
cstanton
  • 2 Dec 2025
  • 4 Downloads