NI LabVIEW Community
  • Products & Partners
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum Getting error when running with custom firmware on pico with labview
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 33 replies
  • Subscribers 132 subscribers
  • Views 6290 views
  • Users 0 members are here
  • LabVIEW and Test Automation Course
  • pico
  • labview
Related

Getting error when running with custom firmware on pico with labview

cbohra00627
cbohra00627 over 2 years ago

I am trying to create a labview driver for controlling the pi pico led. I went through the Digital Out Control.vi VI in pico_scpi_usbtmc_labtool and tried to replicate it for the led control. I took the blink example from pico-sdk examples directory and added the function to control led (i.e. gpio_put(LED_PIN, 1)) to the SCPI_DigitalOutput() function of gpio_utils.c file in pico_scpi_usbtmc_labtool. I created a new firmware with this change and loaded on pi pico. Now, whenever I do digital write HIGH, the led is turning on.

But when I tried to create a separate driver for led control with a separate SCPI command, I am getting some error while running the VI. The build was successful with my change and I loaded the firmware on the pico, but when I am trying to run my VI (snip attached below), I am getting the below error.

image

Code for led control:

led_utils.c:

image

led_utils.h

image

I have added the led executable and dir path to Cmakelists.txt and also added the INSTRUMENT_LED_OUTP_COMMANDS macro to scpi commands list in scpi-def.c

Am I missing something? Has anyone seen this error before?

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 2 years ago +4
    This is failing in the init code, so it’s not even reaching your code. One of the installed tools with LabVIEW is NI I/O Trace. Run that, turn on tracing, then run the VI again and see if that gives you…
  • cbohra00627
    cbohra00627 over 2 years ago in reply to Jan Cumps +3
    Its working now!
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +2
    The init block indeed checks for the IDN* string I haven't exposed the connectors to the button that can turn ID Check off. You can do this yourself, by clicking on the connector location in the…
Parents
  • cbohra00627
    0 cbohra00627 over 2 years ago

    HI Andrew J Jan Cumps , I checked the string constants inside the init block, the "display \ codes" option is checked. Then I tried turning off the ID query for the init block, this time I didn't face the issue. After running with "Step over subVI", it seems the issue occured after the read operation for ID. In the probe watch window, in the possible reason section, it is written "VISA:  (Hex 0xBFFF0015) Timeout expired before operation completed." One more thing, I am getting this error only on alternate runs and that too only in my custom VI. Other example VI's are working fine.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to cbohra00627

    If you look at the comment in the code it says to ignore the timeout and the error code is the same as the one in the probe.  I don’t know why this happens really - Jan has given a hint but it’s not something I’ve seen - but that error should get removed and the VI complete successfully.  Is there a value on the bytes read wire.  Also, use NI I/O Trace to get an idea of what is going on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 2 years ago in reply to cbohra00627

    If you look at the comment in the code it says to ignore the timeout and the error code is the same as the one in the probe.  I don’t know why this happens really - Jan has given a hint but it’s not something I’ve seen - but that error should get removed and the VI complete successfully.  Is there a value on the bytes read wire.  Also, use NI I/O Trace to get an idea of what is going on.