NI LabVIEW Community
  • Products & Partners
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum Getting error when running with custom firmware on pico with labview
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 33 replies
  • Subscribers 132 subscribers
  • Views 6306 views
  • Users 0 members are here
  • LabVIEW and Test Automation Course
  • pico
  • labview
Related

Getting error when running with custom firmware on pico with labview

cbohra00627
cbohra00627 over 2 years ago

I am trying to create a labview driver for controlling the pi pico led. I went through the Digital Out Control.vi VI in pico_scpi_usbtmc_labtool and tried to replicate it for the led control. I took the blink example from pico-sdk examples directory and added the function to control led (i.e. gpio_put(LED_PIN, 1)) to the SCPI_DigitalOutput() function of gpio_utils.c file in pico_scpi_usbtmc_labtool. I created a new firmware with this change and loaded on pi pico. Now, whenever I do digital write HIGH, the led is turning on.

But when I tried to create a separate driver for led control with a separate SCPI command, I am getting some error while running the VI. The build was successful with my change and I loaded the firmware on the pico, but when I am trying to run my VI (snip attached below), I am getting the below error.

image

Code for led control:

led_utils.c:

image

led_utils.h

image

I have added the led executable and dir path to Cmakelists.txt and also added the INSTRUMENT_LED_OUTP_COMMANDS macro to scpi commands list in scpi-def.c

Am I missing something? Has anyone seen this error before?

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 2 years ago +4
    This is failing in the init code, so it’s not even reaching your code. One of the installed tools with LabVIEW is NI I/O Trace. Run that, turn on tracing, then run the VI again and see if that gives you…
  • cbohra00627
    cbohra00627 over 2 years ago in reply to Jan Cumps +3
    Its working now!
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +2
    The init block indeed checks for the IDN* string I haven't exposed the connectors to the button that can turn ID Check off. You can do this yourself, by clicking on the connector location in the…
Parents
  • cbohra00627
    0 cbohra00627 over 2 years ago

    HI Andrew J Jan Cumps , I checked the string constants inside the init block, the "display \ codes" option is checked. Then I tried turning off the ID query for the init block, this time I didn't face the issue. After running with "Step over subVI", it seems the issue occured after the read operation for ID. In the probe watch window, in the possible reason section, it is written "VISA:  (Hex 0xBFFF0015) Timeout expired before operation completed." One more thing, I am getting this error only on alternate runs and that too only in my custom VI. Other example VI's are working fine.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to cbohra00627

    I had to pop out, but looking a bit further.  Your first error you reported was the other one shown in this VI, 1074003951, which implies that the timeout error is being swallowed (check the output wire of the clean error VI that is highlighted in your image.)  So what is on the wire that goes into the string comparison from the VI Read and the Constant PICO-PI,LABTOOL.  Try probing further through that VI execution but please do try NI I/O Trace to see what it says.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    main reason for a timeout is a (maybe previous)  query that's sent without termination. The lib is then waiting for the rest of the message.

    If an invalid command is sent, the lib will handle that properly and push the error on the error stack.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to Jan Cumps

    Thanks for that.  It's surprisingly easy to send a query without termination if the string isn't set to display codes.  I took that problem away in my framework, although it could still be possible for someone to send a command that has what they think is a terminator when in fact it's two bytes (a \ and a n.)  I should check for that and strip it off before adding the correct terminator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    labview has a block to add the right  terminator to a string. Don't know it by heart anymore. But that one makes it easier to not make mistakes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Jan Cumps

    Found it back in the MCCDAQ driver I wrote for a road test:

    image

    So far for being consistent Slight smile.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to Jan Cumps

    Useful.  Is that in the String palette?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    yes

    image

    It's a combination of a string ending in the terminator ";", a Concatete Strings (2nd top line), and a Line Feed Constant (second bottom line).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    yes

    image

    It's a combination of a string ending in the terminator ";", a Concatete Strings (2nd top line), and a Line Feed Constant (second bottom line).