NI LabVIEW Community
  • Products & Partners
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum Getting error when running with custom firmware on pico with labview
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 33 replies
  • Subscribers 132 subscribers
  • Views 6306 views
  • Users 0 members are here
  • LabVIEW and Test Automation Course
  • pico
  • labview
Related

Getting error when running with custom firmware on pico with labview

cbohra00627
cbohra00627 over 2 years ago

I am trying to create a labview driver for controlling the pi pico led. I went through the Digital Out Control.vi VI in pico_scpi_usbtmc_labtool and tried to replicate it for the led control. I took the blink example from pico-sdk examples directory and added the function to control led (i.e. gpio_put(LED_PIN, 1)) to the SCPI_DigitalOutput() function of gpio_utils.c file in pico_scpi_usbtmc_labtool. I created a new firmware with this change and loaded on pi pico. Now, whenever I do digital write HIGH, the led is turning on.

But when I tried to create a separate driver for led control with a separate SCPI command, I am getting some error while running the VI. The build was successful with my change and I loaded the firmware on the pico, but when I am trying to run my VI (snip attached below), I am getting the below error.

image

Code for led control:

led_utils.c:

image

led_utils.h

image

I have added the led executable and dir path to Cmakelists.txt and also added the INSTRUMENT_LED_OUTP_COMMANDS macro to scpi commands list in scpi-def.c

Am I missing something? Has anyone seen this error before?

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 2 years ago +4
    This is failing in the init code, so it’s not even reaching your code. One of the installed tools with LabVIEW is NI I/O Trace. Run that, turn on tracing, then run the VI again and see if that gives you…
  • cbohra00627
    cbohra00627 over 2 years ago in reply to Jan Cumps +3
    Its working now!
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +2
    The init block indeed checks for the IDN* string I haven't exposed the connectors to the button that can turn ID Check off. You can do this yourself, by clicking on the connector location in the…
Parents
  • cbohra00627
    0 cbohra00627 over 2 years ago

    I ran the NI I/O trace, in that I am seeing error in alternate VISA read commands.
    image

    Then I ran the existing VI and my VI, I could see that there is some issue in the VISA Write command.

    image

    The VISA Write commands are different even if I am using similar format in the string.

    imageimage

    The string in my command is not proper and I think that is causing the issue for the next run.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to cbohra00627

    yes.Right-click on the yellow format block, and select Edit Format String

    image

    What do you see (the one from my digital output as example)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cbohra00627
    0 cbohra00627 over 2 years ago in reply to Jan Cumps

    Its showing "%s" only.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to cbohra00627

    You can type the correct string there. Replace the %s with:

    :LED:OUTPUT %s\n

    then press OK,and test again

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    +1 Andrew J over 2 years ago in reply to cbohra00627

    Shouldn't that be into a terminal on the top of the Format block, not the left?  It may just be the way the wire is shown but there is a terminal on the left there (intro string I think) and it's the wrong one so the default %s is tagged on to the end.  Look at how the :Digital:OUTPUT:... to the left is wired.  Also, you'll need to sort out the \\n: that's a result of setting display codes on when you already had the \n in the string - it's all a bit poor unfortunately, but I found the easiest was to delete the \\n then re-edit the string and just add \n.  I think, it's been a while since I had the problem!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    yes well spotted that's it ! The left top is initial string, top format string.

    Wrong connector used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    yes well spotted that's it ! The left top is initial string, top format string.

    Wrong connector used.