Evaluation Board for FONA - Mini Cellular GSM Breakout uFL Version

Manufactured By:adafruit industries
Evaluation Board for FONA - Mini Cellular GSM Breakout uFL Version Evaluation Board for FONA - Mini Cellular GSM Breakout uFL Version
Evaluation Board for FONA - Mini Cellular GSM Breakout uFL Version
Evaluation Board for FONA - Mini Cellular GSM Breakout uFL Version
Part Number:1946
It's your breadboard! Introducing Adafruit FONA MiniGSM, an adorable all-in-one cellular phone module that lets you add voice, text, SMS and data to your project in an adorable little package. This module measures only 1.75"x1.25" but packs a surprising amount of technology into its little frame. At the heart is a GSM cellular module (we use the latest SIM800) the size of a postage stamp. This module can do just about everything. This version has a uFL connector.

You will also need some required accessories to make FONA work. These are not included!
  • SIM Card! A 2G Mini SIM card is required to do anything on the cellular network. US AT&T no longer sells 2G SIMs and will shut off their 2G network, so for American customers we recommend any T-Mobile or reseller (TING, SIMPLE mobile, etc) that uses the T-Mobile network.
  • Lipoly Battery - 500mAh or larger! This 500mAh battery, or this 1200mAh will work great.
  • MicroUSB cable for charging the battery.
  • External Antenna - We like this slim sticker-type, which plugs right in. Alternatively, this straight SMA one or this right-angle SMA one will work but you'll also need a uFL to SMA adapter cable so you can connect to your SMA antenna
There's also some recommended accessories. They are not required but chances are you'll want them!
  • TRRS 4-Pole Headset - Any 'iPhone' or 'Android' compatible (but not iPhone original) should work. We tried about 10 different ones, and basically the more expensive once are more comfortable and louder but our official iPhone headset mic did not work.
  • External Mic & Speaker - If you want to talk directly to your FONA, an electret mic and mini 8 ohm speaker will do quite nicely.
  • Vibrating motor - the FONA can drive this directly, just solder a mini vibrating motor disc in!
  • USB console cable - the microUSB connector is for charging only, but you can wire up a console cable for direct-connection to the module if you want to send commands from a terminal (great for testing and tweaking)

Features

  • Cellular Features
  • Quad-band 850/900/1800/1900MHz - connect onto any global GSM network with any 2G SIM (in the USA, T-Mobile is suggested)
  • Make and receive voice calls using a headset OR an external 8O speaker + electret microphone
  • Send and receive SMS messages
  • Send and receive GPRS data (TCP/IP, HTTP, etc.)
  • Scan and receive FM radio broadcasts (yeah, we don't exactly know why this was included but it works really well)
  • PWM/Buzzer vibrational motor control
  • AT command interface with "auto baud" detectionAdditional Features
  • Onboard LiPoly battery charging circuitry so you can take your project on the go.
  • Standard 4-pole TRRS headphone jack. Use any 'Android' or 'iPhone'-compatible headset with mic
  • Breakouts for external 8O speaker and electret mic if you don't want to use a headphone
  • Level shifting circuitry so you can run it with 2.8V to 5V logic.
  • Vibrational motor (buzzer) driver so you can have noiseless notifications
  • uFL connections for external antenna
  • Indicator LEDs for power and network connectivity
  • Standard SIM slides into the backRequired Accessories for Operation
  • SIM Card! A 2G Mini SIM card is required to do anything on the cellular network. T-Mobile network.reccomended
  • Lipoly Battery -
  • for charging the battery.
  • External Antenna - See below for Antenna optionsOptional Accessories for Operation

Ships With

  • Development Board

Required Tools

Accessory Tools

Documents

Downloads