Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Blog My  own PSOC project
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vsluiter
  • Date Created: 17 Mar 2014 9:07 AM Date Created
  • Views 1866 views
  • Likes 2 likes
  • Comments 2 comments
  • psoc4
Related
Recommended

My  own PSOC project

vsluiter
vsluiter
17 Mar 2014

I've made several posts in the PSOC Smarter Life Challenge, but never used the PSOC in my own designs. After I've seen the possibilities in the challenge, I came across a project at my work where I realized that PSOC could be a nice solution.

We're using some haptic feedback voice coils that need to be driven with a sine wave at a specific frequency. We're also using an EtherCAT based system that should control these motors. To make control easier, I wanted to make something where a digital input would come in, and a sine wave would come out if the input line was asserted for a channel. The other thing I wanted is to synchronize the outputs with the sine wave produced; the output should only be active for a multiple of one sine wave.

 

At first I wanted to use DMA for this, but the PSOC4 doesn't have that and the PSOC5  was too large for the design (and I wanted to play around with the PSOC4, to be honest).

After a day of tinkering, this was the result:


image

 

I'm using PWM1 to generate the PWM of the sine wave. The Digital comparator is contolling the 8 parallel D-flipflops whose outputs are AND-ed with the PWM signal. In my code, I'm writing the sine table sample number to 'DDS_count'. At the first sample, the comparators' output is changing state, and the DFFs latch the input values. The DDS_Sample_Clock determines how fast I'm going through my sine table. It generates an interrupt on which a new sample is written to the PWM block.

To get the software running, I only had to follow this post:Using Math Functions in PSoC Creator for PSoC5's GCC Compiler - Cypress to resolve an error with the linker. This post:Introduction to Interrupts for PSoC 4 Hardware Blocks - Cypress helped me to get going with the interrupts. Here's the code:

 

#include <project.h>
#include <math.h>
#define DDS_LENGTH 100
uint8_t dds_table[DDS_LENGTH] = {0,10,20,30,40,50,60,70,80,90};

CY_ISR(DDS_sample_clock_timer)
{   
    uint32 int_source;
    int_source = DDS_Sample_Clock_GetInterruptSourceMasked();
    DDS_count_Control = DDS_count_Read() + 1;
    if(DDS_count_Read() == DDS_LENGTH)
        DDS_count_Control = 0;
    PWM_1_WriteCompare(dds_table[DDS_count_Read()]<<8);
    DDS_Sample_Clock_ClearInterrupt(int_source);
     
}

void CreateSineTable(void)
{
    int i;
    for(i = 0 ; i < DDS_LENGTH ; i++)
    {
        dds_table[i] = 126*(1.0-cos(i*6.28/DDS_LENGTH));
    }
}


int main()
{
    CreateSineTable();
    /* Place your initialization/startup code here (e.g. MyInst_Start()) */
    PWM_1_Start();
    //DDS_max_count_Control = DDS_LENGTH;
    DDS_count_Control = 0;
    DDS_Sample_Clock_Start();
    DDS_Sample_Clock_SetInterruptMode(DDS_Sample_Clock_INTR_MASK_TC);
    DDS_sample_clock_timer_Start();
    DDS_sample_clock_timer_StartEx(DDS_sample_clock_timer);
    CyGlobalIntEnable;  /* Uncomment this line to enable global interrupts. */
    for(;;)
    {
        /* Place your application code here. */
    }
}

 

That looks simple doesn't it? To enhance the resolution, I only need to increase DDS_LENGTH, and change the DDS_Sample_Clock period.

 

The only thing that I've encountered is that it sometimes would be nice to get access to one of the values in a building block in the CySch directly. For example, it would be nice to directly use the output of an ADC to the DDS_Sample_clock Period value to change the output frequency. I don't  kinow whether/how that's possible

  • Sign in to reply
  • cy.gul
    cy.gul over 12 years ago

    Hey Victor,

    looks like the PSoC bug has bitten you too - great to see you tinker with the platform =)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Hi Victor,

     

    Interesting project.  Keep us posted on how this implementation works out.

     

    DAB