Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits

Blog

  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Getting started with PSoC 6 and ModusToolbox software

    vinayyn
    vinayyn
    We are all aware of AVR, PIC, ARM, and ESPS which are widely used in embedded systems. Besides, there is one new and feature-rich IoT-enabled embedded platform, the PSoC 6 WI-Fi-BT Pioneer Kit that ...
    • 14 Oct 2022
  • PSoC 4 BLE Pioneer Kit Workshop

    fvan
    fvan
    I attended a workshop on the PSoC 4 Bluetooth Low Energy Pioneer Kit, presented by Cypress Semiconductor and hosted by Future Electronics. It was after reading about it on the element14 community site (Thanks clem57) that I checked if a workshop was ...
    • 13 Mar 2015
  • PSoC 4 Prototyping Kit on OSX (or Linux) with VirtualBox

    fvan
    fvan
    Introduction Gurinder Singh Gill has started a blog series on the PSoC 4 Prototyping Kit (CY8CKIT-049-42xx) from Cypress. The fact that the software required to program the kit runs on Windows only, has held me back from using it.But, as I ...
    • 30 Nov 2014
  • My  own PSOC project

    vsluiter
    vsluiter
    I've made several posts in the PSOC Smarter Life Challenge, but never used the PSOC in my own designs. After I've seen the possibilities in the challenge, I came across a project at my work where I realized that PSOC could be a nice solution.We're us...
    • 17 Mar 2014
  • Low Cost DAC Boosts PSoC Amp Performance by Over 30dB

    tpcipri
    tpcipri
    In this blog we will look at how to improve the performance of the Cypress ADC_Differentaial_Preamplifier Starter Design included with PSoC Creator 3. With a simple addition the common mode performance of the circuit can be improved by 30dB using ine...
    • 12 Feb 2014
  • 2013 CY-ARM PSoC Professor Conference

    e14 Contributor
    e14 Contributor
    54 professors from 29 PSoC labs in China joined 2013 annual PSoC professor conference in Shanghai Jiaotong University on Dec. 1st, 2013. 4 professors gave PSoC4 lectures to share their teaching and research experience in PSoC4. I attached the present...
    • 17 Dec 2013
  • Using a Cypress PSoC5 to Sniff Out PCB Shorts

    tpcipri
    tpcipri
    Tracking down and finding short circuits on a PCB can always be a challenge. The resistance can be down to micro-Ohms. Not every meter can measure that low and the meters that can measure micro-Ohms are very costly and you still have to deal with noi...
    • 8 Oct 2013
  • PWM Controled by on board Capacitive Slider

    jason721
    jason721
    From what I have used this for the thing that sold me the most about using this more in the future is the ease of using the PSoC Creator. It reminded me a lot of simulator software I used in school. I decided to start with Project 2 CapSense Sli...
    • 30 Jul 2013
  • Two LEDs flashing using only hardware components of the PSoC

    e14 Contributor
    e14 Contributor
    Hello everybody, It took me some hours of fun making this simple project. It turned out  - after understanding the PSoC - that both the PSoC Creator the Pioneer board are easy to use and offer great flexibility - as they claim. The pro...
    • 26 Jul 2013
  • PSoC 4 Pioneer Kit Community Project#040 - PioneerPnPSensors

    kanatomi
    kanatomi
    Hello! This project demonstrates the PioneerKit Plug and Play Sensor application for direct connection with SNTerminal running on Desktops and Mobiles giving full access to monitor and control the key status, capsense slider, internal temperatur...
    • 26 Jun 2013
  • 第一次尝试.........

    Master_Ping
    Master_Ping
    大家好: 操作系统: Window 7 首次用 PSoC Creator打开一个从 element14社区下载的 “闪烁的LED项目”. 大致来讲,你可以用这个电路板来编C++ 程序. 我还没有进一步研究它还可以支持什么程序语言. 留待下次吧。 当你运行脉宽调制调试模式时, 编好的程序会把LED的 闪烁时间更新在16位记数器内。而你可以把LED闪烁的时间加长或缩短。这个程序有一个好处就是清楚的显示 记数器地址方便你做进一步的调试。 一开始的时候,我有一些混...
    • 30 May 2013
  • My First Project Review.........

    Master_Ping
    Master_Ping
    Hello Everybody: I download the software under window 7 and it was simple enough.  Steps were clear.  I used the link without the download manager. You can use the download manager but I did not use it.  It’s simpler to just downl...
    • 30 May 2013
  • Cypress PsoC4 Pioneer Kit: Further Blurring The Line Between Analog and Digital

    DaveYoung
    DaveYoung
    The new Cypress Pioneer Kit single board computer has come out offering just about anything a maker would want on one board.  It runs a 32-bit ARM CPU on one chip, and a 32-bit microcontroller on a second chip.  The microcontroller has all ...
    • 15 May 2013