Cypress Kits
  • Products
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#16 - Proximity Theremin
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 31 subscribers
  • Views 5679 views
  • Users 0 members are here
  • theremin
  • 100projects
  • proximity
  • capsense
  • 4
  • psoc
Related

PSoC 4 Pioneer Kit Community Project#16 - Proximity Theremin

cy.gul
cy.gul over 13 years ago

Hello folks!

 

Today's project is a personal favorite of mine because it got the amateur/wannabe musician inside me very excited. Building on yesterday's example of how to do proximity sensing with the CapSense Component, today we're going to use that concept in an application. This example project implements a Theremin, a 1920s electronic musical instrument played without physical contact.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The project uses two proximity sensors - one for Pitch and another for Volume. The proximity sensing itself is done using wires that act as antennas, input to the PSoC 4 using the CapSense block.

The theremin has 2 modes - discrete and continuous notes, toggled by using the pushbutton (SW2) on the board. Pitch information is indicated by the color of the LED, while Volume information is indicated by the brightness of the same LED.

The Cortex-M0 CPU takes the analog input from the CapSense proximity sensors and send a parameter indicating distance to the hardware PWMs, that in-turn modulate the LED. The CPU also sends data to the 2 other PWMs that are used to drive the a Buzzer that creates the musical notes.

The project also includes a UART Component so you can read the CapSense proximity sensor data over hyperterminal.

 

image

 

What's cool about this project?

- It uses 5 (five!) hardware 16-bit PWMs - 3 of which are implemented on the TCPWM block (modulating the RGB LEDs), wheres 2 more implemented using UDBs (to drive the buzzer).

- It implements distance sensing using CapSense proximity

- It lets you make music in the air! Check out the demo video above.

 


Hardware Connections:

 

image

 

The RGB LED and the pushbutton switch are on the board. In addition to the PSoC 4 Pioneer Kit, you're going to need -

- an 18 ohm Speaker/Buzzer (P2[0])

- 2 resistors, 2 capacitors

- hanful of jumper wires

 

image

 

 

The project is attached below, its all ready to go. Just build and program on to your PSoC 4 Pioneer Kit, and wire up a small buzzer.

Have fun making music!

 

 

 

 





 



Attachments:
KIT042_Theremin.Bundle01.zip
  • Sign in to reply
  • Cancel

Top Replies

  • jesusantoniocar
    jesusantoniocar over 13 years ago +1
    Hello Gagan. Thanks for give us this amazing project, great design with few elements to build. i will buy some elements that need to make a full test. best regards, jesus antonio.
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to greatunclebulgaria +1
    Hey David, Great question. Actually, you need just one 100ohm resistor and one 8ohm/0.1W speaker (see image below). You could use a speaker with a different rating as well - for this application, it doesn…
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to jesusantoniocar +1
    Hello. It is a new video with the last file project.. best regards, Jesus Antonio. players.brightcove.net/.../index.html
Parents
  • cy.gul
    cy.gul over 13 years ago

    A quick update to share with the community -

     

    We're excited to share a recent PSoC design success in an audio end-product - The KORG Kaossilator 2 and mini KAOSS PAD 2.

    The PSoC 3 in this design handles the CapSense touch and MIDI controller functions of the products.

     

    "Both the Kaossilator 2 synthesizer and mini KAOSS PAD 2 apply Cypress's CapSense capacitive touch technology to implement the ultra-fast responsiveness of the touchpad and slider, improving upon the performance of the resistive touch controls in KORG's previous generation of products. PSoC 3's programmable digital logic drives the signal converter of the products' Organic Electroluminescent (OEL) displays while freeing up their central processing units (CPUs) for optimal performance."

     

     

    More details here - http://www.edn.com/electronics-products/other/4418167/Cypress-s-PSoC-selected-for-intuitive-touchpad-in-Korg-handheld-music-synthesizers

     

     

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cy.gul
    cy.gul over 13 years ago

    A quick update to share with the community -

     

    We're excited to share a recent PSoC design success in an audio end-product - The KORG Kaossilator 2 and mini KAOSS PAD 2.

    The PSoC 3 in this design handles the CapSense touch and MIDI controller functions of the products.

     

    "Both the Kaossilator 2 synthesizer and mini KAOSS PAD 2 apply Cypress's CapSense capacitive touch technology to implement the ultra-fast responsiveness of the touchpad and slider, improving upon the performance of the resistive touch controls in KORG's previous generation of products. PSoC 3's programmable digital logic drives the signal converter of the products' Organic Electroluminescent (OEL) displays while freeing up their central processing units (CPUs) for optimal performance."

     

     

    More details here - http://www.edn.com/electronics-products/other/4418167/Cypress-s-PSoC-selected-for-intuitive-touchpad-in-Korg-handheld-music-synthesizers

     

     

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to cy.gul

    Hello Gagan.

    Spectacular, no words, psoc opens the doors for many applications. Psoc  is a powerful platform to create products,  kaoss pad 2 and kaossilator 2 are great designs.

     

    best regards,

     

    Jesus Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jesusantoniocar

    Hello Fellas,

     

    This project is a great job, but i had a few questions about the Hyperterminal software.

    In fact I download it but I have no idee how to make it work, I looked on youtube but that was useless.

    I want to create a platform on Labview but i need to receive the information from the Psoc on my computer.

    If you have a better solution let me know.

     

    Thank you for your answwers,

     

    Regards

     

    Giulio