Cypress Kits
  • Products
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#035 – UART, I2C, and SPI Joystick Example
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 33 subscribers
  • Views 8270 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#035 – UART, I2C, and SPI Joystick Example

cy.wbz
cy.wbz over 13 years ago

Hello!

 

This Project demonstrates the simultaneous use of UART, SPI and I2C protocols of communication in one single project. SPI is used to communicate the position of the Joystick in the Pmod JSTK Joystick Module. The I2C is used to obtain the current time from the Real Time Clock (RTC). UART is used to print the time obtained via I2C on the Hyperterminal and move its position in accordance with the Joystick.

image

  • PSoC 4 Pioneer Kit
  • PmodJSTK – 2 Axis joystick
  • Real Time Clock DS1307

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • SPI
  • I2C
  • UART
  • CyPins
  • CyClock

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

This firmware example is an excellent demonstration of how the PSoC 4 can interface using three different serial interfaces (SPI, I2C, and UART). The example reads in the time data from the RTC using I2C, then pulls the positioning data from the Joystick using the SPI interface, and then completes the example by sending the RTC value to hyperterminal and using the joystick to control where the RTC value is displayed on the screen.

 

While the example almost seems like a game, please step back and consider how this type of system dynamic would be common in an end design. We can imagine pulling in data from two separate inputs and having to relay those values up to a main host or PC. In many case the input data may affect other data and require some type of data manipulation.

 

Hardware Connections:

 

The user will need to populate and solder the 6 pin Pmod header to the Pioneer kit. This header will allow the user to connect the Pmod Joystick module. The SPI interface that reads the values from the joystick will be configured and set in the PSoC 4 project. There is already a physical connection between the Pmod module and the PSoC 4 device. The SPI pins on the PSoC 4 will be: P3[0], P3[1], P3[5], P0[6], and P0[7].

 

Next connect the Pioneer board to the Real Time Clock board. First connect the Vdd and GND lines from the Pioneer kit to the Clock board. Next connect your I2C lines from the Pioneer board to the Clock board. The I2C lines are: P4[0] and P4[1].

 

Also connect the PSoC 4 UART connections to the PSoC 5LP device so the UART positioning can be relayed up to the host.

 

PSoC 4 P3[7] -> P5LP P12[6]

PSoC 4 P0[5] -> P5LP P12[7]

 


image

 

Test Your Project:

 

After connecting your project please program the example into the PSoC 4 device. Once programmed then launch your Hyperterminal software to view the UART data traffic. Then use the joystick to control the output on the hyperterminal software.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
I2C_SPI_UART.cyprj.Archive01.zip
0447.Project Images.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar +1
    Hello Jesus, There are two types of SPI component available for the PSoC 4 in the PSoC Creator 1) UDB based 2) SCB based For providing the external clock to the UDB based SPI, open the Advanced tab in…
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to jesusantoniocar +1
    Hi. It is an interesting article to share: PSoC 4 Chained Clocks http://www.cypress.com/?rID=81829&source=home_cdc best regards, Jesus Antonio
  • icemanfiveoh
    icemanfiveoh over 12 years ago in reply to icemanfiveoh +1
    Hi, I was successfully able to get the terminal to display the DS1307 RTC Time but it is all over the terminal window. I am going to see if i can strip away some code to stop that from happening. Also…
Parents
  • dandumit
    dandumit over 12 years ago

    Hello,

    I have tried for hours to set  CY8CKIT-042CY8CKIT-042 to use SPI Master on Digilent port P3.5 P3.0 P3.1 and P0.6
    I have found your project and it looks that you have mapped SS to 0.7 and after that you have added another separate pin SS and you are managing it separately from code.

     

    Could you please give me some more details on this specific work around ?

     

    Kind Regards,

    DAniel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dandumit
    dandumit over 12 years ago

    Hello,

    I have tried for hours to set  CY8CKIT-042CY8CKIT-042 to use SPI Master on Digilent port P3.5 P3.0 P3.1 and P0.6
    I have found your project and it looks that you have mapped SS to 0.7 and after that you have added another separate pin SS and you are managing it separately from code.

     

    Could you please give me some more details on this specific work around ?

     

    Kind Regards,

    DAniel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dandumit

    Hello Daniel,

     

    The design uses an (Serial Communication Block) SCB based fixed function SPI Master. The SCB mandates usage of specific pins for MISO, MOSI, SCLK, and Slave Select. Also, the line (Slave Select 1) SS1 can be used only if line (Slave Select 0) SS0 is used. This means that, the design has to connect P0.7 as the slave select for the project to build successfully.

     

    The design will work fine with a stand-alone PSoC 4, but in PSoC 4 Pioneer Kit (CY8CKIT-042) this pin is connected to the user switch*. Also, the pin P0.7 is not available on any of the headers. This is why another pin is used in design to implement Slave Select.

     

    One other way to do this without using an extra pin is to use a USB based SPI Master component from PSoC Creator instead of SCB based SPI Master.

     

    *Note: The pin P0.7 is also used to wakeup the device from low power modes such as Sleep, Deep-Sleep, Hibernate, and Stop. This is the reason for using P0.7 for switch.

     

    Hope this helps.

     

    Happy Programming!

     

    Ranjith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello Friend

     

    Can you get me your contact detail. I have lots of queries regarding SPI in PSoC 4.

     

    Kindly get me reply as soon as possible.

     

    Thnak you.

     

    Bharat Surani

    suranibharat4@gmail.com