Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#042 – Hangman Game
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 28 subscribers
  • Views 2396 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#042 – Hangman Game

cy.wbz
cy.wbz over 13 years ago

Hello!

 

It has been our Friday tradition for the past few weeks to end with a game. This week we have the Hangman game. In this game the user will be using two Pmod boards, an LCD and Button board to display outputs and generate inputs for the system. The user will be presented with a  word that has some letters filled. The user will need to guess letters to complete the word. The words you will be trying to figure out are names of Countries. Your selections (correct and incorrect) will be displayed. The game will let you know if you have guessed the correct letters or have you exceeded the number of incorrect guesses, thus creating the hangman.

 

image

 

image


 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • SPI
  • CyPins
  • ISR

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this project PSoC 4 interfaces with the PmodCLS - Character LCD which has 16x2 Character Display to provide flexible communications using UART, SPI or TWI to give a visual output. In this example we use the SPI communication method. The example project also interfaces a PmodBTN - Push Button module with PSoC 4 to provide a user interface to the game.

 

Hardware Connections:

 

You will need to connect two Pmod modules to the Pioneer board. We are connecting the LCD to the existing Pmod header and having to wire in the second Pmod into the arduino headers. Feel free to use a breadboard sheild for the second Pmod module. The following image provides a wiring diagram for connecting the Pmod boards.

 

image

 

Test Your Project:

 

Connect your hardware and program your project into the PSoC 4. Follow the LCD screen messages to play the game.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
4722.Project Images.zip
Hangman.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hello! I've attached a video of the game in action. Thanks, Renuka players.brightcove.net/.../index.html
Parents
  • DAB
    DAB over 13 years ago

    I like your progression to increasing complexity.

     

    This method should help encourage people to learn Psoc in a step by step manner.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 13 years ago

    I like your progression to increasing complexity.

     

    This method should help encourage people to learn Psoc in a step by step manner.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to DAB

    Hello Matt.

    Great friday project. it has many lines of code specially in the main c, i can see more functions, it is great for all community. Strong examples well documented.

     

    Ready to the next week for our robots projects.

     

    have a good weekend.

     

    best regards,

     

    Jesus Antonio.