Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#050 – SD Card Example
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 37 subscribers
  • Views 8201 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#050 – SD Card Example

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today we are starting a short series targeting SD memory cards. In this first example we are introducing users to the SD card using the custom SD card component. This component will expose simple API level commands to read from and write to the SD card. In this example we are targeting a 2gig SD memory card.


  • PSoC 4 Pioneer Kit
  • SD Card shield
  • 2 gig SD card

 

image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations
  • Custom Component Datasheet

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • SD Card
  • CyClock
  • CyPins

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we ship a custom SD card component and component datasheet to describe the functionality and available APIs and source files. The Component datasheet has been attached to this post. We have used custom components in the past so please refer to those examples for guidance. You will need to import the SD card component from the example project into your design if you want to use the custom component.

 

image

 

This SD card component uses the SPI interface to communicate to the SD card. The SPI interface is part of the SD card component and should be configured in the pin selections in the PSoC Creator DWR window.


In this example we show the user how to setup and initialize the SD card on the SD card shield. The remaining set of code in the example shows the user how to perform a number of common actions on the SD card:


  • Write File
  • Append File
  • Read File
  • Rename File
  • Copy File
  • Delete File

 

An important note before using the SD card, you will need to format the SD card prior to using it in this example. To format the SD card please navigate to the SD card web site to download the SDFormatter tool. Formatting the SD card is a one-time activity to enable it’s use. You will want to use a SD card reader or your SD card slot on your PC.

 

https://www.sdcard.org/downloads/formatter_4/

 

Hardware Connections:

 

The SD card shield uses the 6 pin header for SPI communications. This header on the Pioneer board is, by default, not populated. You will need to solder on a 6 pin header to enable this connection. The Seeedstudio SD card reader uses the 6 pin header to communicate over SPI to the SD card. Once you have added this header connect the Seeedstudio shield to the Pioneer kit.

 


image

 

Test Your Project:

 

Program the example into the PSoC 4 kit. Edit and play around with the commented code to create new files. Then remove the SD card and plug into an SD card reader or PC that has an SD card port to verify the PSoC 4 actions.

 

image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
SDCard_Mass_Storage_Example.zip
6305.Project Images.zip
imageSDCard_V1_0.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +2
    Hi Andrew, Few things to check: 1. You need to format your SDCard with SDFormatter ( https://www.sdcard.org/downloads/formatter_4/ ). Windows formatting does not create a boot record. 2. SD Card should…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +2
    Sriram V S, Thank you, thank you, thank you! I was using a 16GB SD card (I must have missed the 2GB limit in my enthusiasm to try things out). Using a smaller card, everything is working well with my data…
  • danadak
    danadak over 12 years ago +1
    I am trying to bring up the shield and project in Creator 3.0. Some ques/observations - 1) In 3.0 Creator produces ~ 40 warnings on type mismatches used in code. But compiles. 2) In Creator debug I cannot…
  • e14 Contributor
    e14 Contributor over 12 years ago

    Has anybody updated this since the most recent Creator update?  I tried this project but found that dependant components have been updated/obsoleted.  So now, the project is "broken."   I am really not sure what to do.  I am trying to build a system with SD card capability for PSoC4, but am pretty unsuccessful (mainly because I am fairly new to PSoC Creator).  I know PSoC5 has emFile, but PSoC4 is very attractive with regard to pricing.  Anyways, if anybody can provide an update to this, I would be most gracious.

    tech_contentPSoC 4 Pioneer Kit Community Project#050 – SD Card Example

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • thomas_barth
    thomas_barth over 12 years ago in reply to e14 Contributor

    Hey Justin,

    I updated to the newest Version of the components and it just works fine. (SD Card)

    What Card are you reading? SD?

     

    Make sure you have the right voltages, make sure you have not mixed up MISO and MOSI and make sure you have the right CS.

    I have a slightly different setup as my socket is on a TFT board. However, just VDD and GND are provided there.

    I simply connected MISO MOSI CS(the pin, not the SPIM out) and CLK. (and skipped the others)

     

    Only drawback in my eyes is that you have to use SCB0 (no SCB1) pins on the board. And the CS might be a bit confusing (actually, somebody knows why the SPIM CS pin isnt working).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • thomas_barth
    thomas_barth over 12 years ago

    Great project Matt!

     

    Im just wondering one thing, what is happening if the SD card is full?

    It would be nice to also have something like "SDCard_GetFreeSpace". I dont know FAT and if there is any chance to read that information easily or if you need to go through all files.

     

    Anyway, great project and perfect starting point.

     

    What is the difference between SD and SDHC on that low level, maybe also an idea for the next step.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Finally got it working with PSoC Creator 3 on a PSoC4, but one thing caused quite a bit of consternation: in FS.C you check for valid filenames beginning with 'A' to 'Z', but valid filenames can also start with numerals (as mine did). Thus I always got zero files found.

    Nevertheless, great work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey, I tried your program out using a PSoC 4, but when I try to read the SD Card using my PC, the PC returns an error message stating that the SD Card contains an unsupported file system. I've tried formatting it using all possible formats(fat16, fat32, etc.), using SDCard Formatter, using both mmc and micro sd cards, but it returns the same error message all the time. Any idea as to why this is happening and any methods to solve this problem? I've reading and writing to the same SD cards using Arduino programs and it works. Only the PSoC program gives me problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Kabron
    Kabron over 11 years ago in reply to e14 Contributor

    Bug found:

    In the function SDCard_GetFileCount() maximum return value is 110 while the manual said:

     

    "The root directory typically contains 512 entries of 32 bytes each.  When using short filenames (DOS 8.3 format ), this means a maximum of 511 files listed"

     

    I made simply example(attached) that contain (D)ir command to test the problem.  To test you must have SDCard with more than 110 files in root folder.

     

    Should I create a case?

     

    Attaching failed. Here is the link:

     

    https://drive.google.com/open?id=0BwK34EimhNEufmdGZ3dCWHBveGdCdkJDRTVSUGVVazRvUW5kWHZLX09SQmZPMlVmbDczdVE&authuser=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hey Niramay,

     

    I am also facing the same problem. Please let me know if you have solution for the same by this time. I am pretty new to PSoC 4 (Pioneer Kit).

    I am using Micro SD Card Module SD Storage Board TF Card Memory Shield SPI FOR Arduino | eBay    microSD card reader module.

     

    Any help will be appreciated.

     

    Regards,

    Sarang

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Dear Matt

     

    Thanks for this SD project.

     

    I am going to use this firmware in a kind of datalogger. I am just testing the performance and whether ist is working good for me.

     

    My problem: I tried to write  more than 3.5 MB in small portions into one file, always opening and closing this file. After about 3.5 MB the card seemed to be defect, as it did not answer any more when performing the next  SDCard_fputcs(buffer, fp);

    It seems that there is some confusion with the FAT, as after resetting the SD Card by unplugging and plugging it again, I could not open and close the file more than 5 or 6 times. The same with a new file. The software seems to hang at  SDCard_AddFat(uchar Fptr)   when seeking for the next free FAT entry.

    Only by formatting the card I am abble to write again a file with about 3.5 MB. Then I have the same problem again.

     

    Do you have any idea?

    Did anyone have the same problem?

     

    Bert

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi Matt!


    Great project!

    Im wondering if it is possible to get this project to run on a PSoC5LP?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bootnebil
    bootnebil over 11 years ago

    Hello guys

    I'm new to psoc platform could any one help me to interface my psoc 4 ble pioneer kit -042 with an I2C LCD already has a controller to a just sad scl vcc gnd pins

    Thank in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>