Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#029 – Bluetooth Home Automation System
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 32 subscribers
  • Views 6474 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#029 – Bluetooth Home Automation System

cy.wbz
cy.wbz over 13 years ago

Hello!

 

We are continuing with our wireless subseries with the 100 projects in 100 days. Last week we showcased a number of examples using the XBee wireless modules. Yesterday we gave you an example on how to connect your Pioneer kit to a WiFi network. Today we will showcase how to interface with your Pioneer kit using Bluetooth.

 

Today’s project is designed to control the On/Off status of an appliance using Bluetooth. The user is required to have an Android Phone with Bluetooth capabilities through which one can send commands using the Bluetooth SPP Application. This App sends the command to the Bluetooth Shield on PSoC4 which then controls the relays on the Relay Shield. The appliance then turns on or off according to the relay position.

 

  • CY8CKit-042
  • Relay Shield
  • BlueTooth Shield

 

image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
  • Project Schematic
  • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • UART
  • CyClock
  • Interrupt
  • Logic Low ‘0’
  • CyPin

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

If you need any additional information on the shields that we are using today please take a moment to review the following web pages:

  • Relay Shield
  • BlueTooth Shield

 

This example also uses the Bluetooth SPP app for Android phones. This app is available for Android phones only, and can be found at the following link:

  • Bluetooth SPP

 

Once the user has configured the Bluetooth connection they will be able to use the Bluetooth SSP application to control the Pioneer kit. In the header section of the main.c file you see the defined commands that can be sent to the Pioneer kit. These are the values that the user can enter into the SPP application to either turn on or off the appliance (Light). This example supports up to four applications being controlled from a cell phone.

 

Hardware Connections:

 

For this example you will need to have both the Relay and Bluetooth Shields. We will first insert the Bluetooth Shield into the Pioneer kit. On the top of the Bluetooth Shield are headers that will allow us to then insert the Relay Shield. Here we’ve ‘stacked’ the Arduino shields allowing us to use both the Bluetooth and Relay capabilities.

 

Now that the shield boards are connected to the Pioneer kit we then need to connect the Relay shield to the power supply and then to our light bulb setup. 

 

image

 

Test Your Project:

 

Program the Pioneer kit, start the SPP application and then begin to send command controls to the Pioneer kit using the pre-defined values.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
2235.Project Images.zip
Home_Automation_Bluetooth_Relay_Shield.zip
  • Sign in to reply
  • Cancel

Top Replies

  • cy.wbz
    cy.wbz over 13 years ago in reply to uplatise +1
    Uros, I believe robotshop has some Euro locations and they provide Bluetooth shields. They are not the same as seeedstudio, but that might be a start to avoid customs. http://www.robotshop.com/eu/contact…
  • gihu
    gihu over 13 years ago +1
    Hi all, Very nice project. @Uros, a nice BT shield from Microchip is RN 42, I used in a project where I built an app for my cell phone to read an 8 analog input Bluetooth module. @Matthew, not much complicated…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I dont have PSOC 4. I have PSOC 1,3 & 5. could it possible to do this project using either PSOC 1,3 & 5?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    I dont have PSOC 4. I have PSOC 1,3 & 5. could it possible to do this project using either PSOC 1,3 & 5?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cy.wbz
    cy.wbz over 13 years ago in reply to e14 Contributor

    Ralph,

     

    For PSoC 3/5 you should be able to use PSoC Creator to recreate the design using the components designed for the P3/5 devices. You may need to change the name of the API calls and some minor selections in the configuration GUIs for the P3/5 devices.

     

    I spoke with one of our Apps guys here in Washington and he said that it would be best to open the P4 project and then open another instance of Creator and copy the hardware design in the new instance. The selections should be similar. Once you have the hardware design copied you can then go into the code and begin copying sections of code. Note that some of the API names might change or be slightly different. It might require a few builds to clean up the code.

     

    The PSoC 1 port would be a slight challenge and require you to use PSoC Designer to devleop your applciation. PSoC Designer does not implement the schematic capture so the use of cypins and the logic components in this design would need to be changed to align with the Designer User Module paradigm. Designer does have UART user modules so you would be able to easily communicate to the BT module.

     

    If you port the project to P3 or P5 please post that project to this page in case others may want to give it a try!

     

    Please let me know if this helps you.

     

    Thanks,

    Matthew Buza

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cy.wbz
    cy.wbz over 13 years ago in reply to cy.wbz

    Ralph,

     

    I forgot to mention, from your question I'm assuming you have the CY8CKit-001? If so then one of our 3rd party vendors has an expansion board to arduino adapter if you want to easily plug in the Relay shield into the Kit-001.

     

    http://www.patternagents.com/projects/CPM_Shield.html

     

    You don't need to have this hardware but it might make it easy to plug the relay shield into the 001 kit.

     

    -Matt Buza