Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#031 – Ethernet Shield
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 31 subscribers
  • Views 10058 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#031 – Ethernet Shield

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today we are presenting an example on how to use the Arduino Ethernet Shield. In this example we have ported the Arduino Ethernet libraries and dependent core libraries to the PSoC 4. In this example we implement a web server application using the Pioneer Kit. This project can be used as a base platform for any Ethernet application using the PSoC 4 Pioneer Kit.

This example is fairly complex so please take some time to review the supplemental documentation we’ve provided on this example. In this example we’ve ported the C++ libraries from Arduino into PSoC. We’ve included documentation on how the firmware for this project was developed, but also documentation on how we ported the C++ code to PSoC.


  • CY8CKit-042 BUY NOW!BUY NOW!
  • Ethernet Shield  BUY NOW!BUY NOW!

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
  • Project Schematic
  • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Counter
  • SPI
  • CyPins
  • CyClock

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

The detailed firmware description for this example project is long so we’ve attached it to this post. This example ports the Ethernet libraries from the Arduino software to the PSoC 4. The libraries are used to create a simple web server that provides inputs to the user through hyperlinks. When the user selects these links they will be able to control the RGB LED on the Pioneer kit. For more information on the Firmware and the porting from the Arduino libraries please take a look at the attached guide below.

 

Hardware Connections:

 

For this example the user will need to populate the six pin J12 header. This header is located near the CapSense slider on the Pioneer board. The Arduino Ethernet shield uses the 6 pin connector for the SPI communications with the WiFi processor. You will need to populate this header to use this shield board.

 

For more information on the 6 pin header and part number please reference the Pioneer Kit Bill of Materials (BOM) section of the User Guide.

Once the connector is populated then please connect the Ethernet Shield to the Pioneer board. There are no other hardware connections needed.

 

Test Your Project:

 

Stack your Ethernet shield on your Pioneer Board.

 

Open the command prompt on your PC. Type in ‘ipconfig’ and you will get able to find your LAN default gateway. This assumes that your PC is connected to the internet. You will need to modify the main.cpp file with the updated Gateway IP address. For example, if your IP address is “444.444.4.4” then set the IP address in your main.cpp file to “444.444.4.402”.

 

Then recompile the project and program the Pioneer kit. Connect an Ethernet cable from the RJ45 connector on the Ethernet shield to the router.

 

Open a browser  on the PC and type in the IP address that you configured above into the URL bar.

 

The browser will display the web page created by the Pioneer kit and Ethernet shield. Click on the links on the web page to control the RGB LED behavior on the Pioneer kit.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
C++ In Creator.doc
imageFirmware Description.docx
EthWebServer.cyprj.Archive01.zip
75206.Project Images.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Thanks for your effort Matt, a great start to ethernet and PSOC... I have the project running, with no difficulty. But I do have a problem with various browsers I tested. 1/ Chrome, first pass of switching…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    Michael, Glad to know that you were able to have the project running with ease. Coming to the issues you are facing: #1: Yes, your observation is correct. Chrome has this feature of caching the pages and…
  • cy.gul
    cy.gul over 13 years ago in reply to e14 Contributor +1
    Hi Rutger, there's plenty of examples demonstrating such features, take a look around the rest of the projects posted here. Here's a couple you may find useful - PSoC 4 Pioneer Kit Community Project#01…
Parents
  • jesusantoniocar
    jesusantoniocar over 13 years ago

    Hello Matt.

    Excellent project, it will be able to  design our own sensors and monitor for network through a web browser.

    the description of the project  is very good. i have a question which is the speed that supoort this shield via ethernet (10/100/1000)?.

     

    i will get this shield to play with this.

     

    best regards,

     

    Jesus antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Hi Jesus Antonio,

     

    This ethernet shield supports speeds of 10/100 Mbps. The ethernet controller is W5100. In this project, the ethernet controller is configured in auto-negotiation mode. This means that if the network supports 100 Mbps, then the ethernet controller configures itself for this speed, else it will default to 10 Mbps.

     

    Regards,

    Shashikant

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to e14 Contributor

    Hello Shashikant.

    Thanks for your  response and explanation, i have in mind some ideas to build with this.

     

    best regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hola  Shashikant Joshi:

     

    Quisera saber si puedo encontrar un tutorial completo para desarrollar ejemplos en la Tarjeta Psoc  CY8CKIT-042CY8CKIT-042 PSoC 4 PIONNER KIT para iniciar a desarrollas proyectos y

    de la misma manera para la tarjeta shield- Ethernet y la Tarjeta Etherneet de arduino.

    Gracias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hola  Shashikant Joshi:

     

    Quisera saber si puedo encontrar un tutorial completo para desarrollar ejemplos en la Tarjeta Psoc  CY8CKIT-042CY8CKIT-042 PSoC 4 PIONNER KIT para iniciar a desarrollas proyectos y

    de la misma manera para la tarjeta shield- Ethernet y la Tarjeta Etherneet de arduino.

    Gracias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Aura Lucia Pirazan Suarez,

     

    There are resources available at our website to learn PSoC4. Here are some links that you can start with:

    Application Note on Getting Started with PSoC4 - http://www.cypress.com/documentation/application-notes/an79953-getting-started-psoc-4?source=search&cat=technical_documents

    PSoC Creator 101 Video Lessons - Start with http://www.cypress.com/video-library/PSoC-Software/psoc-creator-101-psoc-creator-file-structure/108306

     

    Please let me know the details of your project that you are working on and what support you need. I will try and get you the necessary support.

     

    Regards,

    Shashikant