Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#053 – PSoC Eye
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 29 subscribers
  • Views 3177 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#053 – PSoC Eye

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today we are focusing on integrating sensor detection with motor control. We have created what is lovingly called the ‘PSoC Eye’. In this example we are using the Wii Remote IR tracking sensor to control two servo motors that pan and tilt to track the movement of an IR light emitting target.

  • PSoC 4 Pioneer Kit
  • Pixart WiiMote IR Camera
  • Servo Motors

 

image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • PWM (x2)
  • I2C
  • CyPins

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we use the I2C component to communicate with the IR sensor. The values received by this sensor will determine the movement of the two servo motors to maintain the sensor’s view of the target. We are using two PWM components to control the two servo motors.

 

We have also attached two specifications to this post, one specification for the Pixart sensor and the second for the two servo motors.

 


image

 

Hardware Connections:

 

In this example we have attached both the servo motors and the Pioneer kit to plexiglass. A custom breadboard is used to connect the Pioneer board to the Sensor and Servo motors. The schematic is included below. The two motors are used to pan and tilt the sensor. The bottom motor is fixed to the plexiglass and will spin allowing for azimuthal (pan side to side) angle calculation. Fixed to the top of that motor is the second motor that will move the sensor about the polar angle (tilt up and down). In this example the bottom and top motors will spin 180 degrees allowing you to track all objects in one hemisphere of available space.

 


image

 

Test Your Project:

 

Program your Pioneer kit and then move a IR emitting object around in front of the sensor. You will see that the PSoC 4 device will control the servo motors to track the object.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
PSoC_Eye.zip
1512.Project Images.zip
imageVigor_VS1_Servo.pdf
imagePixart_WiiMote_IR_Camera.pdf
  • Sign in to reply
  • Cancel
Parents
  • jesusantoniocar
    jesusantoniocar over 13 years ago

    Hello Matt.

    Thanks for this project.

    Infrared imaging is used to analyze light at wavelengths longer than those of the visible spectrum and provide analogous displays for interpretation. It has applications in industry, law enforcement, military, medical, and consumer electronics.

    great project and i would like to build a similar application with my pioneer kit.

    http://www.youtube.com/watch?v=JqGr3BRNiN8&feature=player_embedded

     

    best regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jesusantoniocar
    jesusantoniocar over 13 years ago

    Hello Matt.

    Thanks for this project.

    Infrared imaging is used to analyze light at wavelengths longer than those of the visible spectrum and provide analogous displays for interpretation. It has applications in industry, law enforcement, military, medical, and consumer electronics.

    great project and i would like to build a similar application with my pioneer kit.

    http://www.youtube.com/watch?v=JqGr3BRNiN8&feature=player_embedded

     

    best regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cy.wbz
    cy.wbz over 13 years ago in reply to jesusantoniocar

    Jesus,

     

    I've asked the Engineer who developed this to add a video. He will post it when it is complete.

     

    Please feel free to post your project when you are complete.

     

    Thanks,

    Matt