Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#058 – An Introduction to Processing
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 28 subscribers
  • Views 1111 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#058 – An Introduction to Processing

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example talks about using the open source programming software called Processing. This open source development environment is widely used in the Arduino community to create simple computer GUI interfaces for end applications. In this example we will give you a demonstratation of the power and simplicity of Processing. We will generate an application that allows the user to draw  a user created image. We will incorporate Processing in a Pioneer kit example later this week.

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Zip File of Images

 

Components Used:

 

This is a software only example so the user will not use any components.

 

Firmware Description:

 

In this example we will use the programming environment called Processing. This open source coding environment allows the user to generate simple computer based applications. Users can create applciations that generating interfaces, displays, and outputs. The following image is the Processing development window. You will notice, if you have experience with Arduino, that it looks very similar to the Sketching environment for Arduino.

 


image

 

The Processing software is hardware agnostic and can be used to enhance embedded example projects. It also allows customers to rapidly develop custom user interfaces without the need for a C# development environment or compiler.

 

In our Processing example we will allow the user to draw an image using their mouse. The image will be drawn in the GUI created by the Processing code.

To generate a simple GUI that allows you to draw a shape please add the following code to your sketch:

 


image

 

Later in the week we will show you how to take a drawing or selected image and then display that on an LED matrix using your Pioneer kit. 

 

Hardware Connections:

 

This is a software only example. Later in the week we will show users how to interface Processing with the Pioneer kit.

 

Test Your Project:

 

Download and setup your Processing environment. Run the Sketch and begin drawing your example.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
1832.Project Images.zip
  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 13 years ago

    Hi Matt,

     

    I have been meaning to play with Processing for some time.

    Now that you are showing off some of its features I might get ambitious, or find some time, to play with it more seriously.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    DAB,

    Processing is extremely cool. It is easy to learn, cross-platform, text-only (hence copy-pastable), has a ton of examples and allows creating application (.exe) files. Importantly, using Processing, one can begin integrating hardware with software.

    This is the direction the world is moving now, and adding a User Interface (UI) to even a simple LED dimmer is powerful.

     

    Today's example shows how to make a simple 'RGB (+ white) Drawing Pad', though with a little more effort, one can make a slightly more generic drawing pad like that shown below.

    image

    As Matt said, later this week, we will show how to make such drawings real-time simultaneously on the computer screen and an RGB-LED-Matrix (http://www.adafruit.com/products/420) driven by the PSoC.

     

    There are quite a few other LED-related demos coming up as well, so, keep an eye out!

    Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    DAB,

    Processing is extremely cool. It is easy to learn, cross-platform, text-only (hence copy-pastable), has a ton of examples and allows creating application (.exe) files. Importantly, using Processing, one can begin integrating hardware with software.

    This is the direction the world is moving now, and adding a User Interface (UI) to even a simple LED dimmer is powerful.

     

    Today's example shows how to make a simple 'RGB (+ white) Drawing Pad', though with a little more effort, one can make a slightly more generic drawing pad like that shown below.

    image

    As Matt said, later this week, we will show how to make such drawings real-time simultaneously on the computer screen and an RGB-LED-Matrix (http://www.adafruit.com/products/420) driven by the PSoC.

     

    There are quite a few other LED-related demos coming up as well, so, keep an eye out!

    Antonio