Cypress Kits
  • Products
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 38 subscribers
  • Views 8068 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP

cy.wbz
cy.wbz over 12 years ago

Hello!


In today’s example we are including a demonstration project for supporting Audio playback and audio recording using USB digital audio. The PSoC 5LP communicates with any USB host, provides a high-quality recording interface to it, and extras high-quality digital audio from the USB host. In this example we show the PSoC 5LP device communicating to:

  • Windows
  • Mac
  • Linux
  • Android
  • Raspberry Pi
  • BeagleBone Black
  • Android
  • iOS



image


This example project utilizes the PSoC 5LP device on the PSoC 4 Pioneer Kit. This example has the following features:

  • Audio-out (I2S)
  • Audio-in (PDM Mic)
  • USB Host Interface
  • Volume Control
  • Watchdog


The firmware was designed and tested with PSoC Creator 2.2 SP1.


Forum Post Attachments:


At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Project Images
  • Example Documentation


Components Used:


The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • I2C
  • EZI2C
  • SPI
  • UART


Firmware Description:


The main.c firmware is included in the example project. Please review the commented sections for more details.


Attached to this example project is a detailed example description. In this file we include a detailed write up of the external hardware used in the example, the internal firmware architecture, and how to recreate the system on your own. Please feel free to review this document for a detailed understanding of how the example is designed and used.


We are also listing the custom components, hardware, and firmware files necessary to create this example. Please feel free to download the zip file for more information.


Hardware Connections:


The hardware connections are detailed in the attached zip project. We include the codec board schematics in the documentation folder.


Test Your Project:


Please see the below image of the example in action.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I hope this example can help you in your design.

Best,

Matt

Attachments:
imagePioneerKit_P5LP_USB_Audio_UserGuide.pdf
PioneerKit_P5LP_USB_Audio.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +3
    The PSoC 5LP USB Audio example project offers a great way to do a general USB Audio solution. Here, I would like to add that if somebody is looking particularly for native MFi USB audio solution for Apple…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    The PSoC Creator project attached to the original post doesn't work with PSoC Creator 3.0 SP1 (It was build with PSoC Creator 2.2 SP1). I have made minimal changes to the original project (updated Cy_boot…
  • greatunclebulgaria
    greatunclebulgaria over 12 years ago +1
    Matt, Thanks for this post, looks very interesting, BUT I'm having trouble with the hardware connections. POSC4 P5LP header Pin POSC4 P5LP header Name AK4556 J6 Header AK4556 Pin Number CS42L51 CS42L51…
  • cy.gul
    cy.gul over 11 years ago in reply to e14 Contributor

    hold down the reset button on the kit while plugging it into USB.

    the status LED on the board goes to a blinking state, indicating that you have entered bootloader mode.

    after this you should be able to see the correct PID in the Bootloader Host Tool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Who are have datasheet of PDM_CIC ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Can there anybody tell me where to buy the overall package of "PSoC 4 Pioneer Kit Community Project#102"? Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    http://lmgtfy.com/?q=PSoC+4+Pioneer+Kit+

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57

    Hi Martins,

     

    Thanks for your feedback!

    However, I need to buy the whole package inside the top chart of arthur's article. Is there any dedicated shop?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    The audio codec board is limited availability (Prototype). After a quick Google I found Audio Codec PROTO - Development Board with WM8731 Audio Codec which I think does all you are doing with the codec, and is available on a development board in the States for $19?!?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • alwynallan
    alwynallan over 11 years ago in reply to alwynallan

    I solved this problem with help from Pavan at Cypress:

    Which component version you are updating to ? If it is v2.7, please do the below modification.

    This is because we have added a workaround for a known issue. But in v2.7, it is fixed in the component itself.

     

    1)      Go to file – “USBiAP_episr.c”

    2)      Search for Interrupt function – “USBiAP_ARB_ISR”

    3)      Comment out the lines of code available inside comment section –

    /* `#START ARB_BEGIN_USER_CODE` Place your code here */

     

    /* `#END` */

    4)      Comment out the #endif available inside comments –

    /* `#START ARB_END_USER_CODE` Place your code here */

    // #endif

    /* `#END` */

     

    5) Build the project your project should work with USB component version 2.7.

    That file is one of hundreds in the "Generated Source" folder.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    I got Error with USB boot loader when using the  CY8CKIT-059CY8CKIT-059 PSOC-059 PSoc

    Please help to have Bootloader on the PSOC 5LP Prototype board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cmydlarz
    cmydlarz over 10 years ago

    Im using a slightly edited version of the provided example code built to run on the CY8C5667LTI-LP009 MCU. I have a custom board using a PDM output digital mic running into the MCU. I programmed the MCU using the MiniProg3 over SWD with the Cypress Programmer 3.23.1 and it all seemed to go smoothly. However, when I plug in the board via USB to a mac or PC the thing doesn't enumerate. Does anyone have any nuggets of info on why this might be happening?

     

    Is there some special way to program the MCU so that it will enumerate as a USB audio device or should it work when programmed the way I mention?

     

    Any help would be much appreciated and virtual beer tokens can be sent!

     

    Charlie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cyaniccypher
    cyaniccypher over 9 years ago in reply to e14 Contributor

    I was able to get this to work, but what needs to be done to get 96kHz and 24bit, I am only able to get up 48khz sampling rate. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>