Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Blink LED-while loop
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 27 subscribers
  • Views 1066 views
  • Users 0 members are here
Related

Blink LED-while loop

e14 Contributor
e14 Contributor over 12 years ago

I'm trying to Blink and LED while Im holding a switch on the board, my initial code for blinking when the switch is on works fine. but now I'm trying to blink it while I'm holding the switch here is what I have for code, Can any one help point out where my error is, Thanks

 

 

#include <project.h>

int main()

{

   

    uint8 SW_Stat; 

  

    for(;;)

    {

     

       

        SW_Stat=(SW1_Read());

        while(SW_Stat==1)

            LED_Write(1);

            CyDelay(500);

            LED_Write(0);

            CyDelay(350);

            LED_Write(1);

            CyDelay(260);

        return 0;

       

        }

}

  • Sign in to reply
  • Cancel
  • jw0752
    0 jw0752 over 12 years ago

    Hi Jad,

    I am not real familiar with this particular language but it looks like you may want to turn off the LED before you leave the while loop. Then you will always start with it off instead of on.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago

    There are several problems.

     

    First, the C compiler doesn't care about indentation.  It only cares about braces.  So your code:

     

    while(SW_Stat==1)

          LED_Write(1);

          CyDelay(500);

          LED_Write(0);

          CyDelay(350);

          LED_Write(1);

          CyDelay(260);

     

    is going to be interpreted as:

     

    while (SW_Stat==1) {LED_Write(1);}

    CyDelay(500);

    LED_Write(0);

    CyDelay(350);

    LED_Write(1);

    CyDelay(260);

     

    That is, the body of the while loop is the single statement LED_Write(1).

     

    The second problem is that LED_Write(1) doesn't affect SW_Stat, so once SW_Stat == 1, the while loop will never end and the LED will be stuck on.

     

    The third problem is that "return 0" exits main(), ending execution.  Usually embedded programs are infinite loops and execute until someone powers off the device or hits the reset button.  So you don't usually return from main().

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer