Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Bluetooth Version V 2.0
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 26 subscribers
  • Views 435 views
  • Users 0 members are here
Related

Bluetooth Version V 2.0

e14 Contributor
e14 Contributor over 11 years ago

I received an example #30 from Cypress. It helped a great deal. Now I am trying to receive data from a warless device that sends serial strings. I am not sure how to rewrite the following code for Cypress module. I have to send 0x020 to turn the remote device on and I do need to pair the devices?

 

 

///////////////////////////////////////////////////////////////
// Arduino Bluetooth Interface with Mindwave
// Sophi Kravitz edit 11-4
// Shane Clements edit 11-5
////////////////////////////////////////////////////////////////////////
#include <SoftwareSerial.h>     // library for software serial
SoftwareSerial mySerial(5, 6);  // RX, TX
int LED = 8;                    // yellow one
int LED1 = 7;                   //white one
int BAUDRATE = 57600;

// checksum variables
byte payloadChecksum = 0;
byte CalculatedChecksum;
byte checksum = 0;              //data type byte stores an 8-bit unsigned number, from 0 to 255
int payloadLength = 0;
byte payloadData[64] = {0};
byte poorQuality = 0;
byte attention = 0;
byte meditation = 0;

// system variables
long lastReceivedPacket = 0;
boolean bigPacket = false;
boolean brainwave = false;
void setup() {
  pinMode(LED, OUTPUT);
  pinMode(LED1, OUTPUT);
  digitalWrite(LED, HIGH);   // hello sequence
  delay(100);
  digitalWrite(LED, LOW);
  delay(100);
  Serial.begin(57600);       // Bluetooth
  delay(500);
  mySerial.begin(4800);      // software serial
  delay(500);
  mySerial.print("Communicating... ");
  mySerial.println();
}
byte ReadOneByte() {
   int ByteRead;
  // Wait until there is data
  while(!Serial.available());
  //Get the number of bytes (characters) available for reading from the serial port.
  //This is data that's already arrived and stored in the serial receive buffer (which holds 64 bytes)
  ByteRead = Serial.read();
  return ByteRead; // read incoming serial data
  }

unsigned int delta_wave = 0;
unsigned int theta_wave = 0;
unsigned int low_alpha_wave = 0;
unsigned int high_alpha_wave = 0;
unsigned int low_beta_wave = 0;
unsigned int high_beta_wave = 0;
unsigned int low_gamma_wave = 0;
unsigned int mid_gamma_wave = 0;

void read_waves(int i) {
  delta_wave = read_3byte_int(i);
  i+=3;
  theta_wave = read_3byte_int(i);
  i+=3;
  low_alpha_wave = read_3byte_int(i);
  i+=3;
  high_alpha_wave = read_3byte_int(i);
  i+=3;
  low_beta_wave = read_3byte_int(i);
  i+=3;
  high_beta_wave = read_3byte_int(i);
  i+=3;
  low_gamma_wave = read_3byte_int(i);
  i+=3;
  mid_gamma_wave = read_3byte_int(i);
}

int read_3byte_int(int i) {
  return ((payloadData[i] << 16) + (payloadData[i+1] << 8) + payloadData[i+2]);
}

void loop() {
  // Look for sync bytes
  // Byte order: 0xAA, 0xAA, payloadLength, payloadData,
  // Checksum (sum all the bytes of payload, take lowest 8 bits, then bit inverse on lowest
if(ReadOneByte() == 0xAA) {
if(ReadOneByte() == 0xAA) {
payloadLength = ReadOneByte();
if(payloadLength > 169) //Payload length can not be greater than 169
return;
payloadChecksum = 0;
      for(int i = 0; i < payloadLength; i++) {      //loop until payload length is complete
        payloadData[i] = ReadOneByte();             //Read payload
        payloadChecksum += payloadData[i];
      }
      checksum = ReadOneByte();                     //Read checksum byte from stream
      payloadChecksum = 255 - payloadChecksum;      //Take one’s compliment of generated checksum
      if(checksum == payloadChecksum) {
        poorQuality = 200;
        attention = 0;
        meditation = 0;
}
     brainwave = false;
     for(int i = 0; i < payloadLength; i++) { // Parse the payload
          switch (payloadData[i]) {
          case 02:
            i++;
            poorQuality = payloadData[i];
            bigPacket = true;
            break;
          case 04:
            i++;
            attention = payloadData[i];
            break;
          case 05:
            i++;
            meditation = payloadData[i];
            break;
          case 0x80:
            i = i + 3;
            break;
          case 0x83:                         // ASIC EEG POWER INT
            i++;
            brainwave = true;
            byte vlen = payloadData[i];
            //mySerial.print(vlen, DEC);
            //mySerial.println();
            read_waves(i+1);
            i += vlen; // i = i + vlen
            break;
          }                                 // switch
        }                                   // for loop

        if(bigPacket) {
          if(poorQuality == 0){
          }
          else{                             // do nothing
           }
         }


            if(brainwave && attention > 0 && attention < 100) {
            mySerial.print("Attention value is: ");
            mySerial.print(attention, DEC);
            mySerial.println();
            mySerial.print("Delta value is: ");
            mySerial.print(delta_wave, DEC);
            mySerial.println();
            mySerial.print("Theta value is: ");
            mySerial.print(theta_wave, DEC);
      mySerial.println();
            mySerial.print("Low Alpha value is: ");
            mySerial.print(low_alpha_wave, DEC);
            mySerial.println();
            mySerial.print("High Alpha value is: ");
            mySerial.print(high_alpha_wave, DEC);
            mySerial.println();           
            mySerial.print("Alertness value1 is: ");
            mySerial.print(low_beta_wave, DEC);
            mySerial.println();
            mySerial.print("Alertness value2 is: ");
            mySerial.print(high_beta_wave, DEC);
            mySerial.println();          
            mySerial.print(low_gamma_wave, DEC);
            mySerial.println();
            mySerial.print(mid_gamma_wave, DEC);
            mySerial.println();
         }

          if(attention > 40){
            digitalWrite(LED1, HIGH);
          }
          else
            digitalWrite(LED1, LOW);
        }
        }
      }

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    pnielsen3

    With the many Cypress examples, why start off for one using Arduino? Too many differences to mention.

    Clem

    PS. The Arduino code goes into the Arduino IDE which cannot flash Cypress hardware. You need to use PSoC Creator IDE instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    pnielsen3

    With the many Cypress examples, why start off for one using Arduino? Too many differences to mention.

    Clem

    PS. The Arduino code goes into the Arduino IDE which cannot flash Cypress hardware. You need to use PSoC Creator IDE instead.