Atmel Xplained Boards
  • Products
  • Dev Tools
  • Atmel Xplained Boards
  • More
  • Cancel
Atmel Xplained Boards
Forum SAMA5D4 ADC driver - do you know a Linux image that has the driver?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Atmel Xplained Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 6 subscribers
  • Views 3813 views
  • Users 0 members are here
Related

SAMA5D4 ADC driver - do you know a Linux image that has the driver?

Jan Cumps
Jan Cumps over 11 years ago

For the Enchanted Objects Design ChallengeI'm trying to get the ADC Hardware Trigger mechanism working.


I have difficulties with the ADC driver. I am unsure if the 4.7 and 4.6 linux Yocto Poky images have that driver installed.


I have 3 questions :


Is the ADC driver for the sama5d4 included in those Yocto Poky images?

If yes, what's the name of the driver (is it at91_adc)?

If no, is there an image around with the ADC included, or is there a way to get the driver installed on my board running that Yocto Poky image?

 

Here's the blog post that shows what I'm dong: Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2

 

I have issues when the buffer read tool generic_buffer tries to load the driver:

 

Here's where the code fails:

 

    /* Find the device requested */  
    dev_num = find_type_by_name(device_name, "device");  
    if (dev_num < 0) {  
        printf("Failed to find the %s\n", device_name);  
        ret = -ENODEV;  
        goto error_ret;  
    }  
    printf("iio device number being used is %d\n", dev_num); 

 

Error

Failed to find the at91_adc

  • Sign in to reply
  • Cancel

Top Replies

  • noglitch
    noglitch over 11 years ago in reply to Jan Cumps +1 suggested
    Hi, Due to move to DT, the device name has changed. It is now "fc034000.adc" for this device. So, your command line should be: ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2 It seems…
  • noglitch
    noglitch over 11 years ago +1 verified
    FYI, I've just updated the Linux4SAM.org page: http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver to reflect the changes in naming brought by a Device Tree system.
  • noglitch
    noglitch over 11 years ago in reply to Jan Cumps +1
    Oh thanks for the typo correction. I use the Linux4SAM 4.7 kernel + rootfs image. I took the generic_buffer.c file in the linux-3.18-at91 kernel and compiled it with a Code Sourcery toolchain (Sourcery…
  • Workshopshed
    0 Workshopshed over 11 years ago

    Top work by noglitch and Jan Cumps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<