Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog 17 DOF Humanoid
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: _vishaladitya
  • Date Created: 29 Dec 2016 12:57 AM Date Created
  • Views 2450 views
  • Likes 3 likes
  • Comments 1 comment
  • servo board
  • arduino uno
  • raspberrypi.
  • biped robot
  • robotics
  • humanoid robot
  • servo motores
  • 17 dof
  • robokits
Related
Recommended

17 DOF Humanoid

_vishaladitya
_vishaladitya
29 Dec 2016
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
Objective

The objective of this project is to focus in R&D ofAI & Machine Learning

Brief

This robot is a professional small humanoid robot consist of full aluminum parts, smooth surface with smooth edges not hurting hands, the metal is unbleached, beautiful and durable. The High Torque Standard Servo Motor with Dual Ball Bearing and Metal Gears. Provides 14kg/cm at 4.8V and 16kg/cm at 6V. Replacement for HS-645MG. Arduino Uno R3 based USB 18 Servo Controller is ideal for making Autonomous and PC based systems which run over Hobby Servo motors. The software helps to develop the complex sequences in real time on the hardware like robotic arms, walkers, bipeds and any other servo controlled system. It also generates Arduino based code for the developed sequence which can be deployed on the controller on board thereby making the robot autonomous.

Features

 

  • Arches punching, corner cutting
  • Cost-effective and easy-to-use
  • For hobbyists, robot competition, kids
  • Size:40cm(H)*23cm(W)

Servo Motor Specifications

  • Required Pulse: 3-5 Volt Peak to Peak Square Wave
  • Operating Voltage: 4.8-6.0 Volts
  • Operating Temperature Range: -10 to +60 Degree C
  • Potentiometer Drive: Indirect Drive
  • Gear Type: All Metal Gears
  • Connector Wire Length: 12"
  • Dimensions: 1.6" x 0.8"x 1.4" (41 x 20 x 36mm)
  • Weight: 48gm

Initial Timeline

  • Stage I - Develop autonomous humanoid with all basic features like walking, dancing, follow, track co-ordinates, manual control using GUI.
  • Stage II - Image Processing to track in real-time objects using harcascades, machine learning algorithms to make it more intelligent.
  • Stage III - Voice Recognition to give commands and perform basic tasks.
  • Stage IV - Completely autonomous humanoid to interact with users & environment that can make decisions like self-driving cars.

This is just an initial time line and not enough detail is known to provide a better time estimate. These steps may not be carried out in the same order as they appear above either and a more iterative approach is likely to be used.

Conclusion and Future Scope

  • Machine Learning: Help students to learn & implement ongoing researches.
  • Learning by demonstration.
  • Language Acquisition.
  • Gestural Communication.
  • Advance features inspired from NAO, ASIMO, etc. at cheap costs.
  • Virtual Reality Controls.

PROJECT HANDLE:

  1. Vishal Aditya - B.Tech CSE (2013-2017)
  2. Vamishi Reddy - B.Tech CSE (2013-2017)

REFERENCES:

  • 17 DOF Humanoid by Robokits

 

Website: https://raiot-aur.github.io/raiot/17dofhumanoid.html

adminChristyZRoboticsArduinoMembers

  • Sign in to reply
  • mikeyc33
    mikeyc33 over 9 years ago

    Is there any one who has available code for this biped please , perhaps a lot to ask but ive been around all program forums i.e arduino cc and node mcu on github but noone has any sort of control software for this biped robot. I understand there is a lot involved and would be happy with some hints or info on which controllers are best for this biped as im trying to use botboarduino with little joy as my coding skills are minimal at present so any help will be great