Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog A File Cloaking Utility for Secure Transport or Backup
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 7 Sep 2016 8:46 PM Date Created
  • Views 567 views
  • Likes 0 likes
  • Comments 0 comments
  • rhein dale
  • cryptography
  • password_protection
  • rijndael
  • aes-256
  • cloaking
  • tiff
  • raspberry pi
  • aes
  • password-based encryption
  • authentication
  • pbkdf2
  • crypto
  • iot
  • c programming
  • cryptoauthentication
  • sha-512
  • feature_tutorial
Related
Recommended

A File Cloaking Utility for Secure Transport or Backup

e14 Contributor
e14 Contributor
7 Sep 2016

On github, I created a "File Cloaking Utility" (https://github.com/texadactyl/cloaking) that provides password-based security for a single file or a single file system archive file.  The utility is probably most useful in the following situations:

  • Storing backups of sensitive information on the Internet
  • Transporting sensitive information electronically (E.g. email) or manually (E.g. using a flash drive)

 

This project is already proven running on an Intel/AMD environment (Biostar Celeron CPU motherboard) and the Raspberry Pi 2 (ARM 32-bit processor).  I must confess that the choice of C or C++ brought incompatibility nuisances across CPU architectures - all solved - but underscores the reasons why folks have adopted higher-level languages or, at least, to a language which abstracts data physical sizes more efficiently.

 

In terms of development, this project is based on libgcrypt (GnuPG cryptographic library), using:

  • Password-based Key Derivation Function version 2 (PBKDF2)
  • AES data cryptography in Cipher-Block Chaining (CBC) mode
  • Hash-based Message Authentication Code (HMAC) function SHA512

 

Reference: https://gnupg.org/documentation/manuals/gcrypt/

 

Project subfolders:

  • src - C-language source code and a Makefile
  • bin - Upon completion of the `make` utility, this folder holds the `cloak` and `uncloak` executables.
  • docs - project documentation (admittedly, skimpy)
  • data - project example data files

 

The starting point with this project is in the docs/operations.txt file.  Also, the same note contains commands for cloaking the sample cleartext data and uncloaking the ciphertext.

 

Missing: a GUI interface.  Maybe I'll get around to it someday or a reader would like to contribute one which can front-end C-language executables.

 

Feel free to contact me for inquiries and issues, especially if you find any bugs.  I'll respond as soon as I can.