Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Intel’s SD-sized Edison PC will be slightly larger than expected
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Apr 2014 8:31 PM Date Created
  • Views 940 views
  • Likes 0 likes
  • Comments 5 comments
  • intel
  • portable
  • sbc
  • sd_card
  • cabeatwell
  • edison
  • linux
Related
Recommended

Intel’s SD-sized Edison PC will be slightly larger than expected

Catwell
Catwell
28 Apr 2014

image

Intel Edison PC – the size of an SD card, only bigger (via INTEL)


Intel made headlines in January when it promised the delivery of an SD card-sized personal computer at the 2014 Consumer Electronics Show. The company, however, recently admitted that they overestimated their capabilities. The Edison PC will be “slightly larger” than expected, after all.

 

The chip was initially designed to be the size and shape of an SD card and support a Linux-based PC with WiFi and Bluetooth functionality. It was expected to be built using Intel’s Quark system-on-a-chip, but it unfortunately came up short. Now, the technology giant instead opted for dubbing out the Quark for the 22nm Silvermont dual-core Intel Atom SOC processor, which will give the PC more power and reliable performance, but will inevitably increase the expected size of the tiny PC.

 

The Atom increases the capability of the PC through its dual-threaded, dual-core 500MHz CPU. It has an additional MCU and more than 30 I/O interfaces through 70-pin connectors. It is expected to be far more durable, reliable and powerful that the Quark, the inclusion of which Intel claims it is still working on.

 

The capability of the mini PC was also promising. At the CES Intel portrayed the capability of the product through its “Nursery 2.0” concept, which dressed a baby in a sensor-filled onesie that let Mom know when baby was happy or upset, by displaying information on Mom’s coffee mug. Mom was also able to use the technology to start up baby’s bottle warmer wirelessly so a bottle would be ready as soon as it was needed.

 

While this sounded great, when Intel announced changing the size of the Edison PC, it also announced that it might change its function. When Intel presented the chip, it had wearables in mind. With the technology shift, however, the Edison PC is not very different from chips already available on the market, so the company reported it would change its focus to simplify the design process for the building of an SD form factor.

 

Intel did not announce how much larger the Edison PC will be. Regardless, the chip is still expected to launch this upcoming summer.

 

C

See more news at:

http://twitter.com/Cabe_Atwell


Liked this? Try this

10 useful electronics tutorials from Ben Heck

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago in reply to johnbeetem +2
    Maybe they could build them into a George Forman grill so that you get computing and a good meal along the way. DAB
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Sounds like it's just become http://www.minnowboard.org/meet-minnowboard-max/
  • DAB
    DAB over 12 years ago in reply to johnbeetem

    Maybe they could build them into a George Forman grill so that you get computing and a good meal along the way. image

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    Now an Atom, rather than a Quark... #^&$$ marketing spin on the names there image   Funnily enough some of my thoughts have been about whether it's really a good idea to attach something like this to a baby, probably powered by lipo batteries too... Strikes me as a combination I personally wouldn't want to try.

     

    There's some photos of the new one, but with nothing to compare scale, so very difficult to tell if it's 10% or 200% larger. The new 70 pin high density connector suggests a fairly radical re-design though, and that doesn't strike me as something that happens overnight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to DAB

    DAB wrote:

     

    I never liked terms like slightly, likely and other type of loose adjectives.

     

    I would have preferred that they said 5%, 10% or 25% bigger to let designers have some time lead to adjust their potential application devices.

    < satire >

    Well, maybe they're still trying to figure out how big the package needs to be to dissipate the heat produced by the Quark.  After all, we don't want Baby to be upset because she's catching on fire image  But in other applications you want the package small enough to warm up Baby's bottle image  This is what we call a "tradeoff".

    < /satire >

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    I never liked terms like slightly, likely and other type of loose adjectives.

     

    I would have preferred that they said 5%, 10% or 25% bigger to let designers have some time lead to adjust their potential application devices.

     

    Still, if it delivers the performance, the a slight size increase is probably ok.  Maybe.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Sounds like it's just become http://www.minnowboard.org/meet-minnowboard-max/