Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog ODroid - Oh Boy!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 23 Dec 2014 12:42 AM Date Created
  • Views 13092 views
  • Likes 10 likes
  • Comments 118 comments
  • odroid
  • c1
Related
Recommended

ODroid - Oh Boy!

mconners
mconners
23 Dec 2014

I recently picked up one of these little ODROID C1 development boards and i have to say I couldn't be happier!

 

It's a Quad Core ARM dev board based on the Amlogic S805 Cortex A5 processor with a Dual Core Mali 450 GPU. It comes with 1 GB of RAM and can can boot from 2 sources eMMC and Micro SD. $36.95 US.

 

It's layout looks very similar to the Raspberry Pi+, and it is almost the same size. Here is a picture of the 2 side by side:

 

image

 

Some of the features:

4 USB Host Ports

Micro Usb OTG Port

Micro HDMI Port

Gigabit ethernet over RJ45

IR Receiver (I guess that would be handy for a remote control if using as a streaming device)

40 Pin Expansion Port containing

2 - I2C Ports

Serial Port

19 GPIO Pins

2 ADC inputs

1.8V Analog reference

3.3 V Out

2 5V outputs

1 SPI Output

RTC with available battery backup.

 

A quick look at the pinout for both  the ODROID C1 and the Raspberry Pi shows they seem to match up with the exception of pins 37,38, and 40 on the ODroid are used for ADC.

 

It's also missing a few things the B+ has built in, like the camera interface, composite video out, discrete audio outputs, and the Display header.

 

This board will run Android or Ubuntu 14.04 LTS, both available from the Hardkernel site.

Installation of the Ubuntu image was a breeze, simply download it, dd the image to a Micro SD card, and boot. Detailed instructions are available on the Hardkernel site.

 

There is a root user and an odroid user, both seem to use the password odroid.

 

The Hardkernel site (as well as their US distributor) have a wide selection of inexpensive accessories for the odroid.

I was foolish and didn't purchase the power supply, which turned out to require a very small connector which was difficult to find. I was able to cobble together a plug using a Radio Shack Adaptaplug socket, a type A (2.5 mm) Adaptaplug tip, and an old phone charger I had lying around. But it would have been cheaper and easier to have purchased it initially from Ameridroid.

 

I did purchase the tinkerers kit which included a breadboard, a breakout board for the GPIO port, a ribbon cable, a bunch of resistors (like 100 or so, I didn't count), 6 tactile buttons, about a dozen LED's in rd green and yellow,  a Photocell sensor, and a bunch of connection wires.

 

The fact that it runs a modern version of Ubuntu makes me happy, the 14.04 LTS version is from April 2014 and since it is an LTS release it will be supported for several years. I run Ubuntu on my main computer and all my laptops, plus my RIoT Board so this thing will fit right in.

 

In conclusion I just have to say this is a great board, and for $35 US, it's tough to beat. My only words of caution are

1) Buy the power supply, it's worth it, or at least the pigtail connector they sell

2) Look on their site to see the limitations on Micro SD cards, they have some that perform better than others, I had one of the poor performers, it works but it is slow on boot

3) If you need a console, buy their USB uart module, they have a goofy molex connector for serial

 

Other than that, I can't complain.

  • Sign in to reply

Top Comments

  • mconners
    mconners over 11 years ago in reply to mconners +3
    With all four cores blazing, it only got up to about 35C. I'm not sure the heat sink is necessary. Mike
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +3
    Droid-C1 ordered, along with PSU, Serial Cable and HDMI adapter, now the few days of waiting begins , Oh and an LCD display (Why not) I looks like your all getting this thing to perform quite nicely so…
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem +3
    Yes you are (H)alting the Odroid rather than also calling the power off so the power remains on to complete your USB transaction no doubt!! good solution ...nice and easy
  • mconners
    mconners over 11 years ago in reply to mconners

    I work from home, so I have a pair of Microsoft Life Chat Headphones that I use for conference calls and pairing with my co workers. Just for fun, I plugged them into the C1. Recognized them right away. Now I'm listening to blues traveler on amazon music, works great.

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 11 years ago in reply to johnbeetem

    John Beetem wrote:


    ... and I'm back!  I deleted "console=ttyS0,115200n8 " from boot.ini and rebooted.  This does indeed send a bunch of boot messages to HDMI (just like raspbian in case you're nostalgic).  The messages blasted past too quickly to be useful.  Instead of stopping at an error, it simply completed the boot process and I'm running v1.2 off the hard drive.

     

    So either it booted properly by coincidence or it previously required console input as Mike stated upstream, and removing "console=ttyS0,115200n8 " eliminated that hitch.  For now, I'm just going to keep using my C1 as my main computer and see if it is now stable.  In any case, if it hangs I may see a useful message on HDMI.


    Thank you all (especially Mike) for your suggestions!

     

    After updating to 1.3 and rebooting I noticed a bunch of messages scrolling on HDMI without making any changes. I was preoccupied with something else and just briefly caught it out of my eye so I'm not sure if they were shutdown messages, reboot messages, or whatever else, but it was the first time I had witnessed that behavior. Usually the HDMI screen would just go blank.

     

    It does boot fast, that's for sure. From the reboot command to re-login is like 20 seconds.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 11 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Another subtopic: when I move windows around the desktop with v1.1 or v1.2, it's very slow with lots of inertia: that is, the window slowly follows the mouse and catches up after I stop moving.  I couldn't find any preference option to change this behavior.

     

     

     

    I've noticed similar behavior. It hasn't bothered me enough to fix it yet. Or at least look for a fix.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    Another subtopic: when I move windows around the desktop with v1.1 or v1.2, it's very slow with lots of inertia: that is, the window slowly follows the mouse and catches up after I stop moving.  I couldn't find any preference option to change this behavior.

     

    Are others having the same behavior?  Otherwise the graphics are pretty quick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to johnbeetem

    johnbeetem wrote:


    Maybe I just have a bad SD card or hard drive.  Poking around at the ODROID forum I did learn that you can display console messages on HDMI by deleting "console=ttyS0,115200n8 " from boot.ini.  I'll give that a try and see if I can learn something.

    ... and I'm back!  I deleted "console=ttyS0,115200n8 " from boot.ini and rebooted.  This does indeed send a bunch of boot messages to HDMI (just like raspbian in case you're nostalgic).  The messages blasted past too quickly to be useful.  Instead of stopping at an error, it simply completed the boot process and I'm running v1.2 off the hard drive.

     

    So either it booted properly by coincidence or it previously required console input as Mike stated upstream, and removing "console=ttyS0,115200n8 " eliminated that hitch.  For now, I'm just going to keep using my C1 as my main computer and see if it is now stable.  In any case, if it hangs I may see a useful message on HDMI.


    Thank you all (especially Mike) for your suggestions!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>