Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog ODroid - Oh Boy!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 23 Dec 2014 12:42 AM Date Created
  • Views 12502 views
  • Likes 10 likes
  • Comments 118 comments
  • odroid
  • c1
Related
Recommended

ODroid - Oh Boy!

mconners
mconners
23 Dec 2014

I recently picked up one of these little ODROID C1 development boards and i have to say I couldn't be happier!

 

It's a Quad Core ARM dev board based on the Amlogic S805 Cortex A5 processor with a Dual Core Mali 450 GPU. It comes with 1 GB of RAM and can can boot from 2 sources eMMC and Micro SD. $36.95 US.

 

It's layout looks very similar to the Raspberry Pi+, and it is almost the same size. Here is a picture of the 2 side by side:

 

image

 

Some of the features:

4 USB Host Ports

Micro Usb OTG Port

Micro HDMI Port

Gigabit ethernet over RJ45

IR Receiver (I guess that would be handy for a remote control if using as a streaming device)

40 Pin Expansion Port containing

2 - I2C Ports

Serial Port

19 GPIO Pins

2 ADC inputs

1.8V Analog reference

3.3 V Out

2 5V outputs

1 SPI Output

RTC with available battery backup.

 

A quick look at the pinout for both  the ODROID C1 and the Raspberry Pi shows they seem to match up with the exception of pins 37,38, and 40 on the ODroid are used for ADC.

 

It's also missing a few things the B+ has built in, like the camera interface, composite video out, discrete audio outputs, and the Display header.

 

This board will run Android or Ubuntu 14.04 LTS, both available from the Hardkernel site.

Installation of the Ubuntu image was a breeze, simply download it, dd the image to a Micro SD card, and boot. Detailed instructions are available on the Hardkernel site.

 

There is a root user and an odroid user, both seem to use the password odroid.

 

The Hardkernel site (as well as their US distributor) have a wide selection of inexpensive accessories for the odroid.

I was foolish and didn't purchase the power supply, which turned out to require a very small connector which was difficult to find. I was able to cobble together a plug using a Radio Shack Adaptaplug socket, a type A (2.5 mm) Adaptaplug tip, and an old phone charger I had lying around. But it would have been cheaper and easier to have purchased it initially from Ameridroid.

 

I did purchase the tinkerers kit which included a breadboard, a breakout board for the GPIO port, a ribbon cable, a bunch of resistors (like 100 or so, I didn't count), 6 tactile buttons, about a dozen LED's in rd green and yellow,  a Photocell sensor, and a bunch of connection wires.

 

The fact that it runs a modern version of Ubuntu makes me happy, the 14.04 LTS version is from April 2014 and since it is an LTS release it will be supported for several years. I run Ubuntu on my main computer and all my laptops, plus my RIoT Board so this thing will fit right in.

 

In conclusion I just have to say this is a great board, and for $35 US, it's tough to beat. My only words of caution are

1) Buy the power supply, it's worth it, or at least the pigtail connector they sell

2) Look on their site to see the limitations on Micro SD cards, they have some that perform better than others, I had one of the poor performers, it works but it is slow on boot

3) If you need a console, buy their USB uart module, they have a goofy molex connector for serial

 

Other than that, I can't complain.

  • Sign in to reply

Top Comments

  • mconners
    mconners over 11 years ago in reply to mconners +3
    With all four cores blazing, it only got up to about 35C. I'm not sure the heat sink is necessary. Mike
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +3
    Droid-C1 ordered, along with PSU, Serial Cable and HDMI adapter, now the few days of waiting begins , Oh and an LCD display (Why not) I looks like your all getting this thing to perform quite nicely so…
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem +3
    Yes you are (H)alting the Odroid rather than also calling the power off so the power remains on to complete your USB transaction no doubt!! good solution ...nice and easy
  • mconners
    mconners over 11 years ago in reply to johnbeetem

    I just did

     

    apt-get update && apt-get dist-upgrade && apt-get upgrade

    To upgrade to v1.3, rebooted fine.I'm now running kernel 3.10.67-61

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to mconners

    Michael Conners wrote:

     

    I downloaded the 20150120 image, if that means anything. It is from the V1.2 page, but the lsb-release says it is Ubuntu 14.04.1

    That's the v1.2 I'm using.  I think the only way to tell is to get a directory listing of the boot partition and look at the dates.  Maybe I just have a bad SD card or hard drive.  Poking around at the ODROID forum I did learn that you can display console messages on HDMI by deleting "console=ttyS0,115200n8 " from boot.ini.  I'll give that a try and see if I can learn something.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 11 years ago in reply to johnbeetem

    I downloaded the 20150120 image, if that means anything. It is from the V1.2 page, but the lsb-release says it is Ubuntu 14.04.1

     

    I downloaded it from here http://odroid.com/dokuwiki/doku.php?id=en:c1_ubuntu_release_note_v1.2

     

    BTW, I just noticed there is a 1.3 release.

     

    I did a sudo apt-get update and sudo apt-get upgrade and rebooted fine afterwards.

     

    Since I started with a fresh image, I'm reconfiguring and reinstalling some of the extra packages I had installed on my previous install.

     

    I did notice that the boot.ini has quite a few more screen resolutions this time around.

     

    Mine seems to be up and running ok.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to mconners

    Michael Conners wrote:

     

    I just set up my system to boot from sd and mount the hd (ssd)...

    Thanks for the details.  That's pretty much what I did, using fdisk instead of parted for removing the SD card's second partition.  I also added "conv=fsync" to the dd commands, since Hardkernel says to do that elsewhere.  I also did multiple sync commands to make sure everything got written.

     

    Incidentally, which Hardkernel version are you running with the USB HDD?  I'm trying to do this with v1.2, and it's not stable for me.

     

    One thing that bothers me is that when I shutdown the ODROID-C1 turns off USB HDD power as its activity LED is blinking.  I'm wondering if ODROID-C1 is turning off USB power a bit too soon.  I'd try unmounting it before shutdown, but that's hard if the file system is on that HDD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to johnbeetem

    johnbeetem wrote:

     

    Well, now I'm having trouble with software updates.  Like a good user, I requested the software updates with the button at the bottom of the screen.  That managed to screw up both the hard drive and my 2GB boot SDcard.  So I re-imaged them and tried again.  1440x900 came up fine this time, so I ran ODROID utility as I did yesterday.  Well, that screwed up the hard drive (but not the boot SDcard).  So once more I re-imaged the hard drive and now it's OK.  I suspect I updated with unstable software.  I'm going to see what they have about this at the ODROID forum.

    It's still not stable.   The v1.2 with 2 GB SD card for the boot partition and HDD for the file system failed when I rebooted this evening.  No idea why, so I guess I need to use the serial console as Mike suggests.  However, then I need a different computer to run as a terminal emulator, so why not just use that computer as my main computer?

     

    The v1,1 SD card works pretty well, so I'm using it now.  However, I don't like the odds of using an SD card as the main file system -- I'd really prefer a real hard drive.  I think I'll watch the ODROID forum for a while and see if other people are having similar problems.  That and get the parts to make my own serial cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>