Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Parallella - The 64-core mini-computer works in tandem with ARM Cortex-A9
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 26 Apr 2013 6:34 PM Date Created
  • Views 1400 views
  • Likes 3 likes
  • Comments 4 comments
  • research
  • minicomputer
  • kickstarter
  • parallella
  • embedded
  • raspberry_pi
  • cabeatwell
  • prototyping
  • dev
  • adapteva
  • innovation
  • communication
Related
Recommended

Parallella - The 64-core mini-computer works in tandem with ARM Cortex-A9

Catwell
Catwell
26 Apr 2013

image

Parallella Main-board (via Adapteva & Kickstarter)

 

The company Adapteva is currently testing one of their last prototypes of a tiny parallel computer board they are calling Parallella, which you are surely to hear about. This mini computer has reached a speed of 90 GFLOPS using just 5 watts urging some to call this a mini supercomputer. Kickstarter supporters are on pace to get their Parallella during the summer this year.

 

The main principles behind the Parallella mission are to have open access and share open source information on parallel processing while offer the board at an affordable price and “democratizing the access to parallel supercomputing”. The company sees processing in parallel as the future of computing and many would agree.

 

At the core of the device is the energy efficient Epiphany multi-core accelerators produced by Adapteva. The “45 GHz model” (The performance of a system at that speed) has a 64-core accelerator tied to a dual-core ARM Cortex-A9, 1 GB of RAM, microSD slot, two USB 2.0 ports, 10/100/1000 Ethernet port and an HDMI port. All of this is packed in a dev board that fits in your pocket comfortably. Another model uses a 13GHz 16-core accelerator capable of 26 GFLOPS.

 

image

Concept of the Main-board Parallella connected to the Epiphany multi-core accelerator 64 core edition (via Adapteva)

 

The Epiphany multi-core chips are composed of an array of reduced instruction set computing (RISC) chips, whose simple design allows for faster processes. This scalable array is programmed using C or C++ and they communicate between each other using a network embedded in the chips but share the one memory architecture. The Parallella operating system will be Ubuntu 12.04 and the team’s next goal, before release, is getting Linux to boot on the device. 

 

The board hardware schematics and the SDK will be released as open source information and Adapteva has already made their device drivers available to the public. They are doing this because their target audience is developers. The faster and more widespread this information becomes, the sooner we can all benefit from the advantages or parallel processing.

 

The uses for this type of devices are pretty endless. Extreme multitasking and performing all sorts of computational tasks will be much more efficient in parallel than using common linear processing. Real-time analysis of markets, registering fingerprints and recognizing faces could be done with this tiny credit card sized computer board. Encryption and code breaking, efficient multi-media storage and playback, handling multiple real-time streams, keeping track of multi-sensor robotics or

tracking objects could be done in a cost effective, energy efficient and timely manner.

 

The time is now to start thinking more simultaneously. The Parallella development board will be available, in its 16-core form first, this summer.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

C

See more news at:

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Problemchild
    Problemchild over 12 years ago in reply to Catwell

    Cabe, this certainly is very interesting for the lo cost Robot Vision Application.

    What I would be very interested in finding out is what is the state of Paralllel processing Algorithms and equally important the code implementation.

    One could very easily implement these on say a CUDA box as an alternative and if there is a wait for delivery you could experiment before the new toy arrives image

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to jamodio

    Jorge,

     

    What is your plan for the Parallella?

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jamodio
    jamodio over 13 years ago

    I'm one of their backers on Kickstarter and very anxious to get the board, it will be a very interesting and cost effective platform for compute intensive applications on the embedded side, among them image processing for face recognition and such.

     

    There are some documents available at Adapteva's website http://www.adapteva.com/ and they are starting to relase some drivers as open source https://github.com/adapteva.

     

    Cheers

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    An interesting idea.

     

    I can see using this approach for image and acoustic processing or any other application where you can really exploit parallel processing.

     

    I am not sure it will make a good internet platform, but with the A9 core processor, it should do very good for normal use.

     

    Game players will love this approach once the game developers learn to use the array of processors.

     

    The key to its success will be the development of useful tools to develop the parallel processing algorithms that can fully exploit the internal capability.

     

    If I can find enough detailed documents on the architecture, I might be able to do a good analysis of the platform and identify any limitations/unexploited capability for the board.

     

    For the money, I can see where the board would be a very interesting system to play with.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down