Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog The ODROID-U2: Smallest, ultra-compact 1.7GHz Quad Core development board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 May 2013 6:47 PM Date Created
  • Views 1969 views
  • Likes 2 likes
  • Comments 13 comments
  • research
  • industry
  • developer
  • hardkernel
  • sbc
  • odroid_u2
  • raspberry_pi
  • cabeatwell
  • development
  • prototyping
  • code
  • developing
  • innovation
  • communication
Related
Recommended

The ODROID-U2: Smallest, ultra-compact 1.7GHz Quad Core development board

Catwell
Catwell
7 May 2013

image

ODROID-U2 on the left... Hardkernel's corporate card on the right? (via Hardkernel)

 

Hardkernel Co, the open-source hardware company from Korea, has achieved quite a bit of success over the years with the release of several of the world’s first Android, ARM-powered development boards. Their latest release, the ODROID-U2, is an upgrade to its U predecessor sporting a 1.7GHz Quad core platform with 2GB of RAM to offer developers an ultra-compact solution with PC-like performance.

 

As the world’s first company to offer quad core processing power in a palm-sized platform, the ODROID-U2 continues the trend with the use of a Samsung Exynos 4412 Prime ARM Cortex-A9 Processor with POP 2GB of LPDDR2 RAM. An integrated Mali-400 quad core GPU running at 440MHz is included in the package complete with a little headroom available for overclocking. A stacked hub design provides two high-speed USB 2.0 ports and a 10/100Mbps Ethernet connection. A micro HDMI connector outputs video at full 1080p, an audio codec provides sound through a 3.5mm headphone jack, and power is supplied via 5V2A DC jack. Memory storage and system booting is performed through the onboard Micro SD slot or the eMMC module.

 

Though limited in on-board feature availability, the ODROID-U2 is meant to provide developers with a simple, ultra compact design for their rapid development needs on a fast and flexible platform. That being said, several modules are available for purchase that will upgrade its on-board features via USB, UART, eMMC, and PWM interfaces such as: cooling fans, a USB to IO expansion board for GPIO/PWM/SPI/UART/12/ADC interfaces, micro HDMI to HDMI cables, bluetooth modules, eMMC memory modules, and WiFi kits. When they say developers, who did they have in mind for such a platform?

 

The ODROID-U2 will also come packaged with a full-enclosable aluminum shield to cover its incredibly compact 48mmx52mm PCB design (59mm x 57mm x 60mm with case). The fully open ODROID-U2 supports Android & Linux Ubuntu with boot-ready micro SDs available for purchase. The price is currently set at $89 from the Korean manufacturer with worldwide shipping options - and as a heads up, you can expect your device to be shipped at least a full-week after the order has been placed.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

C

See more news at:

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    PM=Personal Message image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Problemchild

    John, Yes I will also need an enclosure of some sort.  I do have some questions.  What do you mean by "Pm us"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    Doug, no problem ...remember we do special order enclosures  that include the potential of putting the panel into the same box!

     

    I also have the new XU which is even more wizz image

     

    Pm us if you need to ask anything

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Problemchild

    Hmmm, sounds like hard work.  All that extra hardware seems like it would cancel out the beauty of the small footprint.  What I was hoping to find was something that would plug straight in.  Ho-hum!

     

    EDIT: Ah, OK, I see what you mean about the ODROID X/2.  That's more like it!  There's even a video on the Hardkernel website of almost EXACTLY what I want to do with USB video cams on a board like this!  I've been developing apps on Android for a year or so now, but taking a board like this and bringing it up from the BSP and adding/interfacing hardware like this would be quite new for me - mind if I pick your brains a little on this one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    It only has a micro HDMI if you want to drive a panel directly you either need one of those pannel + HDMI boards you see quite often on EBAY.....(BTW I've got a project on that so check out my Blog when I put it up0

    Failing that you can use the ODROID X/X2 which are much larger but better equiped and have a 50 pin adaptor board for LCD pannel(I have one of thes already ..Works well!)

     

    Finally you could get an ODROID XU which is an oct Core CPU and everything under the roof  I have a pair of these.... AWESOME!!!! Everying including Display port USB3 etc!! ...will be doing a case and a review soon so again check the blog image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>