Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Toyota to Put Platform 2.1 Through its Paces at California’s GoMentum Station
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Nov 2017 9:20 PM Date Created
  • Views 1005 views
  • Likes 1 like
  • Comments 3 comments
  • transportation
  • autonomous
  • artificial intelligence
  • car
  • autonomous_vehicles
  • cabeatwell
  • ai
  • toyota
  • automotive
  • innovation
Related
Recommended

Toyota to Put Platform 2.1 Through its Paces at California’s GoMentum Station

Catwell
Catwell
2 Nov 2017

image

Toyota’s Platform 2.1 autonomous vehicle features two modes- Guardian and Chauffeur. (Image credit Toyota)

 

Last month Toyota unveiled its latest version of their autonomous vehicle- the Lexus-modified (600hL) Platform 2.1, which features better sensors, improved detection and a pair of steering wheels for better human control. The vehicle is a base for Toyota Research Institute’s autonomous research systems known as Guardian and Chauffeur, which provides increased navigation and safety aspects. Chauffeur is based on autonomous Level 4 driving (there are six altogether), which makes the vehicle highly autonomous- designed to perform all safety-critical driving functions and monitors all roadway conditions, however it’s limited to the ODD (Operation Design Domain) and doesn’t cover all driving scenarios.

 

Guardian mode acts as it sounds- a driver-assist system that monitors the environment around the vehicle and alerting drivers when a hazard appears and assists with crash avoidance when necessary. Moreover, it monitors the driver’s eyes using an infrared sensor mounted on the dashboard to detect drowsiness and distraction and acts accordingly when adverse behavior is encountered.

 

As far as the dual steering wheels are concerned, the passenger side acts as a drive-by-wire system for acceleration and breaking as a method for transferring vehicle control between the human driver and autonomous system. Toyota successfully tested both systems on an enclosed track where they performed admirably, but although it was a great demonstration of proof-of-concept, the track doesn’t provide real-world scenarios, in fact, none of them do, but one of them does come close- California’s GoMentum Station.

 

image

GoMentum Station is known for tough, realistic driving conditions and offers 2,100 acres of testing ground with 19.6-miles of paved roads. (Image credit Wing via Wikimedia)

 

GoMentum Station (Concord Naval Weapons Station) is known for its tough, realistic conditions where automobile companies can test their autonomous vehicles without worrying about damaging property, as it’s a closed-off area boasting 5,000 acres with 19.6 miles of paved roadways. The Toyota Research Institute will use the grounds to further test their Platform 2.1 autonomous vehicle, which now includes a new LIDAR system for longer sensing ranges, a denser point-cloud for detecting the position of 3D objects and a larger FOV that’s dynamically configurable.

 

GoMentum’s grounds offer varied terrain and real-life infrastructure, complete with roads, bridges, tunnels, parking lots, and intersections- most everything encountered in cities and urban areas. TRI’s vice president of autonomous driving Ryan Eustice feels this enclosed testing area will help further Platform 2.1’s development stating, “The addition of GoMentum Station to TRI’s arsenal of automated vehicle test locations allows us to create hazardous driving scenarios for advancing capabilities of both Guardian and Chauffeur and further develop our technology.” That being said, Toyota still has a long way to go before their autonomous vehicles enter the market but this is an important first step as safety for drivers and pedestrians is paramount.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
  • mcb1
    mcb1 over 9 years ago in reply to Catwell

    less congestion

    As long as you don't send it home again ...

     

    and more time saved.

    It's the same/similar route but you get to be passenger, so yes you could do other things.

    That assumes you can travel and read, write without getting car sick image

     

     

     

    Time will tell.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 9 years ago in reply to mcb1

    Imagine; less congestion, less road accidents, more lives saved, and more time saved.

     

    I am looking forward to that day.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    I'm glad to see the reality hasn't yet caught up with the hype from the PR and Spin-doctors.

     

    While human drivers do make mistakes, I'm not aware of a statistic that is used to show crashes per mile (or km).

    Many people have never had an accident or more precisely, never caused an accident or damage.

     

    I also wonder at the cost of these autonomous vehicles. The manufacturer has to recoup their investment and allow for the resulting lawsuit if someone believes it failed.

    This all translates into a higher unit price, which ends up delaying the introduction.

     

    I've had it suggested that it will reduce congestion, but a colleague said why would I have it drive me to work and sit an wait, I may as well send it home again.

     

     

    I can recall a time when computers first starting becoming a household item and we were all told that the days of typing were out, we'd all be speaking to our computer ....image

    I'm still happy to do the driving, and won't be shopping for one of these in the near future.

     

    But thanks for sharing

    Mark