Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum MaaXBoard Chronicles #1 - What Do You Think of the MaaXBoard?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 62 subscribers
  • Views 2867 views
  • Users 0 members are here
  • i.mx8m
  • avnet
  • designed by avnet
  • nxp
  • maaxboard
Related

MaaXBoard Chronicles #1 - What Do You Think of the MaaXBoard?

jafoste4
jafoste4 over 6 years ago

MaaxBoard

 

The MaaXBoard is a low-cost, NXP i.MX 8M processor-based, single board computer ideal for embedded computing and smart edge IoT applications.

image

 

The i.MX 8M family of application processors are based on the ArmRegistered CortexRegistered-A53 and Cortex-M4 cores which provide industry-leading audio, voice, and video processing for applications that scale from consumer home audio to industrial building automation and embedded computers. The MaaXBoard is production ready, FCC-, CE-, and RoHS-certified. It is available in quantities from one to thousands.

The MaaXBoard contains everything necessary to support and create a Linux, Android, Windows 10 IoT Core, or other OS based system. The platform offers several on-board peripherals including 2 GB of DDR4 memory, a Gigabit Ethernet port, dual USB 3.0 host ports, HDMI output, MIPI-DSI, MIPI-CSI, WiFi, Bluetooth Low Energy, and MicroSD card slot. A Raspberry Pi hat compatible expansion connector also provides interfaces for UART, SPI, I2C, and GPIO. These combined capabilities make it an ideal platform for investigating AI, IOT, and multimedia applications.

 

Each MaaXBoard is shipped with a custom passive Heatsink and Quick Start guide to assist developers with getting started on their hardware or software development project. A user supplied 5V/3A USB Type C power supply is required to power the board. A 16 GB microSD card and a HDMI cable is recommended for booting the MaaXBoard and connecting it to a LCD monitor. To jump start your development, Avnet offers supported Android 9.0 and Yocto images available for download. For software debugging, an optional Microchip USB-to-UART evaluation board is recommended, allowing USB terminal access through a UART port on the 40-pin expansion connector.

 

Kit includes:

  • MaaXBoard
  • Passive Heatsink
  • Quick Start Instructions

Features:

Processor
  • NXP i.MX 8M Processor with Quad Arm Cortex-A53 and single Cortex-M4F
Memory
  • 2GB DDR4 SDRAM
  • MicroSD Slot (Default) or 8GB eMMC
User I/O
  • 40 Pin Low Speed Expansion Interface
    • Raspberry Pi Hat Compatible
    • Digital I/O voltage: 3.3V
Mechanical
  • 85mm x 56mm x 12mm form factor
Communications and User Interface
  • Gigabit Ethernet
  • Dual USB 3.0
  • MIPI-DSI
  • MIIP-CSI
  • HDMI – Supports up to 4k resolution
  • Wi-Fi 802.11 b/g/n/ac
  • Bluetooth 4.2 (Bluetooth Low Energy)
  • Onboard Ceramic Antenna (Default)
    • External Antenna supported
  • Audio Expansion
Other
  • Voltage Regulators
  • USB Type C 5V/3A Power input
  • Operating Temperature: 0~70°C

Target Applications:

  • Embedded Computing
  • Machine Vision
  • AI platform
  • Embedded Kiosk
  • Smart IoT Platform

image

 

 

 

If you are interested in the software enablement and support available behind MaaXBoard, please stay on the look out for the MaaXBoard Chronicles #2 coming soon!

 

For additional information please see:

avnet.me/maaxboard

avnet.me/maaxboard-buy

 

So now that you have an idea of the MaaXBoard capabilities and offerings, how would you use this board? What kind of projects would you use this board for? Please leave a comment!

 

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 6 years ago +1
    I think that usability of these RaspberryPi-like boards depends heavily on the supported software (mainly OS) and the support (community) around it. That is why the Raspberry Pi and BeagleBone really stand…
Parents
  • tcmichals
    tcmichals over 6 years ago

    Does the processor support hardware video encoding? i.e. H.264 video encoding?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 6 years ago in reply to tcmichals

    Hi,

     

    No the processor doesn't support hardware video encoding.

    Here are a couple threads that talk about getting SW Video Encoding Support.

     

    https://community.nxp.com/thread/476358

    https://community.nxp.com/thread/475710

    https://community.nxp.com/thread/527612

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jafoste4
    jafoste4 over 6 years ago in reply to tcmichals

    Hi,

     

    No the processor doesn't support hardware video encoding.

    Here are a couple threads that talk about getting SW Video Encoding Support.

     

    https://community.nxp.com/thread/476358

    https://community.nxp.com/thread/475710

    https://community.nxp.com/thread/527612

     

    -Josh