Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16306 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The datasheet did remind me though of a point you mentioned some time back, that the i.MX6's implementation of gigabit Ethernet is constrained by  a design fault which limits its maximum throughput to 400-470Mbps. 

    That's supposedly improved somewhat in more recent steppings, but I agree it's not good.  It doesn't help that seemingly that limitation is aggregate of transmit+receive throughput.

     

    Using PCIe may help, or not. A lot of the desktop gigabit add-in cards (PCIe x1) have a reputation for not being able to reach Gigabit speeds and aparrently this is due to the PCIe connection using small packets and the additional latency this causes. Indeed I have a two port card that uses PCIe x4 obviously in some attempt to mitigate the problem.  The iMX6 only has a single lane PCIe. So you can't expect wonderful performance, especially from a multi-port card.

     

    Solve those issues and you'll still have to work out if the CPU, Memory or other busses within the SoC are up to the task - it's not so long ago that high end servers had problems with gigabit ethernet due to simply not enough cpu horsepower, badly arranged bus topologies etc. They're now having similar sorts of issues with 10Gb ethernet. 

     

    I'd be very surprised if the same sort of issues don't arise for Arm devices. The iMX6 issue is likely just one aspect of this overall problem.  I'm also sure that, in time, there will be a device that's positioned as a communications processor that resolves them. Whether those sorts of SoCs ever appear in a BBB like device is a very different question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I just wonder if there's something more to it, was John right in that other thread suggesting you need two ports ?

     

    Well the only requirement is a physical path to get frames from one EtherCAT device to another --- any physical topology that links masters to slaves will do.  Having two NICs allows you to cascade boards without additional glue hardware so there's a clear cost benefit, but you still have a couple of options available if your boards have only a single NIC.  One is to use them only in pairs, since the start and end of a chain of EtherCAT devices need only one NIC, although that does limit your range of application.  And the other is to use switches configured to replicate traffic on multiple ports to do all the routing between single-NIC EtherCAT boards.  Port replication is available quite widely even on low-end managed switches.

     

    The ICE board also uses a different PHY from BBB, simple cost savings or something not supported ?

     

    I don't know, but my understanding is that there is nothing special about PHYs used for EtherCAT.  As a physical layer device, you would expect it to just encode/decode the standard 802.3 frame without looking at the ethertype.  The choice of PHY is mainly determined by the interface provided by the host MAC, which is typically RMII on application SoCs to keep the pincount low.  The BBB's SMSC LAN8710 PHY supports both MII and RMII, and is supposedly compliant with the various 802.3 specs.

     

    I expect it's all academic though, fairly clear that we simply don't know enough to implement it ourselves right now - at least not without a lot of help from someone who does.

     

    It would indeed be nice to attract some expert on the subject here.  Seeing as Farnell sells so many BBBs for CircuitCo, how about someone asking Gerald Coley to pay us a short visit?  This is actually relevant to current product, because CircuitCo switched over to AM3358 on the original BeagleBone (white) with board revision A6A, so EtherCAT is now gone there, and undoubtedly will disappear soon on BBB as well.  I would like to know the physical reason that prevents the new SoC from supporting it.  It shouldn't be left as a mystery.

     

    Morgaine.

     

     

    PS.  And while we're at it, it would be good to know whether there is anything physically preventing single-NIC EtherCAT operation on AM3359-based BBBs, to avoid disappointment in case someone embarks on an EtherCAT project with expectations of fun.  There are a lot of AM3359-based BBBs out there, as well as A5A BBs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago

    It's Allwinner chips with everything at Olimex! image

     

    • Announcement from their blog.
    • Allwinner chips in Olimex shop.

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

     

    Not only does it support their official position on open hardware by making it easier for people to acquire the necessary components for their own PCBs, but by selling more of the devices, Olimex gains access to more volume from Allwinner and so brings down their own product BOM costs too.  Good plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

    Interesting, but I wonder how many sales of the BGA devices they'll make. Unlike the RPF, I don't presume that it's impossible for hobbiests to handle BGA's at home, but I do think that the number who will have invested the time and effort will be fairly low. Divide that by the number who will want these particular devices and what's left ?

    The other avenue is if they can supply commercial volume, but it wouldn't be unreasonable to think that anyone buying in commercial volumes will either be able to go direct to Allwinner, or will get their outsourced Chinese subcontract manufacturer to just source them locally.

    So good plan, yes. But I must be missing something for this to be much more than interesting PR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Are there places that will just fit a supplied BGA package to a PCB, possibly as part of printing the board?

     

    If so, I can understand enthusiasts in the West being happy to pay Olimex a bit more to avoid liaising with China themselves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Are there places that will just fit a supplied BGA package to a PCB, possibly as part of printing the board?

    I dare say there are. Most of the places I've looked at in the past fall into two broad categories:

    1. PCB Only
    2. Give us the gerbers & BOM we'll source everything and assemble it for you

     

    So I'm sure there's some middle ground if you can find somewhere willing to deal with very low volume prototype stuff.  I've seen places that will supply a laser cut solderpaste stencil almost for free even when ordering relatively small quantities of PCB's.  It starts to become a question of whether the setup of the paste machine, pick&place machine & reflow oven is worth it for one-off or even 10 off type quantities though.

     

    I do seem to remember reading about some newer solderpaste machines that are more like an inkjet printer, so you can selectively do only what's required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    From memory, pcbtrain (excellent manufacturer) will put on a one-off single SMD part (e.g. BGA) for £50, so not cheap, but not completely unaffordable either. I've been working on a reflow machine for over a year now! I might finish it one day. Pcbtrain can supply a metal mask, they sent a sample a while back, it looked very nice (it was steel).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    From memory, pcbtrain (excellent manufacturer) will put on a one-off single SMD part (e.g. BGA) for £50, so not cheap, but not completely unaffordable either.

    Yeah, but whatever you're doing would need to be pretty special to bother. Added to the cost of a PCB and an A20 + PMIC from Olimex and you're likely already at least double the cost of a BBB or RPi.  As a way to prove a prototype for a much bigger production run then sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Sounds like there's a niche for a self-soldering BGA breakout board, containing an on-board heater and clamp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Or a socket: http://www.selwyn.co.uk/index.php?option=com_k2&view=itemlist&task=category&id=13:bga-sockets-adapters

     

    I can imagine those sockets are probably bga's themselves and I'd be surprised if they're not insanely expensive, so 50 quid to get a one-off done may not be so bad after all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>